3.10.4. SGX build guide
The graphics stack on SGX will not receive any new major updates. The last major change occurred in release 09.01. This will capture the build process and some of the caveats of this legacy driver.
As part of the kernel 6.1 support effort, this driver now mimics the build and structure of rogue. The stack consists of 3 main components with varying classifications:
The kernel module (KM) (Open Source, but out-of-tree)
The GLES 2.0 user mode (UM) libraries (Closed Source, binary release)
The mesa shim (Open Source, but out-of-tree)
All 3 of these components are mandatory for GLES support.
3.10.4.1. SGX kernel module
The kernel module is responsible for:
Memory and power management
Monitoring device state
Orchestrating hardware recoveries
Creating an interface for the user space server
The source for this is available at:
3.10.4.1.1. Building the SGX kernel module
The latest branch has the most bug-fixes and has the widest general
compatibility in modern applications. This is 1.17.4948957/mesa/k6.1, and
despite the mention of kernel 6.1 it is also interoperable with kernel 6.6.
The INSTALL file gives a brief overview of how to build and install the
module. This gives you the common variables, but it does omit some of the more
important ones for the build. The following variables are key and must match
with the values used in the UM release:
BUILD– Options:releaseordebug
PVR_BUILD_DIR– Options:<platform>_linux, for exampleti572x_linux
WINDOW_SYSTEM– Options:lws-generic,xorg,wayland, among others
These variables are mandatory. To check for updated build variables see the
EXTRA_OEMAKE variable in the ti-sgx-ddk-km recipe in meta-ti. This will
always contain the latest required variables to compile the driver.
As before mentioned these build options must match with the corresponding UM
build options. Currently we only release binaries with BUILD=release and
WINDOW_SYSTEM=lws-generic. The UM section will go previous exceptions
to this.
3.10.4.2. SGX user space components
The proprietary user space components are necessary for all interactions with the GPU. It has the firmware, GLES implementation, and the primary control server. Unlike rogue, the firmware part of the control sever library.
The binary release is available at:
3.10.4.2.1. Installing the SGX user space components
The repository has binaries for each platform in release specific branches. The
newest release, which matches with the earlier mentioned kernel module branch is
1.17.4948957/mesa/glibc-2.35. This branch deviates from the existing naming
pattern to indicate that unlike previous releases it required a new version of
mesa and was linked against glibc-2.35.
The repository has the following structure:
.
├── LICENSE
├── Makefile
├── README.md
└── targetfs
├── common
│ ├── 50-pvrsrvctl.rules.template
│ ├── etc
│ └── pvrsrvctl.service.template
├── ti335x_linux
│ └── lws-generic
├── ti343x_linux
│ └── lws-generic
├── ti437x_linux
│ └── lws-generic
├── ti443x_linux
│ └── lws-generic
├── ti572x_linux
│ └── lws-generic
└── ti654x_linux
└── lws-generic
Under the targetfs directory there is a subdirectory for each
PVR_BUILD_DIR build variable. Under that directory is a subdirectory
corresponding to the WINDOW_SYSTEM build variable. Finally, under that
directory is a subdirectory corresponding to the BUILD build variable.
This is in the Makefile as:
PRODUCTDIR := ./targetfs/${TARGET_PRODUCT}/${WINDOW_SYSTEM}/${BUILD}
The Makefile simply unpacks this directory structure and installs the
corresponding files into DESTDIR in the install step. Do not worry about the
clean step, as this is for development.
Unlike rogue, there is an additional common directory that has
startup script templates. These templates are automatically modified by the
Makefile as part of the install step.
These are not strictly required, but you will need to manually start the device
with pvrsrvctl if you decide not to use these templates. Please note
that this binary is, and always has been brittle. It likely will not realize
what kernel you are running so you should specify --no-module when
interacting with it.
3.10.4.3. SGX mesa components
Mesa, at this point in time, is a collection of Graphics (GFX) tools and utilities for setting up and interacting with rendering contexts. It has everything from a DRI “megadriver” to full GLES/GL implementations. If you’re interested in learning GFX under Linux it is worth familiarizing yourself with everything else it provides.
For us, the important part is that DRI “megadriver.” This is the mechanism used to decide what GLES / GL implementation gets selected when you bind one of the before mentioned API to a context. This is also where things get tricky.
Historically there has been some issues with embedded GFX because, unlike your standard PC GPU, we tend to mix and match actual Graphics Processing Units and Display Controllers. The megadriver uses the display device name to coordinate between API implementations. As such, we need a shim to act as a DRI driver and coordinate the link with the SGX GLES implementation.
This shim, currently, is in the form of a Gallium Frontend. This is the main reason for the fork and the 60 odd patches we carry at the following repository:
There are also other nice-to-have features there such as additional pixel formats, minor fix-ups, and a few performance tweaks IMG have picked up over the years. The main reason we need it is for that shim.
3.10.4.3.1. Building the SGX mesa components
We recommend following the Mesa build guide for general options. Currently
the mesa components use a standard interface that allows use of any
powervr/* branch equal to or greater than 22.3.5.
The only necessary build options are:
-Dgallium-drivers=sgx– This is a comma separated list, just make sure sgx is present in it.
-Dgallium-sgx-alias=– This should match the display controller you want to bind to. This can either betilcdc,tidss, oromapdrmdepending on the device.
This will produce 3 important files relevant to the shim mechanism we discussed earlier:
sgx_dri.so– Main DRI interface
pvr_dri.so– GPU interface that points back tosgx_dri.so. This is for an application that attempts to interact with the GPU directly because the DRI device is still registered with the namepvr.
<display>_dri.so– Display controller interface that points back atsgx_dri.so. This is from the value specified with-Dgallium-sgx-alias.
3.10.4.4. Using the SGX stack
Assuming you’re using the SDK or you’ve built and installed the preceding correctly, you should see a message similar to the following in dmesg after the kernel module loads:
[ 17.344567] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
If the module loads but does not detect the device, make sure your device tree
has defined the node properly. This corresponds to one of the values of
powervr_id_table in the services4/srvkm/env/linux/module.c.
Upon starting the user space daemon you should see the following message:
[ 29.277564] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
You should now be able to issue a simple test. We recommend glmark2-es2-drm. You should see the following indicating you are using the correct driver:
root@am335x-evm:~# glmark2-es2-drm
MESA: info: Loaded libpvr_dri_support.so
=======================================================
glmark2 2021.12
=======================================================
OpenGL Information
GL_VENDOR: Imagination Technologies
GL_RENDERER: PowerVR SGX 530
GL_VERSION: OpenGL ES 2.0 build 1.17@4948957
=======================================================
The GL_VENDOR should report Imagination Technologies with the renderer
corresponding to the graphics processor in that device.