3.2.2.12.2. Smart Reflex¶
Overview
DRA7 platforms use Class 0 SmartReflex. It is a very simple class of AVS. The SR compensated voltages for different OPPs of various Voltage domains are burnt in the EFUSE registers. So whenever a new OPP is set the SR compensate voltage value for that particular OPP is read from the EFUSE registers and set.
On entering an OPP, the voltage value to be selected is no longer the traditional nominal voltage, but the voltage meant from the efuse offset encoded in millivolts. Each device will have it’s own unique voltage for given OPP. Therefore, it is not possible to encode a range of voltage representing an OPP voltage.
DRA processors may be powered using various PMICs - I2C based ones such as TPS659039 or SPI / GPIO controlled ones as well.
cpufreq/devfreq driver which controls voltage and frequency pairs traditionally used: cpufreq/devfreq --> PMIC regulator \-> clock framework This opens up a few issues: a) PMIC regulator is designed for platforms that may not use SmartReflex based SoCs, encoding the efuse offsets into every possible PMIC regulator driver is practically in-efficient. b) Voltage values are not known a-priori to be encoded into DTB as they device specific.To simplify this, we introduce: cpufreq/devfreq --> SmartReflex Class 0 regulator --> PMIC regulator \-> clock frameworkClass 0 Regulator has information of translating the "nominal voltage" i voltage value stored in efuse offset. Example encoding: uVolts mVolt --> stored as 16 bit hex value of mV 975000 975 --> 0x03CF 1075000 1075 --> 0x0433 1200000 1200 --> 0x04B0[1] https://www.ti.com/lit/ds/sprt659/sprt659.pdf [2] https://www.ti.com/lit/wp/swpy015a/swpy015a.pdf
Source Location
drivers/cpufreq/ti-cpufreq.c