2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the yocto-build/configs/processor-sdk-linux
directory.
Config File |
Description |
Supported machines |
---|---|---|
processor-sdk-linux-09_02_00.txt |
Processor SDK Linux 09_02_00 Release |
am57xx-evm |