6.1. HostΒΆ
- 6.1.1. How to Build a Ubuntu Linux host under VMware
- 6.1.2. Connect to an EVM via Telnet
- 6.1.3. How to Setup a Samba Server
- 6.1.4. Boot Sequence
- 6.1.5. Moving Files to the Target System
- 6.1.6. How to Flash Linux System from U-boot
- 6.1.7. Customizing the SDK Splash Screen
- 6.1.8. How to Develop with 3D Graphics
- 6.1.9. How to Develop accelerated Multimedia using GStreamer on AM57xx
- 6.1.10. Preventing BeagleBone board reset on JTAG Connect
- 6.1.11. Processor SDK IPC Quick Start Guide
- 6.1.12. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux