Processor SDK Linux for AM437X
09_01_00_001
1. Overview
2. Release Specific
3. Foundational Components
4. Industrial Protocols
5. Examples and Demos
6. How to Guides
6.1. Host
6.1.1. How to Build a Ubuntu Linux host under VMware
6.1.2. Connect to an EVM via Telnet
6.1.3. How to Setup a Samba Server
6.1.4. Boot Sequence
6.1.5. Moving Files to the Target System
6.1.6. How to Flash from U-boot Shell
6.1.7. Customizing the SDK Splash Screen
6.1.8. Ubuntu 14.04 Set Up to Network Boot an AM335x/AM437x Based Platform
6.1.9. How to Develop with 3D Graphics
6.1.10. How to Develop accelerated Multimedia using GStreamer on AM57xx
6.1.11. Preventing BeagleBone board reset on JTAG Connect
6.1.12. Processor SDK IPC Quick Start Guide
6.1.13. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux
6.1.14. AM335x to AM437x Hardware Migration Guide
6.2. Target
6.3. Hardware EVM Setup
6.4. Board Port
7. Documentation Tarball
Processor SDK Linux for AM437X
Docs
»
6.
How to Guides
»
6.1.
Host
»
6.1.4.
Boot Sequence
6.1.4.
Boot Sequence
ΒΆ