6. How to GuidesΒΆ
- 6.1. Host
- 6.1.1. How to Build a Ubuntu Linux host under VMware
- 6.1.2. Connect to an EVM via Telnet
- 6.1.3. How to Setup a Samba Server
- 6.1.4. Boot Sequence
- 6.1.5. Moving Files to the Target System
- 6.1.6. How to Flash from U-boot Shell
- 6.1.7. Customizing the SDK Splash Screen
- 6.1.8. Ubuntu 14.04 Set Up to Network Boot an AM335x/AM437x Based Platform
- 6.1.9. How to Develop with 3D Graphics
- 6.1.10. How to Develop accelerated Multimedia using GStreamer on AM57xx
- 6.1.11. Preventing BeagleBone board reset on JTAG Connect
- 6.1.12. Processor SDK IPC Quick Start Guide
- 6.1.13. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux
- 6.1.14. AM335x to AM437x Hardware Migration Guide
- 6.1.14.1. Introduction
- 6.1.14.2. Basic Feature Comparison
- 6.1.14.3. Module Comparison
- 6.1.14.3.1. Processors
- 6.1.14.3.2. Memory Subsystem
- 6.1.14.3.3. Power, Reset, and Clock Management
- 6.1.14.3.4. Multimedia Hardware Components
- 6.1.14.3.5. Communication Interfaces
- 6.1.14.3.6. Timers
- 6.1.14.3.7. Misc
- 6.1.14.3.8. ARM Interrupt Controller
- 6.1.14.3.9. New interfaces in AM437x
- 6.1.14.3.10. Pin and package
- 6.1.14.4. Software Migration Guide
- 6.2. Target
- 6.3. Hardware EVM Setup
- 6.4. Board Port