2.4. Migration Guide for AM437X¶
Overview
This page covers migration information for applications built on top of the Processor SDK for Linux.
As of Oct 2023, Linux SDK for AM437x is in long term maintenance mode. TI will support critical bug fixes and once a year LTS updates but no new development or new features are planned for this device SDK at this time.
2.4.1. Processor SDK 09.xx Releases¶
2.4.1.1. Processor SDK 09.01.00¶
2023 LTS Update release, with new versions of Kernel and U-boot. Please see SDK Components & Versions.
2.4.2. Processor SDK 08.xx Releases¶
2.4.2.1. Processor SDK 08.02.00¶
2021 LTS Update release, with new versions of Kernel and U-boot. Please see SDK Components & Versions.
2.4.3. Processor SDK 07.xx Releases¶
2.4.3.1. Processor SDK 07.03.00¶
2020 LTS Update release, with new versions of Kernel, U-boot, toolchain and Yocto. Please see SDK Components & Versions.
Linux HSR, PRP driver. The source directory is now net/hsr instead of net/hsr-prp and all source files are prefixed as originally with hsr prefix instead of hsr_prp. Consequently CONFIG_HSR_PRP is changed to CONFIG_HSR as well.
ip link command for prp interface creation is changed to use type hsr and a new proto parameter with a value of 1 for prp and 0 for hsr.
PRUETH Driver uses NAPI vs irq thread based processing in older release. User is expected to issue a chrt command and raise priority of softirq daemon to avoid packet loss.
The boot parameters for Ethernet type is now removed. User is expected to switch to HSR/PRP/Switch following instructions from user guide.
Network Storm Prevention now uses tc filter command instead of sysfs file as documented in the User guide.
VLAN/MC filter dump now uses switch-config instead of debugfs.
Tx IRQ is removed for PRUETH EMAC driver because testing showed that performance for small size frames is better with IRQ not used. For MTU frames, Tx IRQ provides better performance. User may add DT entry for Tx IRQ to enable this if the use case is predominantly using MTU size frames to take advantage of this. See Documentation/devicetree/bindings/net/ti-prueth.txt for details on DT changes needed to use Tx IRQ.
PRP Emac mode is obsolete and not supported anymore.
HSR/PRP with PRU-ICSS firmware offload is not supported.
ICSS-EMAC is not supported.
SORTE is not supported.
2.4.4. Processor SDK 06.xx Releases¶
2.4.4.1. Processor SDK 06.03¶
This is a quarterly update release on 2019 LTS stream and final release on that stream.
ICSSM PRUETH: Network storm prevention enhancements. Please check 4.2.4.7 Network Storm Prevention section of user guide, for changes in user interface for configuring storm prevention.
2.4.4.2. Processor SDK 06.02¶
This is a quarterly update release on 2019 LTS stream.
Note that this version of Processor SDK updates only AM5 and AM6 platforms w/ Linux OS.
The SGX driver has been enhanced to replace IMG WSEGL with MESA-EGL which supports the essential EGL 1.5 extensions required by the latest versions of certain graphics applications such as Chromium browser. See here for more details about compatability.
2.4.4.3. Processor SDK 06.01¶
This is a quarterly update release on 2019 LTS stream.
EMAC firmware - PRP Firmware in EMAC mode can be obsolete, as EMAC firmware has been made to be feature parity for SAN
2.4.4.4. Processor SDK 06.00¶
This is the first release in 2019 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch. Please see SDK Components & Versions.
Toplevel Makefile: There are additional packages required on the host, such as flex, bison and libssl-dev, for the top-level Makefile to build successfully. You can find the complete list of required host packages in this chapter
- Resistive Touchscreen TSCADC (resistive touchscreen) wakeup control on AM335x and AM437x has moved from TSCADC MFD device node to TSC input device node.
Disable touchscreen as wakeup source use: echo disabled > /sys/devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc.0.auto/power/wakeup
Enable touchscreen as wakeup source use: echo enabled > /sys/devices/platform/ocp/44e0d000.tscadc/TI-am335x-tsc.0.auto/power/wakeup
- IPC
- Remoteproc core
Error recovery with virtio-rpmsg-bus stack is broken on Upstream vanilla 4.19 kernel. Error recovery is supported only on TI kernels.
- PRUSS remoteproc
The PRUSS remoteproc bindings and drivers have been split up into three separate folders
New bindings are defined in soc/ti/ti,pruss.txt, interrupt-controller/ti,pruss-intc.txt and remoteproc/ti,pru-rproc.txt under the Documentation/devicetree/bindings folder and replaces remoteproc/ti,pruss-remoteproc.txt
PRUSS INTC module pruss_intc.ko is now irq-pruss-intc.ko and is built in drivers/irqchip folder
pruss_soc_bus and pruss platform drivers are now built in drivers/soc/ti folder.
- Userspace
New IPC and CMEM releases are needed to use with 4.19 kernel due to difference in AF_RPMSG family number and other kernel API changes. Minimum required versions are IPC 3.50.03.05 and CMEM 4.16.00.00
- PRUETH
On AM571x IDK boards, the naming of the PRUETH supported ethernet ports has changed. In previous releases, PRU-ICSS1 (J3, J5 on IDK) corresponded to eth4/5, and PRU-ICSS2 (J6, J8 on IDK) corresponded to eth2/3. As of 06.00, this has swapped, and now PRU-ICSS1 corresponds to eth2/3, and PRU-ICSS2 corresponds to eth4/5.
- Jailhouse AM57xx support rebased to v0.10 version
Added shared memory region between Linux, hypervisor, and inmate console
Startup code of the inmate library enables MMU. An inmate has to initialize its MMU table by itself.
2.4.5. Processor SDK 05.xx Releases¶
2.4.5.1. Processor SDK 05.03¶
This release is backwards compatible with 05.02 release.
2.4.5.2. Processor SDK 05.02¶
The minimum SD card size is now 16GB when creating an SD card with the default images for Processor SDK Linux.
Multicast Filtering Mask
The parameter for setting a multicast filtering mask is now ‘pruss<ID>_port<PORT>_mc_mask’ instead of ‘pruss<ID>_mc_mask’ because support was added to enable per port multicast filtering for Dual EMAC.
ip link command
ip link parameter for setting up VLAN tag for HSR/PRP, sv_cfi is renamed to sv_dei.
2.4.5.3. Processor SDK 05.01¶
Introduced AM65x as a new platform. Please refer to release notes for more details
PRUETH Driver
1. debugfs file path has changed
The path for debugfs file has changed to include the PRU-ICSS ID as there could be upto two instances of offloaded hsr/prp prueth driver and so has to distictly identify which instance the debugfs file refers to.
For example, the path for hsr/prp changed from
/sys/kernel/debug/prueth-<hsr/prp>/
to
/sys/kernel/debug/prueth-<hsr/prp>-<ID>/
Where ID is the PRU-ICSS ID as described in the HSR/PRP User Guide.
For HSR on PRU-ICSS2 of AM571x, path is changed to /sys/kernel/debug/prueth-hsr-2/
For HSR on PRU-ICSS1 of AM571x, path is changed to /sys/kernel/debug/prueth-hsr-1/
For PRP on PRU-ICSS2 of AM571x, path is changed /sys/kernel/debug/prueth-prp-2/
for PRP on PRU-ICSS1 of AM571x, path is changed to /sys/kernel/debug/prueth-prp-1/
All of the existing debugfs files except prp_emac_mode have moved to the new location. prp_emac_mode is now changed to sysfs file as decribed in the below section. The files are not writeable anymore as it is meant only for showing debug information. The write functions are moved to the upper layer HSR/PRP driver and implemented though proc entries. See the Linux HSR/PRP driver section for more details.
2. sysfs file path has changed
The path for sysfs files have also changed from
/sys/devices/platform/pruss<ID>_eth/eth2/
to
/sys/devices/platform/pruss<ID>_eth/net/eth2/
Where ID is the PRU-ICSS ID as described in the User Guide.
For example, nsp_credit sysfs file is now accessed at
/sys/devices/platform/pruss2_eth/net/eth2/nsp_credit
prp_emac_mode file is at
/sys/devices/platform/pruss2_eth/net/eth2/prp_emac_mode
Linux HSR/PRP Driver
1. debugfs file path has changed
The debugfs file directory created by the driver now uses the interface name so that multiple instances of the device can co-exist and each will have its own unique path names.
Path is now changed from
/sys/kernel/debug/<hsr/prp>/
to
/sys/kernel/debug/<if_name>/
For example, if hsr interface name is hsr0, the path will be - /sys/kernel/debug/hsr0/
Write functions are now supported through proc entries. So similar functions are removed from debugfs. See below section for details of proc entries. stats file is renamed to lre_info which shows SV frame tx count along with additional debug information about the LRE.
2. proc file paths
Following commands can be used for updating values at the prueth offloaded device which was earlier supported through debugfs files at the prueth device.
/proc/<if_name>/clear-nt - Replaces /sys/kernel/debug/prueth-<hsr/prp>/node_table_clear
/proc/<if_name>/hsr-mode - Replaces /sys/kernel/debug/prueth-<hsr/prp>/hsr_mode
/proc/<if_name>/dlrmt - Replaces /sys/kernel/debug/prueth-<hsr/prp>/dup_list_reside_max_time
/proc/<if_name>/dd-mode - Replaces /sys/kernel/debug/prueth-<hsr/prp>/duplicate_discard
/proc/<if_name>/prp-tr - Replaces /sys/kernel/debug/prueth/transparent_reception
2.4.5.4. Processor SDK 05.00¶
This is the first release for 2018 LTS (Kernel: 4.14, U-boot: 2018.01, gcc: 7.2.1 and Yocto: 2.4 (rocko)).
With Yocto migration, several open source components (Qt, Wayland, Weston, GStreamer, iPerf, etc.) are all upgraded. For the exact versions of the new components, please refer to the Software Manifest., and for any migration issues, refer to the corresponding component’s release notes, and Processor SDK Known Issues list.
Following are major compatability changes for TI drivers, components.
- IPC
- Remoteproc core
RPMSG_VIRTIO is no longer automatically selected by remoteproc platform drivers, has to be enabled specifically in defconfigs
The RSC_CUSTOM remoteproc custom resource type has been replaced with two new RSC_PRELOAD_VENDOR and RSC_POSTLOAD_VENDOR resource types.
Two new debugfs variables “resource_table” and “carveout_memories” are added to print the resource table and carveout memories used by a remoteproc
Error recovery with virtio-rpmsg-bus stack is broken on Upstream vanilla 4.14 kernel. Error recovery is supported only on TI kernels.
- PRUSS remoteproc
- The PRUSS remoteproc bindings have been revised significantly to improve scalability and flexibility
New child nodes are added to represent the CFG, IEP and MII_RT sub-modules.
Default firmware names are moved from driver to DT
Client users will require a new “prus” mandatory property instead of the previous “pruss” property
“ti,pruss-gp-mux-sel” property is removed from PRU nodes and added as an optional property to client nodes.
“label” property is dropped from PRU nodes
“interrupts” and “interrupt-names” properties were moved from INTC node to their parent node.
Client user API has changed to acquire and use a PRU core
- Keystone_remoteproc
The “label” binding property is dropped from the driver bindings, and is replaced with an alias using the stem “rproc”
The “ti,sci-id” property for K2G DSP nodes is also dropped.
The keystone-dsp-mem driver is converted to a regular module from a platform driver, so the dspmem nodes are dropped. The module uses revised bindings.
- Userspace
New IPC and CMEM releases are needed to use with 4.14 kernel due to difference in AF_RPMSG family number and other kernel API changes
iperf2 is now replaced by iperf3
Keystone-2: PA/PA2 is not supported in NetCP driver.
Keystone-2: NWAL is not supported
MMC: AM57x uses sdhci-omap.c driver instead of omap_hsmmc.c driver
PCIe: The way in which PCIe endpoint is configured has changed. More details can be found from PCIe End Point Driver.
AM335x ICE v2: A new DT file (am335x-ice-v2-prueth.dts) is added to support PRUSS Ethernet ports. The following configurations are supported.
am335x-ice-v2.dts: Both ports are CPSW controlled (Board jumpers J18 and J19 at RMII).
am335x-ice-v2-prueth.dts: Both ports are PRUSS controlled (Board jumpers J18 and J19 at MII).
Also note that there is an update to the u-boot env script to select DTB file
name based on jumper settings. So user needs to do following when upgrading
to the latest u-boot from this release:
>env default -a
>saveenv
>reset
2.4.6. Processor SDK 04.xx Releases¶
2.4.6.1. Processor SDK 04.03¶
Added am572x-idk-pps.dts and am571x-idk-pps.dts which are extensions of the am572x-idk.dts abd an571x-idk.dts respectively. The new DTS enables the PPS IO pins (sync/latch) and PTP BC bindings at the modified AM572x-idk and AM571x-idks, where the USB/LCD Display are disabled
Camera support for AM572x GPEVM is not in the default DTB.Use am57xx-evm*-cam-mt9t111.dtb for mt9t111 camera, and am57xx-evm*-cam-ov10635.dtb for ov10635 camera
Processor SDK documentation is now created from reStructuredText sources using Sphinx, and hosted on software-dl.ti.com instead of processors wiki
For AM57xx, with the addition of new components in the filesystem, the minimum SD-card size is 8 GB (4 GB SD cards no longer work).
For am57xx devices, the location of the saved U-Boot environment has moved from the external SD card to eMMC. Because of this change, the state of the U-Boot environment can no longer be guaranteed on a newly created SD card. The uEnv.txt file located on the boot partition of the SD card contains the logic to compensate for this change. Upon the initial boot, the environment will be reset to the default, and the empty file “.psdk_setup” will be created on the boot partition. Subsequent boots will detect this file and bypass resetting the environment.
2.4.6.2. Processor SDK 04.02¶
Linux
PRUETH Driver
2.4.6.3. Processor SDK 04.01¶
IPC
PRUSS remoteproc
PRUs are no longer automatically booted (remoteproc ‘auto_boot’ is set to false) by remoteproc core. A PRU has to be booted either by PRU Client Drivers or a PRU applications in userspace. The kernel-space boot is triggered using the rproc_boot() kernel API, and the user-space applications can use the sysfs to start and stop the corresponding remoteproc. Please see Documentation/ABI/testing/sysfs-class-remoteproc file in kernel for sysfs usage details.
PRU remoteproc driver no longer configures the PRU Ethernet firmwares automatically using board-machine compatibles. The needed firmware names are configured by the PRU Ethernet driver now using the rproc_set_firmware() function.
Userspace PRU applications have to make sure to unload any existing PRU client drivers using a specific PRU, and set their firmware using sysfs before starting and using a PRU
2.4.6.4. Processor SDK 04.00¶
This is the first release for 2017 LTS (Kernel: 4.9, U-boot: 2017.01, gcc: 6.2.1 and Yocto: 2.2 (morty)), with following major changes.
IPC
remoteproc
The debugfs ‘state’ variable is replaced with a sysfs ‘state’ variable accepting ‘start’ and ‘stop’ to boot and shutdown a remote processor from userspace
A new sysfs variable ‘firmware’ is also added to set a new firmware. remoteprocs need to be in stopped state before a firmware can be set. New firmwares still need to reside in /lib/firmware
Booting a remote processor is now triggered by the insertion of the respective remoteproc platform driver. On 4.4, with virtio-rpmsg enabled firmwares, this only happened when both the remoteproc platform driver and virtio_rpmsg_bus module were installed.
Upstream 4.9 remoteproc and rpmsg cores are not suitable for TI platforms. A minimum of 4.10-rc4 (or the required remoteproc/rpmsg patches from 4.10-rc4) is needed if porting TI remoteproc drivers onto upstream.
rpmsg
virtio_rpmsg_bus module split into a ‘rpmsg_core’ and virtio-rpmsg transport specific ‘virtio_rpmsg_bus’ modules.
Removal of virtio_rpmsg_bus no longer stops a remote processor and should be avoided if a remote processor is running. * If removed and installed again, the rpmsg communication devices will not be reprobed.
Keystone_remoteproc
A new ‘label’ binding property is now mandatory. It will have the string names for the DSPs in the format “dsp<X>” (eg: dsp0, dsp7 etc)
K2G DSP nodes will require a new “ti,sci-id” property, and a different value for “power-domains” property (this is generic to all K2G devices)
PRUSS remoteproc
The AM437x specific am437x_pruss_wrapper module has been replaced with a generic pruss_soc_bus module, and is required to be installed on all SoCs.
New compatibles on AM335x and AM437x SoCs - The previous ‘am3352-xxx’ and ‘am4372-xxx’ have been replaced with a ‘am3356-xxx’ and ‘am4376-xxx’ compatibles since PRUSS are not present on AM3352 and AM4372 SoCs. The PRU nodes are also not enabled by default in base ‘am33xx.dtsi’ and ‘am4372.dtsi’ files.
New device hierarchy structure - The PRUSS node hierarchy from 4.4 is moved one-level down under a new parent pruss_soc_bus node.
CPSW CPDMA Descriptor Usage
There is a notable change in how to place cpsw cpdma descriptors in DDR and configure descs number: TI K4.4 device tree property was used “descs_pool_size” - descs_pool_size : total number of CPDMA CPPI descriptors to be used for both ingress/egress packets processing. if not specified the default value 256 will be used which will allow to place descriptors pool into the internal CPPI RAM.
New approach https://processors.wiki.ti.com/index.php/Linux_Core_CPSW_User%27s_Guide#Configure_number_of_TX.2FRX_descriptors
PCI ENDPOINT
The usage of ‘pci-ep’ configfs directory to configure PCI Endpoint has been changed in accordance with upstream review comments. Please see https://processors.wiki.ti.com/index.php/Linux_Core_PCIe_EP_User%27s_Guide#4.9_Kernel, for additional details
Display
fbdev is only set up for the primary display, instead of all displays. This results in the secondary displays to be left disabled by the kernel, until an userspace application enables the displays.
U-Boot RNDIS boot
AM335x USB client (RNDIS) boot and Ethernet boot modes are now supported using default defconfig (am335x_evm_defconfig). Similarly AM437x USB client (RNDIS) boot is now supported by am43xx_evm_defconfig. Separate defconfigs for above boot modes no longer exist.
Keystone-2 features
The following features are not ported to 2017 LTS
SRIO Kernel driver
10G Uboot
IPSec sideband and inflow mode
QoS
2.4.7. Processor SDK 03.xx Releases¶
2.4.7.1. Processor SDK 03.03¶
HDMI-connected monitor no longer takes precedence over built-in LCD as a default graphics display for e.g. Matrix
See the Release Notes for full list of modifications.
2.4.7.2. Processor SDK 03.02¶
The QT QPA eglfs_kms, which supports multiple screens, has been enabled and used as the default eglfs platform plugin. For more information, see QT and Graphics Migration
bootmonitor now goes thru mkimage and as a result the load address changed. Users should manually execute following commands in their u-boot environment to properly install the secure monitor on k2 platforms:
setenv addr_mon 0xc08000
setenv addr_mon_mkimg 0xc07ffc0
setenv mon_size 0x1210
setenv sec_bm_install 'go ${addr_mon}4 0xc084000 ${mon_size}; mon_install ${addr_mon_mkimg}'
run sec_bm_install
HDMI-connected monitor no longer takes precedence over built-in LCD as a default graphics display for e.g. Matrix
2.4.7.3. Processor SDK 03.01¶
defconfig_builder is now used to generate working kernel defconfigs
In K2 U-Boot, added multi slave support.
In K2 Linux PA driver, added pre-classification support. So explicit lut rules for broadcast and multicast are removed and the same is achieved through this feature in PA
10G Ethernet driver now supports auto configuration using MCU firmware (a.k.a 10G KR firmware). The firmware file name is ks2_xgbe_serdes_mcu_fw.bin which is available at the same location as other serdes firmwares.
The current version of the serdes firmware is 03.03.00.02C and the same is not backward compatible with the firmware in the previous SDK release (03.00.00)
2.4.7.4. Processor SDK 03.00¶
First 2016 LTS Release (Linux Kernel: 4.4, U-Boot: 2016.05, GCC 5.3, Yocto 2.1)
Unified kernel configuration based on multi_v7_defconfig
Migrated from SysVinit to systemd for user space initialization.
U-Boot drivers now uses DT, but is transparent to users
The content of <evm>-<os>-sdk-arago-src-<ver>.tar.gz on the download page changed from sources to a fetcher script that obtains the sources. This is to efficiently share the sources between different platforms and OSes supported by Processor SDK. See the README inside the tar-ball for instructions
This release adds support for RT Linux on AM335x ICE and K2G GPEVM
In K2 U-Boot, multi slave support is currently missing. To use multiple interfaces, please disable CONFIG_DM_ET option in u-boot .config and build.
See the Release Notes for full list of modifications.
2.4.8. Processor SDK 02.xx Releases¶
2.4.8.1. Processor SDK 02.00.02¶
This release adds RT Linux support on AM335x, K2H/K, K2E, K2L
This release supports AM572x IDK and K2G EVM
OpenCV now uses OpenCL under the hood, to offload compute tasks to C66x cores. This is transparent to the application
The SGX driver for AM335x has been enhanced to support DRM/WAYLAND based Multi-Window Display. For more information, see AM3 Graphics Migration
See the Release Notes for full list of modifications.
2.4.8.2. Processor SDK 02.00.01¶
This release adds support for devices from the KeyStone architecture: K2E, K2H/K, and K2L
This release also supports RT Linux is supported on AM4 and AM5 device
The SGX driver for AM4 has been enhanced to support DRM/WAYLAND based Multi-Window Display. For more information, see AM4 Graphics Migration
There is no migration impact to customers using AM3, and AM5.
See the Release Notes for full list of modifications.
2.4.8.3. Processor SDK 02.00.00¶
This release adds support for AM57x
First 2015 LTS (Kernel 4.1, U-boot 2015.07) Release
Starting this release, Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines
For AM3, AM4, Graphics SDK is now obsolete and Graphics stack is integrated into Processor SDK, and supports null DRM based Full Window, with Front and Flip modes. For more information, see Graphics Migration
Ethernet performance degraded ~10% on am335x-evm due to move from preempt_voluntary
See the Release Notes for full list of modifications.