2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk
directory of the oe-layersetup git repo.
Config File | Description | Supported machines/platforms |
---|---|---|
processor-sdk-08.02.00.23-config.txt | Processor SDK 08.02.00.23 Release | am64xx-evm, am64xx-hs-evm |
processor-sdk-08.02.00.24-config.txt | Processor SDK 08.02.00.24 Release | am335x-evm, am335x-hs-evm, am437x-evm, am437x-hs-evm |