3.1.1.5. SD, eMMC and USB

The commands for using SD cards, eMMC flash and USB mass storage devices (hard drives, flash drives, card readers, etc) are all very similar. The biggest difference is that on some hardware we may not be able to run U-Boot out of ROM from the storage device as it is unsupported. Once U-Boot is running however, any of these may be used for the kernel and the root filesystem.

Usually in all the platforms there will be two MMC instances of which one would be SD and the other would be eMMC. The index of them can vary from one class of platforms to the other. For a given platform, the device number (device num) can be found in the following way,

U-Boot# mmc list
sdhci@fa10000: 0 (eMMC)
sdhci@fa00000: 1 (SD)

3.1.1.5.1. Partitioning eMMC from U-Boot

The eMMC device typically ships without any partition table. We make use of the GPT support in U-Boot to write a GPT partition table to eMMC. In this case we need to use the uuidgen program on the host to create the UUIDs used for the disk and each partition.

$ uuidgen
...first uuid...
$ uuidgen
...second uuid...
U-Boot # printenv partitions
uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
U-Boot # setenv uuid_gpt_disk ...first uuid...
U-Boot # setenv uuid_gpt_rootfs ...second uuid...
U-Boot # gpt write mmc <device num> ${partitions} /* <device num> is device index obtained from mmc list for eMMC */

A reset is required for the partition table to be visible.

3.1.1.5.2. Updating an SD card from a host PC

This section assume that you have created an SD card using the script “create-sdcard.sh” packaged inside the installer or have made a compatible layout by hand. In this case, you will need to copy the all the boot images (MLO and u-boot.img for 32-bit platforms, tiboot3.bin, sysfw.itb, tispl.bin, u-boot.img for K3 based platforms, except AM64x and J7200 in which sysfw.itb is already combined with tiboot3.bin) files to the boot partition. At this point, the card is now bootable in the SD card slot. We default to using /boot/${bootfile} on the rootfs partition and the device tree file loaded from /boot with the same name as in the kernel.

3.1.1.5.3. Updating an SD card or eMMC using DFU

To see the list of available places to write to (in DFU terms, altsettings) use the mmc part command to list the partitions on the MMC device and printenv dfu_alt_settings_mmc or dfu_alt_settings_emmc to see how they are mapped and exposed to dfu-util.

U-Boot# mmc part

Partition Map for MMC device 0  --   Partition Type: DOS

Partition     Start Sector     Num Sectors     Type
    1                   63          144522       c Boot
    2               160650         1847475      83
    3              2024190         1815345      83
U-Boot# printenv dfu_alt_info_mmc
dfu_alt_info=boot part 0 1;rootfs part 0 2;MLO fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1"

Note

The above command mmc part lists the partitions in the current selected device. So, to list the partitions in eMMC or SD one needs to switch to the required device by using the command mmc dev <device num>.

This means that you can tell dfu-util to write anything to any of:

  • boot

  • rootfs

  • MLO

  • u-boot.img

  • uEnv.txt

And that the MLO, u-boot.img and uEnv.txt files are to be written to a FAT filesystem.

To start DFU on the target on the first MMC device:

U-Boot # setenv dfu_alt_info ${dfu_alt_info_mmc}
U-Boot # dfu 0 mmc 0

On boards like AM57x GP EVM or BeagleBoard x15, where the second USB instance is used as USB client, the dfu command becomes:

U-Boot # dfu 1 mmc 0

Then on the host PC to write MLO to an existing boot partition:

$ sudo dfu-util -D MLO -a MLO

On the host PC to overwrite the current boot partition contents with a new created on the host FAT filesystem image:

$ sudo dfu-util -D fat.img -a boot

3.1.1.5. Updating an SD card or eMMC with RAW writes

In some cases it is desirable to write MLO and u-boot.img as raw images to the MMC device rather than in a filesystem. eMMC requires this, for example. In that case, the following is how to program these files and not overwrite the partition table on the device. We assume that the files exist on a SD card. In addition you may wish to write a filesystem image to the device, so an example is also provided.

U-Boot # mmc dev 0
U-Boot # mmc rescan
U-Boot # mmc dev 1
U-Boot # fatload mmc 0 ${loadaddr} MLO
U-Boot # mmc write ${loadaddr} 0x100 0x100
U-Boot # mmc write ${loadaddr} 0x200 0x100
U-Boot # fatload mmc 0 ${loadaddr} u-boot.img
U-Boot # mmc write ${loadaddr} 0x300 0x400
U-Boot # fatload mmc 0 ${loadaddr} rootfs.ext4
U-Boot # mmc write ${loadaddr} 0x1000 ...rootfs.ext4 size in bytes divided by 512, in hex...

3.1.1.5.4. Booting Linux from SD card or eMMC

Within the default environment for each board that supports SD/MMC there is a boot command called mmcboot that will set the boot arguments correctly and start the kernel. In this case however, you must first run loaduimagefat or loaduimage to first load the kernel into memory. For the exact details of each use printenv on the mmcboot, loaduimagefat and loaduimage variables and then in turn printenv other sub-sections of the command. The most important variables here are mmcroot and mmcrootfstype.

3.1.1.5.5. Booting tiboot3.bin, tispl.bin and u-boot.img from eMMC boot partition (For K3 class of SoCs)

The K3 based processors support booting from the eMMC boot partition. The following commands can be used to download tiboot3.bin, tispl.bin and u-boot.img from an SD card and write them to the eMMC boot0 partition at respective addresses.

Note

By default, SDK chooses boot0 partition for eMMC boot (equivalently done using mmc partconf 0 1 1 1). Boot partition can also be switched from boot0 to boot1 by using mmc partconf 0 1 2 1. This enables booting from boot1 partition. Switch to boot1 partition using mmc dev 0 2 and follow regular eMMC write commands (seen below). On rebooting with regular eMMC dip switch settings, boot1 partition will be used.

=> mmc dev 0 1
=> fatload mmc 1 ${loadaddr} tiboot3.bin
=> mmc write ${loadaddr} 0x0 0x400
=> fatload mmc 1 ${loadaddr} tispl.bin
=> mmc write ${loadaddr} 0x400 0x1000
=> fatload mmc 1 ${loadaddr} u-boot.img
=> mmc write ${loadaddr} 0x1400 0x2000
=> fatload mmc 1 ${loadaddr} sysfw.itb
=> mmc write ${loadaddr} 0x3600 0x800

For loading images from a FAT partition on a different media, replace mmc with the required media. For example, to load images from a FAT partition on a USB Storage device connected to the zeroth instance of usb,

=> fatload usb 0 ${loadaddr} <file name>

To give the ROM access to the boot partition, the following commands must be used for the first time:

=> mmc partconf 0 1 1 1
=> mmc bootbus 0 2 0 0
  • eMMC layout:

           boot0 partition (8 MB)                        user partition
   0x0+----------------------------------+      0x0+-------------------------+
      |     tiboot3.bin (512 KB)         |         |                         |
 0x400+----------------------------------+         |                         |
      |       tispl.bin (2 MB)           |         |                         |
0x1400+----------------------------------+         |        rootfs           |
      |       u-boot.img (4 MB)          |         |                         |
0x3400+----------------------------------+         |                         |
      |      environment (128 KB)        |         |                         |
0x3500+----------------------------------+         |                         |
      |   backup environment (128 KB)    |         |                         |
0x3600+----------------------------------+         |                         |
      |          sysfw (1 MB)            |         |                         |
0x3E00+----------------------------------+         +-------------------------+

To boot from UDA parition of eMMC. Please set following

=> mmc partconf 0 1 7 1
=> mmc bootbus 0 2 0 0

Note

rootfs is written to the user partition. The user partition is first required to be formatted as a ext4 file system and then the rootfs has to be written. It is not possible to format a partition to ext4 in U-Boot. It is required to boot to kernel and write rootfs to user partition after formatting it to ext4. Kernel image and DT are expected to be present in the /boot folder of rootfs.

To boot kernel from eMMC, use the following commands after writing rootfs to user partition:

=> setenv mmcdev 0
=> setenv bootpart 0
=> boot

3.1.1.5.6. Booting to U-Boot prompt from USB storage

Note

While using usb reset or usb start command in U-Boot, or booting from a USB Mass storage device, some of the USB devices fail to get detected. This issue is seen because these USB devices are failing to follow the spec for power good delay. It can be resolved by overriding the power good delay using the environment variable usb_pgood_delay. Setting it to 2000 should be good enough for all cases.

3.1.1.5.7. Booting Linux from USB storage

3.1.1.5. Booting Linux from USB storage

To load the Linux Kernel and rootfs from USB rather than SD/MMC card on AMx/DRA7x EVMs, if we assume that the USB device is partitioned the same way as an SD/MMC card is, we can utilize the mmcboot command to boot. To do this, perform the following steps:

U-Boot # usb start
U-Boot # setenv mmcroot /dev/sda2 ro
U-Boot # run mmcargs
U-Boot # run bootcmd_usb

On K2H/K/E/L EVMs, the USB drivers in Kernel needs to be built-in (default modules). The configuration changes are:

CONFIG_USB=y
CONFIG_USB_XHCI_HCD=y
CONFIG_USB_XHCI_PCI=y
CONFIG_USB_XHCI_PLATFORM=y
CONFIG_USB_STORAGE=y
CONFIG_USB_DWC3=y
CONFIG_USB_DWC3_HOST=y
CONFIG_USB_DWC3_KEYSTONE=y
CONFIG_EXTCON=y
CONFIG_EXTCON_USB_GPIO=y
CONFIG_SCSI_MOD=y
CONFIG_SCSI=y
CONFIG_BLK_DEV_SD=y

The USB should have boot partition of FAT32 format, and rootfs partition of EXT4 format. The boot partition must contain the following images:

keystone-<platform>-evm.dtb
skern-<platform>.bin
k2-fw-initrd.cpio.gz
zImage

where <platform>=k2hk, k2e, k2l

The rootfs partition contains the filesystem from ProcSDK release package.

# mkdir /mnt/temp
# mount -t ext4 /dev/sdb2 /mnt/temp
# cd /mnt/temp
# tar xvf <Linux_Proc_Sdk_Install_DIR>/filesyste/tisdk-server-rootfs-image-k2hk-evm.tar.xz
# cd /mnt
# umount temp

Set up the following u-boot environment variables:

setenv args_all 'setenv bootargs console=ttyS0,115200n8 rootwait'
setenv args_usb 'setenv bootargs ${bootargs} rootdelay=3 rootfstype=ext4 root=/dev/sda2 rw'
setenv get_fdt_usb 'fatload usb 0:1 ${fdtaddr} ${name_fdt}'
setenv get_kern_usb 'fatload usb 0:1 ${loadaddr} ${name_kern}'
setenv get_mon_usb 'fatload usb 0:1 ${addr_mon} ${name_mon}'
setenv init_fw_rd_usb 'fatload usb 0:1 ${rdaddr} ${name_fw_rd}; setenv filesize <hex_len>; run set_rd_spec'
setenv init_usb 'usb start; run args_all args_usb'
setenv boot usb
saveenv
boot

Note:: <hex_len> must be at least the hex size of the k2-fw-initrd.cpio.gz file size.

3.1.1.5. Booting from SD/eMMC from SPL (Single stage or Falcon mode)

Note

Falcon mode is not supported on K3 family of devices.

In this boot mode SPL (first stage bootloader) directly boots the Linux kernel. Optionally, in order to enter into U-Boot, reset the board while keeping ‘c’ key on the serial terminal pressed. When falcon mode is enabled in U-Boot build (usually enabled by default), MLO checks if there is a valid uImage present at a defined offset. If uImage is present, it is booted directly. If valid uImage is not found, MLO falls back to checking if the uImage exists in a FAT partition. If it fails, it falls back to booting u-boot.img.

The falcon boot uses uImage. To build the kernel uImage, you will need to keep the U-Boot tool mkimage in your $PATH

# make uImage modules dtbs LOADADDR=80008000

If kernel is not build with CONFIG_CMDLINE to set correct bootargs, then add the needed bootargs in chosen node in DTB file, using fdtput host utility. For example, for DRA74x EVM:

# fdtput -v -t s arch/arm/boot/dts/dra7-evm.dtb "/chosen" bootargs "console=ttyO0,115200n8 root=<rootfs>"

MLO, u-boot.img (optional), DTB, uImage are all stored on the same medium, either the SD or the eMMC. There are two ways to store the binaries in the SD (resp. eMMC):

* raw: binaries are stored at fixed offset in the medium
* fat: binaries are stored as file in a FAT partition

To flash binaries to SD or eMMC, you can use DFU. For SD boot, from u-boot prompt

=> env default -a; setenv dfu_alt_info ${dfu_alt_info_mmc}; dfu 0 mmc 0

For eMMC boot, from u-boot prompt

=> env default -a; setenv dfu_alt_info ${dfu_alt_info_emmc}; dfu 0 mmc 1

Note: On boards like AM57x GP EVM or BeagleBoard x15, where the second USB instance is used as USB client, replace “dfu 0 mmc X” with “dfu 1 mmc X”

On the host side: binaries in FAT:

$ sudo dfu-util -D MLO -a MLO
$ sudo dfu-util -D u-boot.img -a u-boot.img
$ sudo dfu-util -D dra7-evm.dtb -a spl-os-args
$ sudo dfu-util -D uImage -a spl-os-image

raw binaries:

$ sudo dfu-util -D MLO -a MLO.raw
$ sudo dfu-util -D u-boot.img -a u-boot.img.raw
$ sudo dfu-util -D dra7-evm.dtb -a spl-os-args.raw
$ sudo dfu-util -D uImage -a spl-os-image.raw

If the binaries are files in a fat partition, you need to specify their name if they differ from the default values (“uImage” and “args”). Note that DFU uses the names “spl-os-image” and “spl-os-args”, so this step is required in the case of DFU. From u-boot prompt

=> setenv falcon_image_file spl-os-image
=> setenv falcon_args_file spl-os-args
=> saveenv

Set the environment variable “boot_os” to 1. From u-boot prompt

=> setenv boot_os 1
=> saveenv

Set the board boot from SD (or eMMC respectively) and reset the EVM. The SPL directly boots the kernel image from SD (or eMMC).

3.1.1.5.8. Steps for working around SD card issues

In some cases issue can be seen while using some SD cards, like

  1. Error while trying to initialize,

    U-Boot SPL 2021.01-g74fc69c889 (May 19 2022 - 02:44:29 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi')
    Trying to boot from MMC2
    spl: mmc init failed with error: -110
    SPL: failed to boot from all boot devices
    ### ERROR ### Please RESET the board ###
    

Given below are the list of various workarounds that can be done in the device tree node to get SD card working. The workarounds are ordered in increasing order of reducing performance.

All the mentioned below, are to be done in the MMCSD device tree node corresponding to the SD instance. This is usually the first(index starting from zero) instance.

  1. Restricting to a given speed mode

    • By default the U-Boot driver tries to enumerate a SD card in the highest supported speed mode. Given below is the order in which the driver tries to enumerate a SD card

      • SDR104

      • SDR50

      • DDR50

      • SD HS

      • SD legacy

    • These speed capabilites can be masked using device tree property sdhci-caps-mask.

      • Limit to SDR50: sdhci-caps-mask = <0x00000004 0x00000000>

      • Limit to DDR50: sdhci-caps-mask = <0x00000006 0x00000000>

      • Limit to SD HS: sdhci-caps-mask = <0x00000007 0x00000000>

      • Limit to SD legacy: sdhci-caps-mask = <0x00000007 0x00200000>

        &sdhci1 {
            /* SD/MMC */
           vmmc-supply = <&vdd_mmc1>;
           vqmmc-supply = <&vdd_sd_dv>;
           pinctrl-names = "default";
           pinctrl-0 = <&main_mmc1_pins_default>;
           ti,driver-strength-ohm = <50>;
           disable-wp;
           sdhci-caps-mask = <0x00000006 0x00000000>; /* Limiting to DDR50 speed mode */
        };
        
  2. Increase power cycle period

    • Increasing the delay while power cycling the SD card. This can be done by increasing the delay value in the diff indicated below,

      diff --git a/drivers/mmc/mmc.c b/drivers/mmc/mmc.c
      index f486e2a2c364..38cc956b3d53 100644
      --- a/drivers/mmc/mmc.c
      +++ b/drivers/mmc/mmc.c
      @@ -2761,7 +2761,7 @@ static int mmc_power_cycle(struct mmc *mmc)
               * SD spec recommends at least 1ms of delay. Let's wait for 2ms
               * to be on the safer side.
               */
      -       udelay(2000);
      +       udelay(4000);
              return mmc_power_on(mmc);
       }
      
  3. Reduce the bus width

    • The SD interface supports a bus width of 4. It can be reduced to 1 by changing the bus-width device tree property from 4 to 1.

      diff --git a/arch/arm/dts/k3-am62-main.dtsi b/arch/arm/dts/k3-am62-main.dtsi
      index c06ec7355035..4ab29b6aa4b7 100644
      --- a/arch/arm/dts/k3-am62-main.dtsi
      +++ b/arch/arm/dts/k3-am62-main.dtsi
      @@ -373,7 +373,7 @@
                      ti,itap-del-sel-sdr12 = <0x0>;
                      ti,itap-del-sel-sdr25 = <0x0>;
                      ti,clkbuf-sel = <0x7>;
      -               bus-width = <4>;
      +               bus-width = <1>;
       };
      
       sdhci2: mmc@fa20000 {