3.6.10. Migration from prior releases

3.6.10.1. from Processor SDK 1.x to 2.x for AM3, AM4

The SGX driver has been enhanced to support DRM based Full Window Display in processor SDK 2.0 and the FBdev based Full Window modes are no longer supported. The System startup and most of the Graphics applications are backward-compatible except with the following changes.

Window System Libraries

The FBdev based Full Screen window systems are no longer supported:

  • libpvrPVR2D_FRONTWSEGL.so (for direct writes to FrameBuffer - FRONT mode of operation - directly writes to FrameBuffer without waiting for vsync - fastest mode of operation)

  • libpvrPVR2D_FLIPWSEGL.so (for VSync synchronised writes to Framebuffer - slower, but avoids tearing)

  • libpvrPVR2D_BLITWSEGL.so (for direct writes to back-buffer, which later gets written to *FrameBuffer with sync)

Instead the DRM based Full Screen window system are provided:

  • libpvrDRMWSEGL_FRONT.so (for direct writes to DRM FrameBuffer - FRONT mode of operation - directly writes to FrameBuffer without waiting for vsync - fastest mode of operation)

  • libpvrDRMWSEGL.so (for VSync synchronised writes to DRM Framebuffer - slower, but avoids tearing)

The window system is specified by the PVR configuration parameter WindowSystem at the PVR configuration file /etc/powervr.ini. By default, that parameter is set to libpvrDRMWSEGL_FRONT.so for nullDRM Front mode. To configure the PVR SGX to operate in nullDRM FLIP mode, edit the PVR configuration file to set the parameter WindowSystem to libpvrDRMWSEGL.so. The change will take effect when any graphic application is launched next time.

Obsolete Test Programs

The following test programs are no longer applicable and removed from the SDK file system

  • /usr/bin/sgx_blit_test

  • /usr/bin/sgx_flip_test

  • /usr/bin/sgx_render_flip_test

  • /usr/bin/sgx_render_test

3.6.10.2. from Processor SDK 2.0.0 to 2.0.x for AM4

The SGX driver has been enhanced to support DRM/WAYLAND based Multi-Window Display in processor SDK 2.0.1. The System startup and most of the Graphics applications are backward-compatible except with the following changes.

Window System Libraries

The DRM based Full Screen window systems are no longer supported:

  • libpvrDRMWSEGL_FRONT.so (for direct writes to DRM FrameBuffer - FRONT mode of operation - directly writes to FrameBuffer without waiting for vsync - fastest mode of operation)

  • libpvrDRMWSEGL.so (for VSync synchronised writes to DRM Framebuffer - slower, but avoids tearing)

Instead the DRM/WAYLAND based multi-window system are provided:

  • libpvrws_KMS.so

  • libpvrws_WAYLAND.so

The window system will be dynamically loaded by DDK based on the application use case, so that the PVR configuration parameter WindowSystem at the PVR configuration file /etc/powervr.ini is no longer used.

3.6.10.3. from Processor SDK 2.0.1 to 2.0.x for AM3/4/5

The SGX driver has been enhanced to support DRM-based Full Screen(NullDRM) and Multi-Window(Wayland) Display in processor SDK 2.0.2. The System startup and most of the Graphics applications are backward-compatible except with the following changes.

Window System Libraries

The DRM based Full Screen window system is supported:

  • libpvrDRMWSEGL.so (for VSync synchronised writes to DRM Framebuffer - slower, but avoids tearing)

The DRM/WAYLAND based multi-window systems are also provided:

  • libpvrGBMWSEGL.so

  • libpvrws_WAYLAND.so

The window system will be dynamically loaded by DDK based on the application use case, so that the PVR configuration parameter WindowSystem at the PVR configuration file /etc/powervr.ini is no longer required.

3.6.10.4. from Processor SDK 3.1 to 3.x for AM3/4/5

The QT QPA eglfs_kms, which supports multiple screens, has been enabled and used as the default eglfs platform plugin in processor SDK 3.2. To fallback to the standard single-screen eglfs plugin, issue the following instruction at the command line or add the same at the QT environment configuration file qt_env.sh at /etc/profile.d

  • export QT_QPA_EGLFS_INTEGRATION=none

3.6.10.5. from Processor SDK 6.1 to 6.2 for AM3/4/5/6

The SGX driver has been enhanced to replace IMG WSEGL with MESA-EGL which supports the essential EGL 1.5 extensions required by the latest versions of certain graphics applications such as Chromium browser. The System startup and most of the Graphics applications are backward-compatible except with the following changes.

Window System Libraries

With MESA-EGL, all window system modules are embedded in the libEGL.so, both GBM(DRM) full-screen and Wayland window systems are supposrted and dynamically invoked based on the application use case. The following IMG WSEGL libraries are no longer used and provided:

  • libpvrDRMWSEGL.so

  • libpvrGBMWSEGL.so

  • libpvrws_WAYLAND.so

The QT QPA eglfs raw mode is no longer supported and thus should be replaced with eglfs_kms by setting the environment variable at the QT environment configuration file qt_env.sh at /etc/profile.d

  • export QT_QPA_EGLFS_INTEGRATION=eglfs_kms