3.5.2.5.2.4.1. Initializing the PRU from a TI-RTOS Core (Legacy)¶
Note
The PRU Getting Started Labs do not cover TI-RTOS cores controlling the PRU. TI-RTOS SDKs are available for the following processors: AM335x, AM437x, AM57x, AM65x. Some legacy information is provided here for AM335x, AM437x, AM57x customers using PROCESSOR-SDK-RTOS 6.3. HOWEVER, this information has not been tested or validated in several years. These steps are provided as-is. TI cannot answer questions about these steps. Because of the lack of support, These sections are marked as legacy.
TI no longer provides support for TI-RTOS / baremetal SW development for AM335x & AM437x. See this notice for more information.
Launch CCS and open a Workspace
Go to File > New > CCS Project
Select your Target in the first dropdown menu and your Board in the second dropdown menu. Select your Connection in the third dropdown menu.
Select the Cortex A [ARM] tab and give your project a name. Select the GNU (Linaro) compiler.
Under Project templates and examples select SYS/BIOS and then GNU Target Examples and finally Typical.
Select Next >. Under Products and Repositories select <processor> PDK, SYS/BIOS, and XDAIS.
Select the Platform that you’re using from the drop down menu.
Right click the project folder in the Project Explorer. Select Properties from the drop down menu. Select CCS Build > GNU Linker > Libraries
Select Add… in the top bar of the Libraries box. Click Browse. Navigate to: <PDK Directory>/packages/ti/osal/lib/tirtos/<processor>/<ARM core>/release. You should see a file titled ti.osal.a<ARM core>fg. If you don’t see the file, make sure you’re browsing all file types. Select that file.
Note
For AM335x / AM437x / AM572x, ARM core is a8 / a9 / a15, and the file is named ti.osal.aa8fg / ti.osal.aa9fg / ti.osal.aa15fg.
Open your app.cfg file in the project. Copy the code found in pru-software-support-package/Getting_Started_Labs/PRU_FROM_RTOS/app<processor>.cfg into your app.cfg:
There are a few things that should be noted in this configuration file. Jump to the section for the processor that you are using:
AM335x Configuration File
var Mmu = xdc.useModule('ti.sysbios.family.arm.a8.Mmu');
Mmu.enableMMU = true;
/* Force peripheral section to be NON cacheable strongly-ordered memory */
var peripheralAttrs = {
type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
tex: 1,
bufferable : false, // bufferable
cacheable : false, // cacheable
shareable : false, // shareable
noexecute : true, // not executable
};
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x4A300000;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
In the above code: Mmu.enableMMU = true; enables the MMU. Mmu.setFirstLevelDescMeta sets the page of memory starting at peripheralBaseAddr to be non cacheable as described in peripheralAttrs.
var socType = "am335x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A8.
Click here to move on to the next step: Continue.
AM437x Configuration File
var Mmu = xdc.useModule('ti.sysbios.family.arm.a8.Mmu');
Mmu.enableMMU = true;
var peripheralAttrs = {
type : Mmu.FirstLevelDesc_SECTION, // SECTION descriptor
tex: 0,
bufferable : false, // bufferable
cacheable : false, // cacheable
shareable : false, // shareable
noexecute : true, // not executable
};
/* Define the base address of the 1 Meg page the peripheral resides in. */
var peripheralBaseAddr = 0x54400000;
/* Configure the corresponding MMU page descriptor accordingly */
Mmu.setFirstLevelDescMeta(peripheralBaseAddr,
peripheralBaseAddr,
peripheralAttrs);
System.SupportProxy = SysMin;
Mmu.enableMMU = true; enables the MMU. Mmu.setFirstLevelDescMeta sets the page of memory starting at peripheralBaseAddr to be non cacheable as described in peripheralAttrs. There is a quirk here where the A9 uses the A8’s MMU configuration. This is intended.
var socType = "am437x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A9.
Click here to move on to the next step: Continue.
AM572x Configuration File
var socType = "am572x";
/* Load the PRUSS package */
var Pruss = xdc.loadPackage('ti.drv.pruss');
Pruss.Settings.socType = socType;
/* Load the uart package */
var Uart = xdc.loadPackage('ti.drv.uart');
Uart.Settings.socType = socType;
/*use CSL package*/
var Csl = xdc.loadPackage('ti.csl');
Csl.Settings.deviceType = socType;
/* Load the board package */
var Board = xdc.loadPackage('ti.board');
Board.Settings.boardName = "<YOUR_BOARD_HERE>";
The above configuration code loads in the modules neccesary to load the PRU from the A15.
Continue
Board options for <YOUR_BOARD_HERE> can be found in <PDK>/Packages/ti/board/src. Change <YOUR_BOARD_HERE> to be one of those options listed.
You will need the PRU program that you wish to load to be in hex array format as a .h file that is included in your project folder. Instructions on how to do that can be found above in the Compiling to a Hex Array File section.
- You’ll need to create a target configuration file in order to launch your board
and initialize PRU-ICSS. You can do this by navigating to Window > Show Viewv > Target Configurations. Then select New Target Configuration File. Select your Board and Connection type and select save.
Right-click the newly created .ccxml file and select Launch selected configuration
Connect to the Cortex A core, Reset the CPU, and then navigate to Scripts > PRU_ICSS > PRU_ICSS_INIT for AM335x & AM437x, or Scripts > AM572X MULTICORE Initialization > AM572X_MULTICORE_EnableAllCores for AM572x. Select the init script.
Load the PRU program and run it.
- Connect to the PRU (for AM335x), or to a PRU in PRU-ICSS0 (for AM437x &
AM572x). Pause the PRU. Navigate to Window > Show View > Disassembly and select it.
The PRU Program that you compiled into a hex array should now appear in the IRAM of the PRU.