2.3. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>


The following config files are located in the yocto-build/configs/processor-sdk/ directory.
Config File Description Supported machines
processor-sdk-08.06.00-am65xx-config.txt Processor SDK Linux 08_06_00 Release am65xx-evm, am65xx-hs-evm