3. Foundational Components¶
- 3.1. U-Boot
- 3.1.1. User’s Guide
- 3.1.1.1. General Information
- 3.1.1.2. USB Device Firmware Upgrade (DFU)
- 3.1.1.3. Network (Wired or USB Client)
- 3.1.1.3.1. Booting U-Boot from the network
- 3.1.1.3.2. Multiple Interfaces
- 3.1.1.3.3. Network configuration via DHCP
- 3.1.1.3.4. Manual network configuration
- 3.1.1.3.5. Disabling Gigabit Phy Advertising
- 3.1.1.3.6. Booting Linux from the network
- 3.1.1.3.7. Sample Script for AM65 SR1
- 3.1.1.3.8. Sample Script for AM65 SR2
- 3.1.1.4. NAND
- 3.1.1.5. SD, eMMC and USB
- 3.1.1.5.1. Partitioning eMMC from U-Boot
- 3.1.1.5.2. Updating an SD card from a host PC
- 3.1.1.5.3. Updating an SD card or eMMC using DFU
- 3.1.1.5.4. Booting Linux from SD card or eMMC
- 3.1.1.5.5. Booting tiboot3.bin, tispl.bin and u-boot.img from eMMC boot partition (For K3 class of SoCs)
- 3.1.1.5.6. Booting to U-Boot prompt from USB storage
- 3.1.1.5.7. Booting Linux from USB storage
- 3.1.1.5.8. Steps for working around SD card issues
- 3.1.1.6. SPI
- 3.1.1.7. OSPI/QSPI
- 3.1.1.8. NOR
- 3.1.1.9. UART
- 3.1.1.10. SATA
- 3.1.1.11. UFS
- 3.1.1.12. DDR3 ECC
- 3.1.1.13. HyperBus and HyperFlash
- 3.1.1.14. RemoteProc
- 3.1.2. Troubleshooting
- 3.1.1. User’s Guide
- 3.2. Boot Monitor
- 3.3. Kernel
- 3.3.1. Users Guide
- 3.3.1.1. Overview
- 3.3.1.2. Getting the Kernel Source Code
- 3.3.1.3. Preparing to Build
- 3.3.1.4. Configuring the Kernel
- 3.3.1.5. Compiling the Sources
- 3.3.1.6. Creating the kernel fitImage for high security device (using SDK)
- 3.3.1.7. Creating the kernel fitImage for high security device (using Kernel source)
- 3.3.1.8. Installing the Kernel
- 3.3.2. Kernel Release Notes
- 3.3.3. RT Kernel Release Notes
- 3.3.4. Kernel Drivers
- 3.3.4.1. ADC
- 3.3.4.2. Audio
- 3.3.4.3. CAL
- 3.3.4.4. Crypto
- 3.3.4.5. DCAN
- 3.3.4.6. DSS
- 3.3.4.7. GPIO
- 3.3.4.8. I2C
- 3.3.4.9. PRUSS
- 3.3.4.10. PCIe End Point
- 3.3.4.11. PCIe Root Complex
- 3.3.4.12. PWM
- 3.3.4.13. OSPI/QSPI
- 3.3.4.14. SPI
- 3.3.4.15. NAND
- 3.3.4.16. MMC/SD
- 3.3.4.17. UART
- 3.3.4.18. USB DWC3
- 3.3.4.19. Voltage & Thermal Management (VTM)
- 3.3.5. LTP-DDT Validation
- 3.3.6. FAQs
- 3.3.1. Users Guide
- 3.4. Filesystem
- 3.5. Tools
- 3.6. PRU Subsystem
- 3.6.1. Overview of PRU Subsystem
- 3.6.1.1. Getting Started Information
- 3.6.1.2. Hardware Information
- 3.6.1.3. Training Material
- 3.6.1.4. Development Tools
- 3.6.1.5. Software Information
- 3.6.1.6. Examples
- 3.6.1.7. Evaluation Hardware
- 3.6.1.8. TI Designs
- 3.6.1.9. Support
- 3.6.1.10. PRU FAQ
- 3.6.1.10.1. PRU Applications & Support questions
- 3.6.1.10.1.1. What is the difference between the PRU subsystem and ICSS?
- 3.6.1.10.1.2. Is TI providing libraries for the PRU?
- 3.6.1.10.1.3. Can I develop my own industrial protocols on the PRU-ICSS?
- 3.6.1.10.1.4. Can the PRU run a High Level Operating System?
- 3.6.1.10.1.5. My processor has a PRU. Is the PRU supported in the Linux Processor SDK?
- 3.6.1.10.2. PRU Memory Access questions
- 3.6.1.10.3. PRU GPI/O questions
- 3.6.1.10.3.1. What is the maximum speed for toggling PRU GPO pins via PRU software?
- 3.6.1.10.3.2. When does the PRU start capturing from the input pins?
- 3.6.1.10.3.3. Can the module be modified so that the GPI start bit is a zero instead of a one?
- 3.6.1.10.3.4. What happens after 28 bit GPI shifts?
- 3.6.1.10.3.5. Can data be pre-loaded into shadow registers prior to configuring the PRU GPO mode to shift out mode?
- 3.6.1.10.3.6. When does PRU<n>_CLOCKOUT start running?
- 3.6.1.10.3.7. When does the PRU start shifting data in the shadow registers?
- 3.6.1.10.3.8. The shadow registers are loaded by writing to PRU<n>_R30 [0:15]. Does this change the state of the corresponding device-level pins?
- 3.6.1.10.3.9. When the PRU<n>_ENABLE_SHIFT bit is cleared, does the PRU immediately stop shifting PRU<n>_DATAOUT?
- 3.6.1.10.3.10. Does the PRU shift data out LSB or MSB first?
- 3.6.1.10.3.11. What happens to the content stored in R30 when the PRU changes to a different GPO mode?
- 3.6.1.10.4. PRU INTC and System Event questions
- 3.6.1.10.5. PRU Debugger questions
- 3.6.1.10.1. PRU Applications & Support questions
- 3.6.2. Training
- 3.6.2.1. PRU Getting Started Labs
- 3.6.2.2. Lab 1: How to Create a PRU Project
- 3.6.2.3. Lab 2: How to Write PRU Firmware
- 3.6.2.4. Lab 3: How to Compile PRU Firmware
- 3.6.2.5. Lab 4: How to Initialize the PRU
- 3.6.2.6. Lab 5: Basic Debugging of PRU Firmware
- 3.6.2.7. PRU Hands-on Labs
- 3.6.2.7.1. Lab Configuration
- 3.6.2.7.2. LAB 1: Toggle LED with PRU GPO
- 3.6.2.7.3. LAB 2: Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO
- 3.6.2.7.4. LAB 3: Temperature Monitor
- 3.6.2.7.5. LAB 4: Introduction to Linux driver
- 3.6.2.7.6. LAB 5: RPMsg Communication between ARM and PRU
- 3.6.2.7.6.1. Build the PRU Firmware - Using CCSv6
- 3.6.2.7.6.2. Build the PRU Firmware - Using the Provided Makefile
- 3.6.2.7.6.3. Build the RPMsg Client Sample Driver
- 3.6.2.7.6.4. Copy files to the target file system
- 3.6.2.7.6.5. Part 1: Kernel space communication
- 3.6.2.7.6.6. What just happened?
- 3.6.2.7.6.7. Part 2: User Space Communication
- 3.6.2.7.6.8. Part 3: User Space Application
- 3.6.2.7.6.9. What just happened?
- 3.6.2.7.7. LAB 6: Blinking LEDs with RPMsg from Linux User Space
- 3.6.2.7.7.1. Build the PRU Firmware - Using CCSv6
- 3.6.2.7.7.2. Build the PRU Firmware - Using the Provided Makefile
- 3.6.2.7.7.3. Copy files to the target file system
- 3.6.2.7.7.4. Part 1: Linux Command Line LED Toggling
- 3.6.2.7.7.5. What just happened?
- 3.6.2.7.7.6. Part 2: Linux Shell Script LED Toggling
- 3.6.2.7.7.7. What just happened?
- 3.6.2.8. Getting Started with PRU Software Support Package
- 3.6.2.9. RPMsg Quick Start Guide
- 3.6.2.9.1. Introduction
- 3.6.2.9.2. Getting the Linux Processor SDK
- 3.6.2.9.3. Configuring and Building the Linux Kernel with RPMsg Support
- 3.6.2.9.4. Creating a Bootable SD Card with RPMsg Support
- 3.6.2.9.5. Booting the Board and Testing RPMsg
- 3.6.2.9.6. Getting Started with RPMsg Development
- 3.6.2.9.7. Common Issues
- 3.6.3. Linux Drivers
- 3.6.3.1. RemoteProc
- 3.6.3.2. RPMsg
- 3.6.3.3. PRU_ICSSG Ethernet
- 3.6.3.3.1. Introduction
- 3.6.3.3.2. Supported platforms
- 3.6.3.3.3. Features supported
- 3.6.3.3.4. Driver Configuration
- 3.6.3.3.5. Device tree bindings
- 3.6.3.3.6. User guide
- 3.6.3.3.7. Tips
- 3.6.3.3.8. CPSW / PRU Ethernet Selection
- 3.6.3.3.9. Time Senstive Network (TSN) Offload Support
- 3.6.3.3.10. SRAM Requirement
- 3.6.3.4. PRU_ICSSG Two Port Ethernet Switch
- 3.6.3.4.1. Enabling Switch mode
- 3.6.3.4.2. Going back to Dual EMAC mode
- 3.6.3.4.3. Turn On/Off Spanning Tree Protocol (STP)
- 3.6.3.4.4. VLAN configuration
- 3.6.3.4.5. Adding extra VLANs
- 3.6.3.4.6. Forwarding Data Bases (FDBs)
- 3.6.3.4.7. Multicast Data Bases (MDBs)
- 3.6.3.4.8. Multicast flooding
- 3.6.3.4.9. Limitations of switch mode offloading support
- 3.6.3.4.10. SRAM Requirement
- 3.6.3.5. PRU_ICSSG Ethernet SR1.0
- 3.6.4. Firmware Development
- 3.6.5. Hardware
- 3.6.1. Overview of PRU Subsystem
- 3.7. IPC Low Level Driver
- 3.8. Graphics and Display
- 3.8.1. Introduction
- 3.8.2. Software Architecture
- 3.8.3. Graphics Demos
- 3.8.4. Display
- 3.8.5. Wayland/Weston
- 3.8.6. Using the PowerVR Tools
- 3.8.7. SOC Performance monitoring tools on AM5 Devices
- 3.8.8. QT Graphics Framework
- 3.8.9. GTK+ Graphics Framework
- 3.8.10. Migration from prior releases
- 3.8.11. AM3 Beagle Bone Black Board Configuration
- 3.8.12. SGX Debug Info
- 3.9. Virtualization
- 3.10. ARM Trusted Firmware-A
- 3.11. OP-TEE