2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/psdkla
directory of the configs directory.
Config File | Description | Supported machines |
---|---|---|
psdkla-07_00_00_00.txt | Processor SDK Linux Automotive 07_00_00_00 Release | j7-evm |