3.7.2.3.2. Writing Assembly Code
If the PRU project was created in CCS, follow section Writing Assembly Code in CCS.
If the PRU project was created in the Linux terminal, follow section Writing Assembly Code in Linux.
3.7.2.3.2.1. Writing Assembly Code in CCS
Start with the empty PRU project created in Creating a CCS PRU Project.
Add the main ASM file
The PRU project needs an .asm file for the firmware assembly code. Use “Add Files” to copy the main.asm file from <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/.
Select Project->Add Files…
Note
If there are multiple projects open in CCS, make sure to select the correct project in the Project Explorer view before adding the file.
Note
Many steps that involve Project->something can also be done by clicking on the Project Explorer view. For example, “Add Files” can also be accessed by right clicking on the project top-level folder and selecting Add Files. To keep things simple, later steps will only document Project->Add Files…. Either process can be used.
Navigate to <PSSP_PATH>/Getting_Started_Labs/assembly_code folder. Select main.asm. Select open.
Select Copy files and click OK.
Go to the Project Explorer view and double click on main.asm. The text in the file should match the text in <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/main.asm
Add the linker command file
The linker combines all of the PRU code into a single executable object file (i.e., the linker creates the binary file that is loaded into the PRU). The linker command file is used to tell the linker where to place code, how to resolve addresses, and more.
If a linker command file was added to the project folder automatically, delete that linker command file. The automatically generated linker files are not updated like the linker files in the PSSP.
Example: AM335x. Look for AM335x_PRU.cmd and delete it.
Delete the include link that points to automatically generated linker files:
Select Project->Properties.
Select Build->PRU Compiler->Include Options.
In the box marked “Add dir to #include search path”, select ${CCS_BASE_ROOT}/pru/include
Delete the include path by clicking the file icon with a red X.
Save the changes by clicking Apply and close.
Select Project->Add Files….
Navigate to the <PSSP_PATH>/Getting_Started_Labs/linker_cmd folder. Select the linker command file that matches the project’s PRU core. Copy the file into the project.
Example: AM335x PRU: Select AM335x_PRU.cmd
Example: AM62x PRU0: Select AM62x_PRU0.cmd
Example: AM64x TX_PRU0: Select AM64x_TX_PRU0.cmd
Note
AM335x, AM57x: Use the same linker command file for all PRU cores.
AM437x: Use AM437x_PRU_SS0.cmd for PRU cores in PRU-ICSS0. Use AM437x_PRU_SS1.cmd for PRU cores in PRU-ICSS1.
AM62x: Use PRU0.cmd for PRU0, use PRU1.cmd for PRU1.
AM64x, AM65x: Use PRU0.cmd for PRU0 in any PRU_ICSSG. Use PRU1.cmd for PRU1 in any PRU_ICSSG. Similarly, use RTU0.cmd for any RTU0, RTU1.cmd for any RTU1, TX_PRU0.cmd for any TX_PRU0, and TX_PRU1.cmd for any TX_PRU1.
Configure the PRU INTC (optional)
The PRU Interrupt Controller (INTC) can be configured by the core that loads the PRU, or by the PRU itself.
The PRU Getting Started Labs do not configure the INTC. However, these steps are provided as a resource for customers who will configure the INTC in their projects.
Does the PRU project use interrupts?
Yes –> Continue reading.
No –> INTC configuration is not needed. Jump to section Add the resource table (optional)
Will the PRU project be loaded by a core running an OS from the MCU+ SDK?
Yes –>
Should the INTC be configured by the MCU+ core?
Yes –> Reference the documentation in the MCU+ SDK docs, section “SOC Peripheral Drivers” > “PRUICSS”. Continue the PRU Getting Started Labs by jumping to Add the resource table (optional).
No –> Continue reading.
Will the PRU project be loaded by a core running Linux?
Yes –> At this point in time, the Linux RemoteProc driver only accepts INTC configurations from PRU projects written in C code. PRU projects written in assembly code will need to configure the PRU INTC from the PRU instead of from the Linux driver. Continue reading.
No –> Continue reading.
If you got to this step, then the project uses interrupts, and the PRU INTC will be configured by the PRU firmware instead of by another core. Be very careful if deciding to configure the PRU INTC from two different cores! There are no settings to prevent one core from overwriting the other core’s INTC settings.
For an example of configuring the PRU INTC from PRU firmware, reference the PRU Hands-on Labs LAB 2: Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO, section “Build the PRU Firmware”. Note that different processors will have different names for the INTC registers.
Add the resource table (optional)
Will the PRU project be loaded by a core running Linux kernel 5.4 or earlier?
Yes –> Jump to section Add the resource table with Linux 5.4 or earlier
No –> Resource tables are not used. Continue reading.
Will the PRU project be loaded by a core running Linux kernel 5.10 or later?
Yes –> Ensure the PSSP version is v6.0.0 or later. No additional steps are needed. Jump to section Write the PRU firmware.
No –> Continue reading.
If you got to this step, then the PRU project will not be loaded by a core running Linux. The project does not need a resource table.
Check which version of PSSP is used:
v6.0.0 or later: No additional steps are needed. Jump to section Write the PRU firmware.
v5.9.0 or earlier: An empty resource table is included by default in these versions of the PSSP.
Go to the main.asm file
Delete the resource table lines:
; Resource table needed for remoteproc Linux driver .global ||pru_remoteproc_ResourceTable|| .sect ".resource_table:retain", RW .retain .align 1 .elfsym ||pru_remoteproc_ResourceTable||,SYM_SIZE(20) ||pru_remoteproc_ResourceTable||: .bits 1,32 ; pru_remoteproc_ResourceTable.base.ver @ 0 .bits 0,32 ; pru_remoteproc_ResourceTable.base.num @ 32 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[0] @ 64 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[1] @ 96 .bits 0,32 ; pru_remoteproc_ResourceTable.offset[0] @ 128Jump to section Write the PRU firmware.
Add the resource table with Linux 5.4 or earlier
A resource table is required if the PRU project is loaded by a Linux core running Linux kernel 5.4 or earlier.
Note
PSSP projects for Linux 5.4 or earlier have different resource tables than PSSP projects for Linux 5.10 or later. Check the tag on your PSSP to make sure you are using PSSP v5.9.0 or earlier.
Does the PRU project use RPMsg?
Yes –> TI only supports PRU RPMsg with C code. Steps for building a C code project (including how to add RPMsg Resource Tables) are at Writing C Code.
No –> Define an empty resource table.
The getting started labs include empty resource tables.
Check that the main.asm file includes an empty resource table:
; Resource table needed for remoteproc Linux driver .global ||pru_remoteproc_ResourceTable|| .sect ".resource_table:retain", RW .retain .align 1 .elfsym ||pru_remoteproc_ResourceTable||,SYM_SIZE(20) ||pru_remoteproc_ResourceTable||: .bits 1,32 ; pru_remoteproc_ResourceTable.base.ver @ 0 .bits 0,32 ; pru_remoteproc_ResourceTable.base.num @ 32 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[0] @ 64 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[1] @ 96 .bits 0,32 ; pru_remoteproc_ResourceTable.offset[0] @ 128Check that the linker command file includes a section for the resource table.
Example: AM335x PRU0
.resource_table > PRU_DMEM_0_1, PAGE 1
Example: AM65x PRU0
/* Ensure resource_table section is aligned on 8-byte address for ARMv8 (64-bit) kernel */ .resource_table : ALIGN (8) > PRU0_DMEM_0, PAGE 1
The resource table includes rsc_types.h. Add the appropriate include path:
Select Project->Properties.
Select Build->PRU Compiler->Include Options.
In the box marked “Add dir to #include search path”, click the file icon with a green +.
The empty resource table that is used in the PRU Getting Started Guide does not need to be modified.
Jump to section Write the PRU firmware
Write the PRU firmware
Look for the TODO comments in the main.asm code for guidance on completing the example code. The complete solution for the main.asm code can be found in <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/solution.
Ready to compile the PRU firmware? Go to Lab 3: How to Compile PRU Firmware.
3.7.2.3.2.2. Writing Assembly Code in Linux
Start with the basic PRU project created in Creating a Linux PRU Project. Start in the same directory as in Lab 1: <PSSP_PATH>/examples/<processor>
Add the main ASM file
The PRU project needs an .asm file for the firmware assembly code.
The basic PRU project should already have a main.c file. Delete the existing main.c file.
Example: AM335x with PRU0:
$ cd PRU_Add $ ls $ rm main.c
Example: AM64x with RTU1:
$ cd RTU_Add $ ls $ rm main.c
Copy the main.asm file from <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/ to the current directory.
$ cp ../../../labs/Getting_Started_Labs/assembly_code/main.asm .
The main.asm file in the current directory should match the main.asm file in labs/Getting_Started_Labs/assembly_code/.
Example: AM335x with PRU0, based on PRU_Halt:
$ diff ../../../labs/Getting_Started_Labs/assembly_code/main.asm main.asm # there should be no output
Add the Makefile
The PRU project needs a Makefile in order to build the firmware through the Linux terminal.
The basic PRU project should already have a Makefile. Delete the existing Makefile.
Example: AM335x with PRU0:
$ cd PRU_Add $ ls $ rm Makefile
Example: AM64x with RTU1:
$ cd RTU_Add $ ls $ rm Makefile
Copy the Makefile file from <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/solution/<processor>/ to the current directory.
Example: AM335x with PRU0:
$ cp ../../../labs/Getting_Started_Labs/assembly_code/solution/am335x/Makefile .
Example: AM64x with RTU1:
$ cp ../../../labs/Getting_Started_Labs/assembly_code/solution/am64x/Makefile .
The Makefile in the current directory should match the Makefile in labs/Getting_Started_Labs/assembly_code/solution/<processor>/.
Example: AM335x with PRU0, based on PRU_Halt:
$ diff ../../../labs/Getting_Started_Labs/assembly_code/solution/am335x/Makefile Makefile # there should be no output $ diff ../PRU_Halt/Makefile Makefile # Makefile in PRU_Halt should be different
The Makefile may need modifications depending on which PRU core the project uses. See more information in Add the linker command file.
Add the linker command file
The linker combines all of the PRU code into a single executable object file (i.e., the linker creates the binary file that is loaded into the PRU). The linker command file is used to tell the linker where to place code, how to resolve addresses, and more.
The basic PRU project should already have a linker command file. Make sure that the linker command file matches the project’s PRU core.
Example: AM335x PRU: Select AM335x_PRU.cmd
Example: AM62x PRU0: Select AM62x_PRU0.cmd
Example: AM64x TX_PRU0: Select AM64x_TX_PRU0.cmd
Note
AM335x, AM57x: Use the same linker command file for all PRU cores.
AM437x: Use AM437x_PRU_SS0.cmd for PRU cores in PRU-ICSS0. Use AM437x_PRU_SS1.cmd for PRU cores in PRU-ICSS1.
AM62x: Use PRU0.cmd for PRU0, use PRU1.cmd for PRU1.
AM64x, AM65x: Use PRU0.cmd for PRU0 in any PRU_ICSSG. Use PRU1.cmd for PRU1 in any PRU_ICSSG. Similarly, use RTU0.cmd for any RTU0, RTU1.cmd for any RTU1, TX_PRU0.cmd for any TX_PRU0, and TX_PRU1.cmd for any TX_PRU1.
Make sure that the project Makefile LINKER_COMMAND_FILE matches the linker command file used:
Open the Makefile in a text editor.
If LINKER_COMMAND_FILE does not match the project linker command file, update it.
Example: AM335x using AM335x_PRU.cmd:
LINKER_COMMAND_FILE=./AM335x_PRU.cmd
Example: AM64x TX_PRU0 using AM64x_TX_PRU0.cmd:
LINKER_COMMAND_FILE=./AM64x_TX_PRU0.cmd
If the Makefile required changes, save the changes. Close the Makefile.
Configure the PRU INTC (optional)
The PRU Interrupt Controller (INTC) can be configured by the core that loads the PRU, or by the PRU itself.
The PRU Getting Started Labs do not configure the INTC. However, these steps are provided as a resource for customers who will configure the INTC in their projects.
Does the PRU project use interrupts?
Yes –> Continue reading.
No –> INTC configuration is not needed. Jump to section Add the resource table (optional)
Will the PRU project be loaded by a core running an OS from the MCU+ SDK?
Yes –>
Should the INTC be configured by the MCU+ core?
Yes –> Reference the documentation in the MCU+ SDK docs, section “SOC Peripheral Drivers” > “PRUICSS”. Continue the PRU Getting Started Labs by jumping to Add the resource table (optional).
No –> Continue reading.
Will the PRU project be loaded by a core running Linux?
Yes –> At this point in time, the Linux RemoteProc driver only accepts INTC configurations from PRU projects written in C code. PRU projects written in assembly code will need to configure the PRU INTC from the PRU instead of from the Linux driver. Continue reading.
No –> Continue reading.
If you got to this step, then the project uses interrupts, and the PRU INTC will be configured by the PRU firmware instead of by another core. Be very careful if deciding to configure the PRU INTC from two different cores! There are no settings to prevent one core from overwriting the other core’s INTC settings.
For an example of configuring the PRU INTC from PRU firmware, reference the PRU Hands-on Labs LAB 2: Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO, section “Build the PRU Firmware”. Note that different processors will have different names for the INTC registers.
Add the resource table (optional)
Will the PRU project be loaded by a core running Linux kernel 5.4 or earlier?
Yes –> Jump to section Add the resource table with Linux 5.4 or earlier
No –> Resource tables are not used. Continue reading.
Will the PRU project be loaded by a core running Linux kernel 5.10 or later?
Yes –> Ensure the PSSP version is v6.0.0 or later. No additional steps are needed. Jump to section Write the PRU firmware.
No –> Continue reading.
If you got to this step, then the PRU project will not be loaded by a core running Linux. The project does not need a resource table.
Check which version of PSSP is used:
v6.0.0 or later: No additional steps are needed. Jump to section Write the PRU firmware.
v5.9.0 or earlier: An empty resource table is included by default in these versions of the PSSP.
Go to the main.asm file
Delete the resource table lines:
; Resource table needed for remoteproc Linux driver .global ||pru_remoteproc_ResourceTable|| .sect ".resource_table:retain", RW .retain .align 1 .elfsym ||pru_remoteproc_ResourceTable||,SYM_SIZE(20) ||pru_remoteproc_ResourceTable||: .bits 1,32 ; pru_remoteproc_ResourceTable.base.ver @ 0 .bits 0,32 ; pru_remoteproc_ResourceTable.base.num @ 32 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[0] @ 64 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[1] @ 96 .bits 0,32 ; pru_remoteproc_ResourceTable.offset[0] @ 128Jump to section Write the PRU firmware.
Add the resource table with Linux 5.4 or earlier
A resource table is required if the PRU project is loaded by a Linux core running Linux kernel 5.4 or earlier.
Note
PSSP projects for Linux 5.4 or earlier have different resource tables than PSSP projects for Linux 5.10 or later. Check the tag on your PSSP to make sure you are using PSSP v5.9.0 or earlier.
Does the PRU project use RPMsg?
Yes –> TI only supports PRU RPMsg with C code. Steps for building a C code project (including how to add RPMsg Resource Tables) are at Writing C Code.
No –> Define an empty resource table.
The getting started labs include empty resource tables.
Check that the main.asm file includes an empty resource table:
; Resource table needed for remoteproc Linux driver .global ||pru_remoteproc_ResourceTable|| .sect ".resource_table:retain", RW .retain .align 1 .elfsym ||pru_remoteproc_ResourceTable||,SYM_SIZE(20) ||pru_remoteproc_ResourceTable||: .bits 1,32 ; pru_remoteproc_ResourceTable.base.ver @ 0 .bits 0,32 ; pru_remoteproc_ResourceTable.base.num @ 32 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[0] @ 64 .bits 0,32 ; pru_remoteproc_ResourceTable.base.reserved[1] @ 96 .bits 0,32 ; pru_remoteproc_ResourceTable.offset[0] @ 128Check that the linker command file includes a section for the resource table.
Example: AM335x PRU0
.resource_table > PRU_DMEM_0_1, PAGE 1
Example: AM65x PRU0
/* Ensure resource_table section is aligned on 8-byte address for ARMv8 (64-bit) kernel */ .resource_table : ALIGN (8) > PRU0_DMEM_0, PAGE 1
The resource table includes rsc_types.h. Add the include path for rsc_types.h so that the compiler can find the header file.
Open the Makefile in a text editor.
Ensure that the project Makefile INCLUDE points to the directory with rsc_types.h.
Example: AM335x:
INCLUDE=--include_path=../../../include --include_path=../../../include/am335x
If the Makefile required changes, save the changes. Close the Makefile.
The empty resource table that is used in the PRU Getting Started Guide does not need to be modified.
Jump to section Write the PRU firmware
Write the PRU firmware
Look for the TODO comments in the main.asm code for guidance on completing the example code. The complete solution for the main.asm code can be found in <PSSP_PATH>/labs/Getting_Started_Labs/assembly_code/solution.
Ready to compile the PRU firmware? Go to Lab 3: How to Compile PRU Firmware.