4.1.6. How to enable DT overlays in linux
The Processor SDK Linux AM62x supports various features in the form of device-tree overlays appended on top of the board device-tree source files. These features can only be used after enabling their respective overlay blobs (*.dtbo files). Below are the steps to compile the DT overlay sources, install them on the SD Card, and enable them at the u-boot stage. The SD Card wic image (tisdk-default-image
) comes with the overlay blobs pre-loaded on the SD Card, and steps 3 through 5 can be skipped, if there are no custom changes required on the DT overlay sources.
Important
These steps are only applicable for GP and HS-FS devices. For HS-SE devices, follow steps 1 through 4, and post that, kindly refer to: Creating the kernel fitImage for high security device / GP devices, to package the requrired DTBOs in the fitImage.
4.1.6.1. Steps to enable DT overlays:
Flash the SD card with the
tisdk-default-image
available at AM62x-SDK-Download-page.If the SD card got auto-ejected after flashing, re-plug it.
On the host machine, build dtbs in the PSDK linux source tree, without any changes. Refer to Users Guide for more details.
$ make CROSS_COMPILE=aarch64-none-linux-gnu- ARCH=arm64 clean $ make CROSS_COMPILE=aarch64-none-linux-gnu- ARCH=arm64 dtbs
If the build is successful, the required DT overlay files shall be found as below:
$ ls arch/arm64/boot/dts/ti/k3-<required-soc>-*.dtbo
Copy this DT overlay file to the
boot/dtb/ti
directory of the root partition of the SD card.$ sudo cp arch/arm64/boot/dts/ti/k3-<overlay>.dtbo <path-to-sd-root>/boot/dtb/ti/
Update the
uEnv.txt
file under the boot partition of the SD card, to let u-boot recognize the overlay. Depending on the use-case, multiple DT overlays can also be added, using “space” as the delimiter.name_overlays=ti/k3-<overlay-1>.dtbo ti/k3-<overlay-2>.dtbo ti/k3-<overlay-3>.dtbo
Unmount and eject the SD card. Plug it back in the AM62x board and turn the board on.