4.1.16. How to Setup and Debug using Lauterbach
Introduction Lauterbach
This guide discusses how to use TRACE32 and Lauterbach for Debugging.
Lauterbach provides integrated debug environments for embedded designs.
- The tool chain in Lauterbach includes:
Debugger
Real-time trace for program/data flow
Logic analyzer
These capabilities are implemented by dedicated hardware components.
TRACE32
The TRACE32 toolset supports a large number of microprocessors, real-time operating systems, integrations, and eco-systems.
Connecting Lauterbach to Board
For connecting Lauterbach to the board, following things are required:
7-9 V power supply
Debug Cable (JTAG)
20 pin JTAG Header
USB Cable
Connect the USB Cable to the host machine. The Debug Cable (JTAG) will be connected to the board via the 20 pin JTAG Header.
Following image shows the setup of AM62x with Lauterbach
For more information regarding the setup please refer this.
Downloading and Installing TRACE32
You can download and install the latest version of TRACE32 from here.
Debugging with TRACE32
To open the TRACE32 software after installing, search for Trace 32 (ARM V8 USB) Launcher Application on your system and open it.
A window will popup as shown below
Now as per your debugging requirements, select the desired cmm files. For this, from menu bar go to File –> Open Script. Select the desired cmm file and select Do. This will set target type, open some windows, assemble some code in SRAM, execute that code. You should be able to trace this code in the list window.
CMM Files
To download cmm files for AM62x go to AM62 cmm files and search am62xx.
Tracing a Simple demo script for Cortex-A53
Go to Lauterbach website and download the hardware-arm-am62xx-am62x-skevm-am62x-ca53_20221026000946_all_files.zip and hardware-arm-am62xx-am62x-skevm-scripts_20221026000946_all_files.zip and place them in a single directory.
Extract both the directories and rename the hardware-arm-am62xx-am62x-skevm-scripts_20221026000946_all_files to scripts because the cmm files expect it.
Open the Trace 32 (ARM V8 USB) Launcher Application on your system. From menu bar go to File –> Open Script. Select any cmm file from hardware-arm-am62xx-am62x-skevm-am62x-ca53_20221026000946_all_files directory (Eg: am62x_sieve_sram.cmm).
The am62x_sieve_sram.cmm file loads the sieve demo application into PSRAM and sets up a demo debug scenario.
Click on Do in the Menu bar to start the execution. The B::List:auto command inside the am62x_sieve_sram.cmm file will open the sieve.c file for debugging.
Inside the B::List:auto window, there are local buttons for all basic debug commands. We can click on Step to Single stepping and Over to Step over call.
You can stop the execution at any point by clicking on Break in B::List:auto window.
A sample output after breaking at a particular point is shown below.
For more information on debugging with TRACE32 refer this.