4.1. Developer NotesΒΆ
- 4.1.1. Connect to an EVM via Telnet
- 4.1.2. How to Setup a Samba Server
- 4.1.3. Moving Files to the Target System
- 4.1.4. SDK File System Optimization/Customization
- 4.1.5. How to Suspend to RAM (Deep Sleep) on AM62x
- 4.1.6. How to enable MCAN in Linux
- 4.1.7. How to enable DT overlays in linux
- 4.1.8. How to playback audio over HDMI
- 4.1.9. How to enable Microtips LVDS Panel on AM62 SK EVM
- 4.1.10. How to Use K3Conf Tool
- 4.1.11. How to check some device tree information from user-space of Linux?
- 4.1.12. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM62x?
- 4.1.13. K3 Resource Partitioning Tool
- 4.1.14. How to Setup and Debug using Lauterbach
- 4.1.15. Enabling and Parsing SYSFW Trace
- 4.1.16. Minimal Platform Development