3.1.2.2. Debugging SPL in OpenOCD¶
The following guide demonstrates how to connect a board to OpenOCD and load the SPL symbols for debugging with a K3 generation device. For the guide below, users are expected to generate custom binaries, boot their board from an SD card and work with OpenOCD in a Linux environment. This guide uses the AM625-SK for device specific examples but can be extended to any K3 generation device. Use the U-Boot documentation below to begin using OpenOCD with a K3 generation device.