2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the user experience, Processor SDK Linux AM62L installer provides everything needed as discussed below to create the embedded system from “scratch” :

  • Platform/board-support software and configuration files for Linux

  • U-Boot and Kernel sources and configuration files

  • An ARM cross-compiling toolchain as well as other host binaries and components

  • A Yocto/OE compliant filesystem and sources for example applications

  • A variety of scripts and Makefiles to automate certain tasks

  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets

  • Reference Examples, benchmarks

This release supports High Security - Field Securable (HS-FS) devices.

2.1.2. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

2.1.3. Release 11.01.16.13

Released on Oct 2025

2.1.3.1. What’s new

Processor SDK Linux AM62LX Release has following new features:

Component version:

  • Kernel (Including RT) 6.12.43

  • U-Boot 2025.01

  • Toolchain GCC 13.4

  • ATF 2.12+

  • TIFS Firmware v11.01.12 (Click on the link for more information)

  • Yocto scarthgap 5.0

  • Armbian-based Debian 13 (Trixie)

  • Buildroot 2024.11.1

2.1.4. Build Information

2.1.4.1. Arago (Yocto/OE)

Component

Branch Info

Tag Info

Config Info

U-Boot

ti-u-boot-2025.01

11.01.16

Build Config

TF-A

ti-master

v2.12+

OPTEE

master

4.7.0+

k3-am62lx

Linux Firmware

ti-linux-firmware

11.01.16

Linux Kernel

ti-linux-6.12.y

11.01.16

non-RT , RT

meta-ti

scarthgap

11.01.16

am62lxx-evm

meta-arago

scarthgap

11.01.16

meta-tisdk

scarthgap

11.01.16.13

2.1.4.2. Debian (Armbian)

Component

Branch Info

Tag Info

Config Info

U-Boot

ti-u-boot-2025.01

11.01.16

Build

ATF

ti-master

v2.12+

Build

OPTEE

master

4.7.0+

Build

Linux Firmware

ti-linux-firmware

11.01.16

Git Clone

Linux Kernel

ti-linux-6.12.y

11.01.16

non-RT, RT

Armbian Build

2025.10-release

11.01.16.13

Build, Board

2.1.5. Issues Tracker

Note

  • Release Specific Issues including details will be published through Software Incident Report (SIR) portal

  • Further Information can be found at SIR Portal

2.1.5.1. Issues Resolved

Record ID

Title

EXT_SITMPUSW-165

inapplicable wl18xx message in Linux boot log

EXT_EP-12816

SDK Docs: Broken URL in How To Guides > EVM Setup

EXT_EP-12780

AM62L Dynamic IP address cannot be obtained when eth interface brought down with command

EXT_EP-12674

AM62L: Enabling wkup uart causes Linux console (main_uart0) garbled

EXT_EP-12340

Suspend-to-RAM failure: tps65219: device creates a circular dependency and device fails to enter suspend

EXT_EP-12977

AM62L: PM: add missing PDs (devices) in the scmi wrapper

EXT_EP-12973

AM62L: Suspend-Resume (RTC+DDR): MMC fails

EXT_EP-12976

DSI fails to reconnect after suspend/resume

EXT_EP-12975

DSS clock warnings appear during suspend/resume when HDMI is connected

EXT_EP-12784

AM62L: LPM: 2nd core randomly fails to come online during suspend/resume

EXT_EP-12778

AM62L: PG1.1: PM: during clock init the pm driver is touching wkup PLL

EXT_EP-12974

AM62L: Heartbeat LED stops blinking on resume from RTC+DDR

EXT_EP-12978

AM62L: Suspend-Resume (RTC+DDR): spi-nor resume() fails

2.1.5.2. Issues Open

Record ID

Title

EXT_EP-12970

AM6x - Sitara Socs MCASP and BCDMA issue.

EXT_EP-12980

AM62L: Random kernel crash observed on stress test

EXT_EP-12979

AM62L: Suspend-Resume (RTC+DDR): davinci_mdio timed out waiting for user access