4.11. Android Secure Build Application Note

This page describes how to setup secure Android build.

The process is an example, feel free to adapt following your needs.

Warning

This process is only supported with Android user images

4.11.1. Fetching Bootloader, Kernel, and Android

  • Bootloaders:

    $ export YOUR_PATH=~/src/
    $ mkdir ${YOUR_PATH}/ti-bootloader-aosp/ && cd $_
    $ repo init -u https://git.ti.com/git/android/manifest.git -b android16-release -m releases/RLS_11_00_Bootloader.xml
    $ repo sync
    
  • Kernel:

    $ mkdir ${YOUR_PATH}/ti-kernel-aosp/ && cd $_
    $ repo init -u https://git.ti.com/git/android/manifest.git -b android16-release -m releases/RLS_11_00_Kernel.xml
    $ repo sync
    
  • Android:

    $ export YOUR_PATH=~/src/
    $ mkdir ${YOUR_PATH}/ti-aosp-16 && cd $_
    $ repo init -u https://git.ti.com/git/android/manifest.git -b android16-release -m releases/RLS_11_00.xml
    $ repo sync
    

4.11.2. Build Secure Bootloaders

  • Generate TA cryptographic keys:

    $ cd ${YOUR_PATH}/ti-bootloader-aosp/build
    $ ./secure.sh generate_ta_keys
    $ ls -1 .keys/
    ta.pem
    ta_pub.pem
    
  • Generate AVB public/private keys:

    $ cd ${YOUR_PATH}/ti-bootloader-aosp/build
    $ ./secure.sh generate_avb_keys
    $ ls -1 .keys/
    avb.key
    avb_pub.key
    

That will generate avb.key and avb_pub.key under build/.keys.

Note

Dependency on avbtool:

The ./secure.sh generate_avb_keys command has a dependency on the avbtool binary. The tool is present in the kernel repository at prebuilts/kernel-build-tools/linux-x86/bin/avbtool. If the command fails with the message: avbtool: command not found, update your PATH environment variable to include the avbtool path:

$ export PATH=$PATH:${YOUR_PATH}/ti-kernel-aosp/prebuilts/kernel-build-tools/linux-x86/bin

The bootloaders scripts will detect that avb_pub.key is present and will include it into U-Boot.

The user can also specify the absolute path of the avb_pub key in yaml config (build/config/boards/am67a-evm.yaml):

secure:
  avb_pub_key: ${YOUR_PATH}/ti/avb_pub.key
Table 4.2 Security Keys

Key

Description

avb.key

(Optional) Private key used by Android to sign images

avb_pub.key

(Optional) Public key used by U-Boot to verify Android images

ta.pem

(Optional) Private key used to sign Trusted Application (OP-TEE)

ta_pub.pem

(Optional) Public key used to sign Trusted Application (OP-TEE)

Build and copy secure images to Android:

$ ./build/release_android.sh --aosp=~${YOUR_PATH}/ti-aosp-16 --mode=factory

Warning

By default on factory mode, OP-TEE is built with this flag:

  • CFG_RPMB_WRITE_KEY:

    This flag configure the RPMB if this one is not initialized yet.

    This operation is performed one time only, once the RPMB is initialized with the key we cannot override it anymore.

Note

RPMB corruptions:

If we do several flashes with different builds, we may be faced with RPMB corruptions. Indeed some metadata are stored in the RPMB and by default if there is a mismatch OP-TEE fails to load Trusted Applications. Thus the OP-TEE keymaster service fails and the device doesn’t boot. To avoid this situation we can add the flag CFG_REE_FS_ALLOW_RESET=y in build_optee.sh:

Allow secure storage in the REE FS to be entirely deleted without causing anti-rollback errors. This is used to reset the secure storage to a clean, empty state.

Testing Case:

If you want to test and be sure to reuse RPMB partition you can set CFG_RPMB_TESTKEY=y in build_optee.sh:

OP-TEE can either embed a built-in RPMB key or derive it from platform specific secrets. The former case might be useful during development while the later is recommended for production devices.

Copy avb.key in Android:

$ cd ${YOUR_PATH}/ti-bootloader-aosp/build
$ cp .keys/avb.key "${YOUR_PATH}/ti-aosp-16/device/ti/am62x/"

Replace the following configs in device/ti/am62x/BoardConfigCommon.mk:

BOARD_AVB_ALGORITHM := SHA256_RSA4096
BOARD_AVB_KEY_PATH := device/ti/am62x/avb.key
BOARD_AVB_BOOT_KEY_PATH := device/ti/am62x/avb.key
BOARD_AVB_INIT_BOOT_KEY_PATH := device/ti/am62x/avb.key
BOARD_AVB_VBMETA_VENDOR_DLKM_KEY_PATH := device/ti/am62x/avb.key
BOARD_AVB_VBMETA_SYSTEM_DLKM_KEY_PATH := device/ti/am62x/avb.key

Check images generated in Android:

$ cd ~${YOUR_PATH}/ti-aosp-16
$ git status

4.11.3. Build Kernel

Before building Kernel we need to modify it to support RPMB features.

Download patch : RPMB_enabling.patch and put it ${YOUR_PATH}/ti-kernel-aosp/common folder.

Update symbol list and build kernel:

$ cd ${YOUR_PATH}/ti-kernel-aosp/common
$ git am RPMB_enabling.patch
$ cd ${YOUR_PATH}/ti-kernel-aosp/
$ export DIST_DIR=${YOUR_PATH}/ti-aosp-16/device/ti/am62x-kernel/kernel/6.12
$ ./update_symbol_list.sh -d ti -b private/devices/ti/am6x
$ ./tools/bazel run --config=ti //private/devices/ti/am6x:ti_dist -- --destdir=$DIST_DIR

4.11.4. Build Android

$ cd ${YOUR_PATH}/ti-aosp-16
$ source build/envsetup.sh
$ lunch am67a-bp2a-user

$ export FACTORY_BUILD=true
$ m -j$(nproc)                # OR nice -n19 build/soong/soong_ui.bash --make-mode -j$(nproc)

4.11.5. Flash Android

To reflash on a device which already has Android installed, run:

Reboot to U-Boot

$ adb reboot bootloader

Flash using the script: in a different terminal,

change directory to out/target/product/am67a and run the flashall.sh script:

# for AM67A EVM
$ sudo ./flashall.sh --board am67a-evm

Warning

Device Locking and Unlock Capability

After flashing with secure build, the device will be locked and fastboot flashing unlock commands will be disabled by default.

To enable unlock capability, you have several options:

Option 1: Enable at compile time

Set the U-Boot environment variable before compilation:

fastboot.unlock_ability=1

Option 2: Enable at runtime

Set the U-Boot environment variable in the console (note that saveenv is disabled in factory mode, so these settings will be lost at each reboot):

=> setenv fastboot.unlock_ability 1

Unlock Process

When running fastboot flashing unlock or fastboot flashing unlock_critical, the system will prompt for confirmation in the console. To bypass this confirmation prompt, you can set (these settings will also be lost at each reboot):

=> setenv fastboot.unlock_confirm 1
=> setenv fastboot.unlock_critical_confirm 1