4.3. Android Bootloader on SD Card
This application note contains steps to flash initial bootloaders from SD Card instead of using snagboot.
4.3.1. SD Card Creation
In order to flash the AM62x board’s eMMC the fist time, a SD card containing the required bootloaders will have to be used to boot into U-Boot and use fastboot.
Warning
Make sure to use the same bootloaders as the release you are flashing.
The latest release is 10.00.00.
4.3.1.1. Identify the SD Card
To start, identify your SD card with:
$ sudo fdisk -l
In this example, the SD card will be: /dev/mmcblk0.
4.3.1.2. Prepare the SD Card
The preparation of the SD Card is done via the flashall.sh script.
Make sure to identify the board model, and the SD card path.
Then, run:
# If you are using binaries built locally
$ cd out/target/product/am62x
(OR)
# If you are using pre-built binaries from SDK download page
$ cd AM62x_10.00.00_emmc
# for AM62x SK EVM (GP)
$ sudo ./flashall.sh --board am62x-sk --bootloader --sdcard /dev/mmcblk0
# for AM62x SK EVM (HS-FS)
$ sudo ./flashall.sh --board am62x-sk --hsfs --bootloader --sdcard /dev/mmcblk0
# for AM62x LP SK EVM (GP)
$ sudo ./flashall.sh --board am62x-lp-sk --bootloader --sdcard /dev/mmcblk0
# for AM62x LP SK EVM (HS-FS)
$ sudo ./flashall.sh --board am62x-lp-sk --bootloader --hsfs --sdcard /dev/mmcblk0
4.3.2. eMMC flashing
4.3.2.1. Flashing instructions
Once the build is complete, follow the steps below to flash the images to eMMC. Use the SD card created in previous step to get started.
Procedure is same whether the pre-built images from SDK download page is used or the images are built from source.
Change the Boot Mode DIP switches to SD card boot mode:
Switch Label
SW2: 12345678
SW3: 12345678
SD
01000000
11000010
Insert the SD card into the AM62x SK EVM.
Ensure the device is plugged in with USB host and debug UART/serial debug
Open a terminal debugger to view console output from the device:
$ sudo picocom -b 115200 -r -l /dev/ttyUSB0
Boot the board with SD card.
Stop at U-Boot console (interrupt the auto-boot countdown) and do below commands to setup Android partition table:
=> env default -f -a; saveenv
Then, continue following the default flashing instructions from step 5.