4.10. Beagle Play
The Beagle Play is very similar to the AM62x SK EVM. Therefore, the AM62x SDK can be installed on the Beagle Play as well.
This application note contains steps to install the AM62x SDK on the Beagle Play board.
4.10.1. Initial Flashing procedure
Flashing Android the first time requires booting from DFU.
First, make sure to install snagboot following
the official instructions
Then, the following steps are required:
Make sure the board is powered down. No SD card is present.
Plug in the serial connector to view debug logs. In a terminal, open:
$ sudo picocom -b 115200 -r -l /dev/ttyUSB0
Hold the
USRbutton. While holding the button, insertUSBcable from PC to board.Wait for DFU mode to come up. DFU mode is a backup boot mode for the Beagle Play. To check if the device enumerates via DFU, run
dfu-util -l:$ dfu-util -l Found DFU: [0451:6165] ver=0200, devnum=99, cfg=1, intf=0, path="1-1", alt=1, name="SocId", serial="01.00.00.00" Found DFU: [0451:6165] ver=0200, devnum=99, cfg=1, intf=0, path="1-1", alt=0, name="bootloader", serial="01.00.00.00"
Run
snagrecoverto load the bootloaders:# run from out/target/product/am62x $ snagrecover -s am625 -f ./am625-beagleplay.yaml
The debug console will show:
Press SPACE to abort autoboot in 2 seconds =>
In the debug console, hit the SPACE key to halt in U-Boot
Make sure the default U-Boot environment is configured:
=> env default -a -f => saveenv
Start fastboot:
=> fastboot usb 0
Run the flashing script:
# run from out/target/product/am62x $ sudo ./flashall.sh --board am625-beagleplay
Unplug USB power and replug to switch to normal boot mode.