4.9. Sample Maps Application for Car Variant
As part of 10.0 SDK release, Android SDK now includes a pre-built maps application created by Snapp Automotive. The app is developed on top of the OSMDroid library and the source code of the app is available at https://github.com/snappautomotive/SnappMaps.
Note
For more information on this application, please visit the Snapp Automotive website at https://www.snappautomotive.io/
4.9.1. Background
When building the Car variant of AOSP there are no map applications
included and instead a green placeholder screen is seen. This application gets
included when building the userdebug builds to replace the green screen
placeholder.
4.9.2. Launching the app
Boot the EVM with binaries built using
am62p_car-bp2a-userdebuglunch target
The SnappMaps application should be visible by default on the home screen
Note
Internet connection is required for this application to work.