AM263x MCU+ SDK  09.02.00
i2c_lld.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2024 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
54 #ifndef I2C_LLD_H_
55 #define I2C_LLD_H_
56 
57 /* ========================================================================== */
58 /* Include Files */
59 /* ========================================================================== */
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 #include <stdint.h>
66 #include <stdbool.h>
67 #include <stdlib.h>
68 #include <stddef.h>
69 #include <drivers/i2c/v1/cslr_i2c.h>
70 #include <drivers/hw_include/hw_types.h>
71 #include <drivers/hw_include/cslr_i2c.h>
72 
73 /* ========================================================================== */
74 /* Macros & Typedefs */
75 /* ========================================================================== */
76 
84 #define I2C_STS_SUCCESS ((int32_t) 0)
85 
87 #define I2C_STS_ERR ((int32_t)-1)
88 
90 #define I2C_STS_ERR_TIMEOUT ((int32_t)-2)
91 
92 #define I2C_STS_ERR_INVALID_PARAM ((int32_t)-3)
93 
94 #define I2C_STS_ERR_BUS_BUSY ((int32_t)-4)
95 
97 #define I2C_STS_ERR_NO_ACK ((int32_t)-5)
98 
100 #define I2C_STS_ERR_ARBITRATION_LOST ((int32_t)-6)
101 
102 #define I2C_STS_RESTART ((int32_t)-7)
103 
114 #define I2C_NO_WAIT ((uint32_t)0)
115 
117 #define I2C_WAIT_FOREVER ((uint32_t)-1)
118 
127 #define I2C_STATE_RESET ((uint8_t) 0U)
128 
130 #define I2C_STATE_IDLE ((uint8_t) 1U)
131 
133 #define I2C_STATE_BUSY ((uint8_t) 2U)
134 
136 #define I2C_STATE_ERROR ((uint8_t) 3U)
137 
148 #define I2C_100KHZ ((uint8_t) 0U)
149 
150 #define I2C_400KHZ ((uint8_t) 1U)
151 
161 #define I2C_MEM_ADDR_SIZE_8_BITS ((uint8_t) 1U)
162 
163 #define I2C_MEM_ADDR_SIZE_16_BITS ((uint8_t) 2U)
164 
174 #define I2C_WRITE_STATE ((uint8_t) 10U)
175 
176 #define I2C_READ_STATE ((uint8_t) 11U)
177 
178 #define I2C_TARGET_XFER_STATE ((uint8_t) 12U)
179 
180 #define I2C_TARGET_RESTART_STATE ((uint8_t) 13U)
181 
184 /* ========================================================================== */
185 /* Structure Declarations */
186 /* ========================================================================== */
187 
198 typedef struct {
199 
201  uint8_t *writeBuf;
203  uint32_t writeCount;
205  uint8_t *readBuf;
207  uint32_t readCount;
208 
210 
220 typedef struct {
221 
225  uint32_t txnCount;
230  uint32_t targetAddress;
232  void *arg;
234  uint32_t timeout;
239  bool expandSA;
240 
242 
247 typedef struct {
248 
249  uint32_t deviceAddress;
251  uint8_t *buffer;
253  uint32_t size;
255  bool expandSA;
260 
265 typedef struct {
266 
269  uint32_t memAddr;
271  uint8_t memAddrSize;
275 
276 
293 typedef struct {
294 
296  const uint8_t *writeBuf;
298  uint32_t writeCount;
300  uint8_t *readBuf;
302  uint32_t readCount;
304  uint32_t timeout;
307  bool expandSA;
308 
310 
311 /* ========================================================================== */
312 /* Function pointers Declarations */
313 /* ========================================================================== */
314 
322 typedef uint32_t (*I2C_Clock_getTicks) (void);
323 
333 typedef uint32_t (*I2C_Clock_usecToTicks) (uint64_t usecs);
334 
342 typedef void (*I2C_Clock_uSleep) (uint32_t usec);
343 
352 typedef void (*I2C_lld_transferCompleteCallback) (void *args,
353  const I2CLLD_Message *msg,
354  int32_t transferStatus);
365  const I2CLLD_targetTransaction * targetTxn,
366  int32_t transferStatus);
367 
368 /* ========================================================================== */
369 /* Structure Declarations */
370 /* ========================================================================== */
371 
375 typedef struct {
376 
382  uint32_t baseAddr;
384  uint32_t intrNum;
386  uint8_t bitRate;
388  uint32_t funcClk;
390  uint32_t ownTargetAddr;
401 
407  uint8_t state;
409  uint32_t intStatusErr;
410 
420  uint8_t *writeBufIdx;
422  uint32_t writeCountIdx;
424  uint8_t *readBufIdx;
426  uint32_t readCountIdx;
428  uint32_t startTicks;
430  uint32_t currentTxnCount;
436  uint8_t *dataArray;
438  uint8_t addBuff[2];
440  uint8_t memAddrSize;
447  void* args;
448 
450 
451 /* ========================================================================== */
452 /* Function Declarations */
453 /* ========================================================================== */
454 
462 int32_t I2C_lld_init(I2CLLD_Handle handle);
463 
472 
481 
490 
503  I2C_ExtendedParams *extendedParams,
504  uint32_t timeout);
505 
516  I2C_ExtendedParams *extendedParams);
517 
530  I2C_ExtendedParams *extendedParams,
531  uint32_t timeout);
532 
543  I2C_ExtendedParams *extendedParams);
544 
557  I2C_Memory_ExtendedParams * mem_extendedParams,
558  uint32_t timeout);
559 
570  I2C_Memory_ExtendedParams * mem_extendedParams);
571 
584  I2C_Memory_ExtendedParams * mem_extendedParams,
585  uint32_t timeout);
586 
597  I2C_Memory_ExtendedParams * mem_extendedParams);
598 
610 
622 
635 
644 int32_t I2C_lld_probe(I2CLLD_Handle handle, uint32_t targetAddr);
645 
654 int32_t I2C_lld_setBusFrequency(I2CLLD_Handle handle, uint32_t busFrequency);
655 
656 /* ========================================================================== */
657 /* ISR Function Declarations */
658 /* ========================================================================== */
659 
667 
675 
676 #ifdef __cplusplus
677 }
678 #endif
679 
680 #endif /* I2C_LLD_H_ */
681 
I2CLLD_Object::Clock_getTicks
I2C_Clock_getTicks Clock_getTicks
Definition: i2c_lld.h:392
args
void * args
Definition: hsmclient_msg.h:4
I2CLLD_Object::startTicks
uint32_t startTicks
Definition: i2c_lld.h:428
I2CLLD_Message::txn
I2CLLD_Transaction * txn
Definition: i2c_lld.h:223
I2CLLD_Transaction::readCount
uint32_t readCount
Definition: i2c_lld.h:207
I2C_lld_Transaction_init
int32_t I2C_lld_Transaction_init(I2CLLD_Transaction *transaction)
API to set default values of I2CLLD_Transaction in transaction.
I2CLLD_Object::currentTargetTransaction
I2CLLD_targetTransaction * currentTargetTransaction
Definition: i2c_lld.h:418
I2CLLD_Object::writeCountIdx
uint32_t writeCountIdx
Definition: i2c_lld.h:422
I2CLLD_Object::writeBufIdx
uint8_t * writeBufIdx
Definition: i2c_lld.h:420
I2CLLD_targetTransaction::writeCount
uint32_t writeCount
Definition: i2c_lld.h:298
I2C_lld_Message_init
int32_t I2C_lld_Message_init(I2CLLD_Message *msg)
API to set default values of I2CLLD_Message in msg.
I2CLLD_targetTransaction::readCount
uint32_t readCount
Definition: i2c_lld.h:302
I2CLLD_Message::targetAddress
uint32_t targetAddress
Definition: i2c_lld.h:230
I2C_lld_targetTransferCompleteCallback
void(* I2C_lld_targetTransferCompleteCallback)(void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)
The definition of a transfer completion callback function used by the I2C driver when used in Target ...
Definition: i2c_lld.h:364
I2C_lld_write
int32_t I2C_lld_write(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
API to initiate the write transaction in polled mode.
I2CLLD_Object::funcClk
uint32_t funcClk
Definition: i2c_lld.h:388
I2CLLD_Message
I2C Message.
Definition: i2c_lld.h:220
I2CLLD_Object::Clock_uSleep
I2C_Clock_uSleep Clock_uSleep
Definition: i2c_lld.h:396
I2C_Memory_ExtendedParams::memAddr
uint32_t memAddr
Definition: i2c_lld.h:269
I2CLLD_Message::arg
void * arg
Definition: i2c_lld.h:232
I2CLLD_targetTransaction::readBuf
uint8_t * readBuf
Definition: i2c_lld.h:300
I2C_lld_read
int32_t I2C_lld_read(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
API to initiate the read transaction in polled mode.
I2CLLD_Transaction::writeBuf
uint8_t * writeBuf
Definition: i2c_lld.h:201
I2C_lld_transferCompleteCallback
void(* I2C_lld_transferCompleteCallback)(void *args, const I2CLLD_Message *msg, int32_t transferStatus)
The definition of a transfer completion callback function used by the I2C driver when used in Control...
Definition: i2c_lld.h:352
I2CLLD_Transaction::readBuf
uint8_t * readBuf
Definition: i2c_lld.h:205
I2CLLD_Message::timeout
uint32_t timeout
Definition: i2c_lld.h:234
I2CLLD_Object::i2ctxn
I2CLLD_Transaction i2ctxn
Definition: i2c_lld.h:434
I2CLLD_Object::ownTargetAddr
uint32_t ownTargetAddr
Definition: i2c_lld.h:390
I2CLLD_Message::expandSA
bool expandSA
Definition: i2c_lld.h:239
I2C_lld_readIntr
int32_t I2C_lld_readIntr(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
API to initiate the read transaction in Interrupt mode.
I2C_ExtendedParams::expandSA
bool expandSA
Definition: i2c_lld.h:255
I2CLLD_Object::currentMsg
I2CLLD_Message * currentMsg
Definition: i2c_lld.h:416
I2CLLD_Transaction
I2C Transaction.
Definition: i2c_lld.h:198
I2C_ExtendedParams::buffer
uint8_t * buffer
Definition: i2c_lld.h:251
I2C_lld_mem_read
int32_t I2C_lld_mem_read(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
Function to initiate a transfer from I2C in interrupt mode.
I2C_lld_mem_write
int32_t I2C_lld_mem_write(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
Function to initiate a transfer from I2C in interrupt mode.
I2CLLD_targetTransaction::timeout
uint32_t timeout
Definition: i2c_lld.h:304
I2CLLD_Object::dataArray
uint8_t * dataArray
Definition: i2c_lld.h:436
I2CLLD_Object::intrNum
uint32_t intrNum
Definition: i2c_lld.h:384
I2CLLD_Object::baseAddr
uint32_t baseAddr
Definition: i2c_lld.h:382
I2C_lld_transferIntr
int32_t I2C_lld_transferIntr(I2CLLD_Handle handle, I2CLLD_Message *msg)
Function to initiate a transfer from I2C in interrupt mode.
I2CLLD_targetTransaction::expandSA
bool expandSA
Definition: i2c_lld.h:307
I2C_lld_targetIsr
void I2C_lld_targetIsr(void *args)
This is the I2C Target ISR and can be used as IRQ handler in Target mode.
I2CLLD_Message::txnCount
uint32_t txnCount
Definition: i2c_lld.h:225
I2C_lld_transferPoll
int32_t I2C_lld_transferPoll(I2CLLD_Handle handle, I2CLLD_Message *msg)
Function to initiate a transfer from I2C in polled mode.
I2CLLD_Object::readCountIdx
uint32_t readCountIdx
Definition: i2c_lld.h:426
I2C_lld_init
int32_t I2C_lld_init(I2CLLD_Handle handle)
This API Initializes the I2C instance.
I2CLLD_Object::transferCompleteCallback
I2C_lld_transferCompleteCallback transferCompleteCallback
Definition: i2c_lld.h:398
I2C_Memory_ExtendedParams::extendedParams
I2C_ExtendedParams extendedParams
Definition: i2c_lld.h:267
I2CLLD_Transaction::writeCount
uint32_t writeCount
Definition: i2c_lld.h:203
I2C_Clock_getTicks
uint32_t(* I2C_Clock_getTicks)(void)
The definition of a get System Tick function used by the I2C driver to keep track of time.
Definition: i2c_lld.h:322
I2CLLD_Object::memTxnActive
bool memTxnActive
Definition: i2c_lld.h:443
I2CLLD_Object::memAddrSize
uint8_t memAddrSize
Definition: i2c_lld.h:440
I2CLLD_Message::controllerMode
bool controllerMode
Definition: i2c_lld.h:236
I2CLLD_targetTransaction::writeBuf
const uint8_t * writeBuf
Definition: i2c_lld.h:296
I2C_Clock_usecToTicks
uint32_t(* I2C_Clock_usecToTicks)(uint64_t usecs)
The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microsec...
Definition: i2c_lld.h:333
I2C_Memory_ExtendedParams
Data structure used with I2C_lld_mem_write(), I2C_lld_mem_writeIntr(), I2C_lld_mem_read(),...
Definition: i2c_lld.h:265
I2C_ExtendedParams::deviceAddress
uint32_t deviceAddress
Definition: i2c_lld.h:249
I2C_lld_writeIntr
int32_t I2C_lld_writeIntr(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
API to initiate the write transaction in Interrupt mode.
I2C_Clock_uSleep
void(* I2C_Clock_uSleep)(uint32_t usec)
The definition of a sleep function used by the I2C driver for delay.
Definition: i2c_lld.h:342
I2CLLD_Object::intStatusErr
uint32_t intStatusErr
Definition: i2c_lld.h:409
I2C_ExtendedParams
Data structure used with I2C_lld_write(), I2C_lld_writeIntr(), I2C_lld_read(), I2C_lld_readIntr()
Definition: i2c_lld.h:247
I2C_lld_mem_readIntr
int32_t I2C_lld_mem_readIntr(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
Function to initiate a transfer from I2C in interrupt mode.
I2CLLD_Object::readBufIdx
uint8_t * readBufIdx
Definition: i2c_lld.h:424
I2CLLD_Object::bitRate
uint8_t bitRate
Definition: i2c_lld.h:386
I2C_lld_probe
int32_t I2C_lld_probe(I2CLLD_Handle handle, uint32_t targetAddr)
Function to probe I2C.
I2C_lld_setBusFrequency
int32_t I2C_lld_setBusFrequency(I2CLLD_Handle handle, uint32_t busFrequency)
Function to set the bus frequency.
I2C_lld_mem_writeIntr
int32_t I2C_lld_mem_writeIntr(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
Function to initiate a transfer from I2C in interrupt mode.
I2C_lld_controllerIsr
void I2C_lld_controllerIsr(void *args)
This is the I2C Controller ISR and can be used as IRQ handler in Controller mode.
I2CLLD_Object::targetTransferCompleteCallback
I2C_lld_targetTransferCompleteCallback targetTransferCompleteCallback
Definition: i2c_lld.h:400
I2C_lld_deInit
int32_t I2C_lld_deInit(I2CLLD_Handle handle)
This API De-Initializes the I2C instance.
I2CLLD_Object::state
uint8_t state
Definition: i2c_lld.h:407
I2C_ExtendedParams::size
uint32_t size
Definition: i2c_lld.h:253
I2CLLD_Object::i2cTargetTransaction
I2CLLD_targetTransaction i2cTargetTransaction
Definition: i2c_lld.h:445
I2CLLD_Object
I2C Driver Object.
Definition: i2c_lld.h:375
I2CLLD_Object::Clock_usecToTicks
I2C_Clock_usecToTicks Clock_usecToTicks
Definition: i2c_lld.h:394
I2CLLD_Object::i2cMsg
I2CLLD_Message i2cMsg
Definition: i2c_lld.h:432
I2CLLD_targetTransaction
I2C Target Transaction.
Definition: i2c_lld.h:293
I2CLLD_Object::args
void * args
Definition: i2c_lld.h:447
I2CLLD_Handle
struct I2CLLD_Object * I2CLLD_Handle
I2C_lld_targetTransferIntr
int32_t I2C_lld_targetTransferIntr(I2CLLD_Handle handle, I2CLLD_targetTransaction *txn)
Function to initiate a transfer from I2C in target mode.
I2C_Memory_ExtendedParams::memAddrSize
uint8_t memAddrSize
Definition: i2c_lld.h:271
I2CLLD_Object::currentTxnCount
uint32_t currentTxnCount
Definition: i2c_lld.h:430