This module contains FastRTS APIs for optimized trignometric and math functions.
◆ RTS_TEXT_SECTION
#define RTS_TEXT_SECTION __attribute__((section(".trigText"))) __attribute__((always_inline)) |
◆ RTS_DATA_SECTION
#define RTS_DATA_SECTION __attribute__((aligned(8), section(".trigData"))) |
◆ FastRTS_cosf()
float FastRTS_cosf |
( |
const float |
theta | ) |
|
The Cosine Function.
- Parameters
-
[in] | theta | - Angle in radians |
- Returns
- The cosine of the angle
◆ FastRTS_sinf()
float FastRTS_sinf |
( |
const float |
theta | ) |
|
The Sine Function.
- Parameters
-
[in] | theta | - Angle in radians |
- Returns
- The sine of the angle
◆ FastRTS_sincos()
void FastRTS_sincos |
( |
const float |
theta, |
|
|
float * |
retValues |
|
) |
| |
The Sine/Cosine Function.
- Parameters
-
[in] | theta | - Angle in radians |
[in] | retValues | - pointer that stores return sine and cosine values |
◆ FastRTS_acosf()
float FastRTS_acosf |
( |
const float |
theta | ) |
|
The Arccosine Function.
- Parameters
-
[in] | theta | - Angle in radians |
- Returns
- The cosine of the angle
◆ FastRTS_asinf()
float FastRTS_asinf |
( |
const float |
theta | ) |
|
The Arcsine Function.
- Parameters
-
[in] | theta | - Angle in radians |
- Returns
- The sine of the angle
◆ FastRTS_atanf()
float FastRTS_atanf |
( |
const float |
x | ) |
|
The Arctangent function.
- Parameters
-
[in] | x | the arc subtended by the angle theta |
- Returns
- theta , the angle subtended by the arc of length x
◆ FastRTS_atan2f()
float FastRTS_atan2f |
( |
const float |
y, |
|
|
const float |
x |
|
) |
| |
The Arctangent(y,x) function.
- Parameters
-
[in] | y | - numerator of the ratio y/x which is the length of the arc subtended by the angle theta |
[in] | x | - denominator of the ratio y/x which is the length of the arc subtended by the angle theta |
- Returns
- theta , the angle subtended by the arc of length y/x
◆ FastRTS_expf()
float FastRTS_expf |
( |
const float |
x | ) |
|
The Exponent function.
- Parameters
-
[in] | x | - argument whose exponent is to be calculated |
- Note
- due to the allowable range of 32-bit float, the maximum exponent allowed is +/-88
- Returns
- e^x , the exponent of the argument
◆ FastRTS_logf()
float FastRTS_logf |
( |
const float |
x | ) |
|
The Natural Logarithm function.
- Parameters
-
[in] | x | - argument whose logarithm is to be calculated |
- Returns
- log(x) , the natural logarithm of the argument
◆ FastRTS_sqrtf()