Defines the ESMO controller object.
float32_t ESMO_Handle::scaleFreq_Hz |
float32_t ESMO_Handle::speed_sf |
float32_t ESMO_Handle::voltage_sf |
float32_t ESMO_Handle::current_sf |
float32_t ESMO_Handle::Ts |
float32_t ESMO_Handle::base_wTs |
float32_t ESMO_Handle::filterFc_sf |
float32_t ESMO_Handle::Fdsmopos |
float32_t ESMO_Handle::Fqsmopos |
float32_t ESMO_Handle::Gdsmopos |
float32_t ESMO_Handle::Gqsmopos |
float32_t ESMO_Handle::Kslf |
float32_t ESMO_Handle::E0 |
float32_t ESMO_Handle::Kslide |
float32_t ESMO_Handle::KslideMax |
float32_t ESMO_Handle::KslideMin |
float32_t ESMO_Handle::Valpha |
float32_t ESMO_Handle::Vbeta |
float32_t ESMO_Handle::EstIalpha |
float32_t ESMO_Handle::EstIbeta |
float32_t ESMO_Handle::Ealpha |
float32_t ESMO_Handle::Ebeta |
float32_t ESMO_Handle::Zalpha |
float32_t ESMO_Handle::Zbeta |
float32_t ESMO_Handle::Ed |
float32_t ESMO_Handle::Eq |
float32_t ESMO_Handle::Eq_mag |
float32_t ESMO_Handle::thetaOffset_rad |
float32_t ESMO_Handle::thetaElec_rad |
float32_t ESMO_Handle::thetaErr |
float32_t ESMO_Handle::thetaErrSF |
float32_t ESMO_Handle::theta |
float32_t ESMO_Handle::thetaPll |
float32_t ESMO_Handle::thetaDelta |
float32_t ESMO_Handle::offsetSF |
float32_t ESMO_Handle::thetaEst |
float32_t ESMO_Handle::speedRef |
float32_t ESMO_Handle::speedEst |
float32_t ESMO_Handle::speedFlt |
float32_t ESMO_Handle::pll_Out |
float32_t ESMO_Handle::pll_Umax |
float32_t ESMO_Handle::pll_Umin |
float32_t ESMO_Handle::pll_ui |
float32_t ESMO_Handle::pll_Kp |
float32_t ESMO_Handle::pll_KpMax |
float32_t ESMO_Handle::pll_KpMin |
float32_t ESMO_Handle::pll_KpSF |
float32_t ESMO_Handle::pll_Ki |
float32_t ESMO_Handle::lpf_b0 |
float32_t ESMO_Handle::lpf_a1 |
float32_t ESMO_Handle::lpfFc_Hz |