Top level header that contains all DCL common strctures and functions.
Go to the source code of this file.
Macros | |
#define | IEEE754_TYPES |
Defines single,double precision data type. More... | |
#define | _DCL_CODE_ACCESS static inline |
Defines the scope of dcl functions. More... | |
#define | _DCL_CRIT_ACCESS static __attribute__((always_inline)) |
Defines the scope of critical dcl functions. More... | |
#define | _DCL_VOLATILE |
Defines volatile for DCL strctures. More... | |
#define | DCL_setBreakPoint() |
Set a software breakpoint assembly instruction. More... | |
#define | DCL_disableInts() 0 |
Define enable and disable interrupt operations. More... | |
#define | DCL_restoreInts(v) |
Typedefs | |
typedef float | float32_t |
typedef double | float64_t |
typedef uint32_t | dcl_interrupt_t |