AM263x Motor Control SDK  09.01.00

Introduction

Contains PI2 (double integrator) controller with its related structures and functions.

Go to the source code of this file.

Data Structures

struct  DCL_PI2_SPS
 Defines DCL_PI2 shadow parameter set used for updating controller parameter. More...
 
struct  dcl_pi2
 DCL_PI2 object for storing PI2 specific parameters PI2 - PI controller with double integrators. More...
 

Macros

#define PI2_SPS_DEFAULTS   { 1.0f, 0.0f, 1.0f, -1.0f }
 Defines default values to initialize DCL_PI2_SPS. More...
 
#define PI2_DEFAULTS
 Defines default values to initialize DCL_PI2. More...
 
#define PI2_INT_DEFAULTS
 Macro for internal default values to initialize DCL_PI2 Example: DCL_PI2 pi2_ctrl = { .Kp = 1.0f, .Ki = 0.0f, .Umax = 1.0f, .Umin = -1.0f, PI2_INT_DEFAULTS };. More...
 
#define DCL_initPI2()   &(DCL_PI2)PI2_DEFAULTS
 Initialize DCL_PI2 struct with default parameters Example: DCL_PI2 pi2_ctrl = DCL_initPI2();. More...
 
#define DCL_initPI2asParam(kp, ki, umax, umin)
 Initialize DCL_PI2 struct with input controller parameters Example: DCL_PI2* pi2_ctrl = DCL_initPI2asParam(1.0f,0.0f,1.0f,-1.0f); Note: input parameter needs to be in the same order as listed in PI2_SPS struct. More...
 
#define DCL_initPI2asSPS(pi2_ptr, sps_ptr)
 Initialize DCL_PI2 struct with sps parameters Example: DCL_PI2_SPS pi2_sps = { .Kp = , .Ki = , ...}; DCL_PI2 pi2_ctrl; DCL_initPI2asSPS(&pi2_ctrl,&pi2_sps);. More...
 

Typedefs

typedef _DCL_VOLATILE struct dcl_pi2 DCL_PI2
 
typedef _DCL_VOLATILE struct dcl_pi2PI2_Handle
 

Functions

_DCL_CODE_ACCESS void DCL_resetPI2 (DCL_PI2 *pi2)
 Resets PI2 internal storage data with interrupt protection. More...
 
_DCL_CODE_ACCESS void DCL_forceUpdatePI2 (DCL_PI2 *pi2)
 Loads PI2 tuning parameter from its SPS parameter without interrupt protection. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION void DCL_updatePI2NoCheck (DCL_PI2 *pi2)
 Loads PI2 tuning parameter from its SPS parameter with interrupt protection. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION bool DCL_updatePI2 (DCL_PI2 *pi2)
 A conditional update based on the update flag. If the update status is set, the function will update PI2 parameter from its SPS parameter and clear the status flag on completion. Note: Use DCL_setUpdateStatus(pi2) to set the update status. More...
 
_DCL_CODE_ACCESS _DCL_CODE_SECTION float32_t DCL_runPI2Series (DCL_PI2 *pi2, float32_t rk, float32_t yk)
 Executes an inline series form PI2 controller on the FPU32. More...