Introduction
The Transformation module consists of transformation commonly found in motor-control applications.
Features Supported
Transformation module includes:
- Clarke transformation
- Park transformation
- Inverse Park transformation
- Space Vector Generation (SVGEN)
- Common-mode subtraction approach
- DPWM Generation (Part of SVGEN)
- Maximum Modulation
- Minimum Modulation
Features Not Supported
N/A
Benchmark Results
A benchmark on R5F core has been conducted to observe the following results when running the following functions:
Transform Function | Cpu Cycles |
Clarke Transform |
CLARKE_run_twoInput | 16 |
CLARKE_run_threeInput | 18 |
Park Transform |
PARK_run | 19* |
Inverse Park Transform |
IPARK_run | 19* |
Space Vector Generation |
SVGEN_runCom | 41 |
DPWM Generation |
SVGEN_runMax | 36 |
SVGEN_runMin | 36 |
- Note
- both PARK and IPARK does not include trigonometric calculations of phasor. For R5F core, it's recommened to leverage the fast ti_arm_sincos() function found in ti_arm_trig/mathlib of MCU+ SDK.
- Ran with TI Clang Compiler v3.2.0.LTS, with -Os flag and functions force-inlined onto the benchmarking function placed in TCM memory. Obtained the average result from 600 consecutive loops of running transform functions with DPL CycleCountP, mimicking the usage of a control loop.
- Actual result may vary depending on provided datasets and memory configuration. For R5F, it is recommended for users to map control loops to TCM for the best performance.
Provided Examples
The following examples has been provided to demonstrate transformation module:
Additional References
N/A
API
APIs for Transformation Algorithms