Simple data test incorporating foc-related libraries
This example runs verifies various transforms libraries used in motor-control application, specifically as a building block of Field of Control (FOC) motor design.
It demonstrates how to run clarke, park, inverse park transform and space-vector generation (svgen). This test trys to mimic a conventional workflow of passing current values into clarke transform, then park, then inverse park (PI controllers are neglected here but should exist for both open and close-loop design) and finally passing to svgen to generate the three-phase ABC value.
The test used an aribitary phasor angle that feeds into park/ipark, as opposed to an angle generation module required by an actual FOC design.
The test vector then compares the PARK, SVGEN results to ensure the integraty of the library.
Folder/Files | Description |
---|---|
${SDK_INSTALL_PATH}/examples/transforms/transforms_test | |
transforms_test.c | Main function for transforms library testing |
transforms_test.h | Contains all initialization of test strctures and variables |
${SDK_INSTALL_PATH}/source/transforms | |
clarke/ | Folder containing CLARKE library source |
park/ | Folder containing PARK library source |
ipark/ | Folder containing IPARK library source |
svgen/ | Folder containing SVGEN library source |
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 nortos |
r5fss0-0 freertos | |
Toolchain | ti-arm-clang |
Boards | am263x-cc, am263x-lp |
Example folder | examples/transforms/transforms_test |
Shown below is a sample output when the application is run, assuming when all test passes: