AM263x MCU+ SDK  09.00.00
SDL_MCRC_SignatureRegAddr_t Struct Reference

Detailed Description

Structure for accessing MCRC registers address which are 64 bit wide.

Data Fields

uint32_t regL
 
uint32_t regH
 

Field Documentation

◆ regL

uint32_t SDL_MCRC_SignatureRegAddr_t::regL

Lower 32 bits of the 64 bit MCRC Signature register address

◆ regH

uint32_t SDL_MCRC_SignatureRegAddr_t::regH

Upper 32 bits of the 64 bit MCRC Signature register address