AM263x MCU+ SDK  09.00.00

Introduction

This peripheral driver supports ICSSG Ethernet peripheral found in Jacinto 7 processor family.

Data Structures

struct  Icssg_TxTsEvtCbInfo
 Icssg TX timestamp event callback info structure. This is passed to application when TX timestamp is retrieved by ICSSG driver. More...
 
struct  IcssgMacPort_SetQueueCtPremptModeInArgs
 Input arguments for ICSSG_MACPORT_IOCTL_SET_QUEUE_CUT_THROUGH_PREEMPT_SELECT command. More...
 
struct  IcssgMacPort_ConfigSpecialFramePrioInArgs
 Input arguments for ICSSG_MACPORT_IOCTL_CONFIG_SPL_FRAME_PRIO command. More...
 
struct  IcssgMacPort_SetPortStateInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_PORT_STATE command. More...
 
struct  Icssg_SetAcceptFrameCheckInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK command. More...
 
struct  Icssg_MacAddr
 MAC address. More...
 
struct  IcssgMacPort_SetMacAddressInArgs
 Input args for ICSSG_MACPORT_IOCTL_SET_MACADDR command. More...
 
struct  Icssg_VlanFidParams
 VLAN FID entry parameters. More...
 
struct  Icssg_VlanFidEntry
 VLAN FID table entry. More...
 
struct  Icssg_FdbEntry
 FDB entry configuration. More...
 
struct  Icssg_DfltVlanCfg
 Default VLAN configuration. More...
 
struct  Icssg_MacPortDfltVlanCfgInArgs
 Input arguments for ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID command. More...
 
struct  Icssg_IngressRateLim
 Input arguments for ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM command. More...
 
struct  Icssg_custom_Fw
 ICSSG custom firmware. More...
 
struct  Icssg_FwPoolMem
 ICSSG buffer pool memories. More...
 
struct  Icssg_MdioLinkStateChangeInfo
 PHY link status change event information. More...
 
struct  Icssg_mdioLinkIntCfg
 
struct  Icssg_Cfg
 ICSSG peripheral configuration parameters. More...
 
struct  IcssgMacPort_Cfg
 ICSSG mac port configuration parameters. More...
 

Functions

const Icssg_FwPoolMemEnetCb_GetFwPoolMem (Enet_Type enetType, uint32_t instId)
 ICSSG memory pool callback function. More...
 
void IcssgMacPort_initCfg (IcssgMacPort_Cfg *macPortCfg)
 Initialises Mac Port COnfiguration. More...
 
uint32_t Icssg_getSliceNum (Enet_Type enetType, uint32_t instId, Enet_MacPort macPort)
 ICSSG memory pool callback function. More...
 

Typedefs

typedef void(* Icssg_MdioLinkStateChangeCb) (Icssg_MdioLinkStateChangeInfo *info, void *appArg)
 Icssg PHY link state change callback function. More...
 

Enumerations

enum  Icssg_Instance_Num { ICSSG_INSTANCE_NUM_0, ICSSG_INSTANCE_NUM_1, ICSSG_INSTANCE_NUM_2 }
 ICSSG instance numbers. More...
 
enum  Icssg_Ioctl {
  ICSSG_MACPORT_IOCTL_ENABLE_PROMISC_MODE = ICSSG_PUBLIC_IOCTL(0U), ICSSG_MACPORT_IOCTL_DISABLE_PROMISC_MODE = ICSSG_PUBLIC_IOCTL(1U), ICSSG_PER_IOCTL_VLAN_RESET_TABLE = ICSSG_PUBLIC_IOCTL(2U), ICSSG_PER_IOCTL_VLAN_SET_ENTRY = ICSSG_PUBLIC_IOCTL(3U),
  ICSSG_PER_IOCTL_VLAN_GET_ENTRY = ICSSG_PUBLIC_IOCTL(4U), ICSSG_PER_IOCTL_SET_PORT_STATE = ICSSG_PUBLIC_IOCTL(5U), ICSSG_FDB_IOCTL_ADD_ENTRY = ICSSG_PUBLIC_IOCTL(6U), ICSSG_FDB_IOCTL_REMOVE_ENTRY = ICSSG_PUBLIC_IOCTL(7U),
  ICSSG_FDB_IOCTL_REMOVE_ALL_ENTRIES = ICSSG_PUBLIC_IOCTL(8U), ICSSG_FDB_IOCTL_REMOVE_AGEABLE_ENTRIES = ICSSG_PUBLIC_IOCTL(9U), ICSSG_MACPORT_IOCTL_SET_MACADDR = ICSSG_PUBLIC_IOCTL(10U), ICSSG_HOSTPORT_IOCTL_SET_MACADDR = ICSSG_PUBLIC_IOCTL(11U),
  ICSSG_PER_IOCTL_TAS_TRIGGER = ICSSG_PUBLIC_IOCTL(12U), ICSSG_PER_IOCTL_TAS_ENABLE = ICSSG_PUBLIC_IOCTL(13U), ICSSG_PER_IOCTL_TAS_DISABLE = ICSSG_PUBLIC_IOCTL(14U), ICSSG_PER_IOCTL_TAS_RESET = ICSSG_PUBLIC_IOCTL(15U),
  ICSSG_PER_IOCTL_VLAN_SET_HOSTPORT_DFLT_VID = ICSSG_PUBLIC_IOCTL(16U), ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID = ICSSG_PUBLIC_IOCTL(17U), ICSSG_FDB_IOCTL_SET_AGING_PERIOD = ICSSG_PUBLIC_IOCTL(18U), ICSSG_MACPORT_IOCTL_ENABLE_UCAST_FLOOD = ICSSG_PUBLIC_IOCTL(19U),
  ICSSG_MACPORT_IOCTL_DISABLE_UCAST_FLOOD = ICSSG_PUBLIC_IOCTL(20U), ICSSG_MACPORT_IOCTL_ENABLE_MCAST_FLOOD = ICSSG_PUBLIC_IOCTL(21U), ICSSG_MACPORT_IOCTL_DISABLE_MCAST_FLOOD = ICSSG_PUBLIC_IOCTL(22U), ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK = ICSSG_PUBLIC_IOCTL(23U),
  ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM = ICSSG_PUBLIC_IOCTL(24U), ICSSG_MACPORT_IOCTL_SET_QUEUE_CUT_THROUGH_PREEMPT_SELECT = ICSSG_PUBLIC_IOCTL(25U), ICSSG_MACPORT_IOCTL_CONFIG_SPL_FRAME_PRIO = ICSSG_PUBLIC_IOCTL(26U), ICSSG_INTERNAL_IOCTL_REGISTER_HANDLER = ICSSG_PUBLIC_IOCTL(27U)
}
 ICSSG IOCTL commands. More...
 
enum  Icssg_QueuePreemptMode { ICSSG_QUEUE_PREEMPT_MODE_EXPRESS, ICSSG_QUEUE_PREEMPT_MODE_PREEMPT }
 Queue preemptive mode: express or preemptive. More...
 
enum  Icssg_QueueForwardMode { ICSSG_QUEUE_FORWARD_MODE_STOREANDFWD, ICSSG_QUEUE_FORWARD_MODE_CUTTHROUGH }
 Queue forward mode: cut-through or store-and-forward. More...
 
enum  Icssg_PortState {
  ICSSG_PORT_STATE_DISABLED, ICSSG_PORT_STATE_BLOCKING, ICSSG_PORT_STATE_FORWARD, ICSSG_PORT_STATE_FORWARD_WO_LEARNING,
  ICSSG_PORT_STATE_TAS_TRIGGER, ICSSG_PORT_STATE_TAS_ENABLE, ICSSG_PORT_STATE_TAS_RESET, ICSSG_PORT_STATE_TAS_DISABLE
}
 Port states. More...
 
enum  Icssg_AcceptFrameCheck { ICSSG_ACCEPT_ONLY_VLAN_TAGGED, ICSSG_ACCEPT_ONLY_UNTAGGED_PRIO_TAGGED, ICSSG_ACCEPT_ALL }
 Acceptable frame check criteria. More...
 

Macros

#define ICSSG_PUBLIC_IOCTL(x)
 Helper macro to create IOCTL commands for ICSSG per. More...
 
#define ICSSG_PORT_NUM   (3U)
 Number of supported ports (host port, physical ports 1 and 2). More...
 
#define ICSSG_MAC_PORT_MAX   (ICSSG_PORT_NUM - 1U)
 Maximum number of MAC ports per ICSSG instance. More...
 
#define ICSSG_PER_DUALMAC_PORT_MAX   (1U)
 Maximum number of MAC ports in a ICSSG peripheral in Dual-MAC mode. Note that each port in Dual-MAC is handled as a separate Enet peripheral. More...
 
#define ICSSG_PER_SWITCH_PORT_MAX   (ICSSG_MAC_PORT_MAX)
 Maximum number of MAC ports in a ICSSG peripheral in Switch mode. More...
 
#define ICSSG_INSTANCE_NUM   (2U)
 Number of supported icssg instances. More...
 
#define ICSSG_MAX_NUM_BUFFER_POOLS   (24U)
 Max number of buffer pools. More...
 
#define ICSSG_DUALMAC_TX_CH_NUM   (8U)
 Number of TX channels per slice in Dual-MAC mode. More...
 
#define ICSSG_DUALMAC_RX_FLOW_NUM   (8U)
 Number of RX flows per slice in Dual-MAC mode. More...
 
#define ICSSG_SWITCH_TX_CH_NUM   (8U)
 Number of TX channels in Switch mode. More...
 
#define ICSSG_SWITCH_RX_FLOW_NUM   (8U)
 Number of RX flows in Switch mode. More...
 
#define ICSSG_DUALMAC_PORT_BUFFER_POOL_NUM   (0U)
 Number of port buffer pools required for Dual-MAC. More...
 
#define ICSSG_DUALMAC_HOST_EGRESS_QUEUE_NUM   (2U)
 Number of host egress queues required for Dual-MAC. More...
 
#define ICSSG_SWITCH_PORT_BUFFER_POOL_NUM   (8U)
 Number of port buffer pools required for Dual-MAC. More...
 
#define ICSSG_SWITCH_HOST_EGRESS_QUEUE_NUM   (2U)
 Number of host egress queues required for Dual-MAC. More...
 
#define ICSSG_HOST_EGRESS_BUFFER_PADDING   (2048U)
 Host egress queue padding size. More...
 
#define ICSSG_SCRATCH_BUFFER_SIZE   (ENET_UTILS_ALIGN((2048U), ICSSG_CACHELINE_ALIGNMENT))
 Size of the scratch buffer used for error frames and large frames. More...
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH0   (0U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH1   (1U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH2   (2U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH3   (3U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH4   (4U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH5   (5U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH6   (6U)
 
#define ICSSG_RATE_SRC_SEL_FT1_MATCH7   (7U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH0   (8U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH1   (9U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH2   (10U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH3   (11U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH4   (12U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH5   (13U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH6   (14U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH7   (15U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH8   (16U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH9   (17U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH10   (18U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH11   (19U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH12   (20U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH13   (21U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH14   (22U)
 
#define ICSSG_RATE_SRC_SEL_FT3_MATCH15   (23U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_UC   (24U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_MC   (25U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_BC   (26U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_SAV   (27U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_FWD   (28U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_RCV   (29U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_VLAN   (30U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_DA_P   (31U)
 
#define ICSSG_RATE_SRC_SEL_FT_RX_DA_I   (32U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW0   (33U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW1   (34U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW2   (35U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW3   (36U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW4   (37U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW5   (38U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW6   (39U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW7   (40U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW8   (41U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW9   (42U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW10   (43U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW11   (44U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW12   (45U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW13   (46U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW14   (47U)
 
#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW15   (48U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH0   (0U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH1   (1U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH2   (2U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH3   (3U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH4   (4U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH5   (5U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH6   (6U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH7   (7U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH8   (8U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH9   (9U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH10   (10U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH11   (11U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH12   (12U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH13   (13U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH14   (14U)
 
#define ICCSG_RX_CLASS_DATA_FT3_MATCH15   (15U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH0   (16U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH1   (17U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH2   (18U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH3   (19U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH4   (20U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH5   (21U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH6   (22U)
 
#define ICCSG_RX_CLASS_DATA_FT1_MATCH7   (23U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_DA_I   (24U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_DA_P   (25U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_VLAN   (26U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_RCV   (27U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_FWD   (28U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_BC   (29U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_MC   (30U)
 
#define ICCSG_RX_CLASS_DATA_FT_RX_SAV   (31U)
 
#define ICSSG_TAS_MIN_CYCLE_TIME_NS   (1000000)
 Minimum cycle time supported by implementation (in ns). More...
 
#define ICSSG_TAS_MIN_WINDOW_DURATION_NS   (10000)
 Minimum TAS window duration supported by implementation (in ns). More...
 

ICSSG FDB entry fields.

#define ICSSG_FDB_ENTRY_P0_MEMBERSHIP   (ENET_BIT(0U))
 Host port membership. More...
 
#define ICSSG_FDB_ENTRY_P1_MEMBERSHIP   (ENET_BIT(1U))
 Physical port 1 membership. More...
 
#define ICSSG_FDB_ENTRY_P2_MEMBERSHIP   (ENET_BIT(2U))
 Physical port 2 membership. More...
 
#define ICSSG_FDB_ENTRY_AGEABLE   (ENET_BIT(3U))
 Ageable bit. More...
 
#define ICSSG_FDB_ENTRY_BLOCK   (ENET_BIT(4U))
 Block bit. More...
 
#define ICSSG_FDB_ENTRY_SECURE   (ENET_BIT(5U))
 Secure bit. More...
 
#define ICSSG_FDB_ENTRY_TOUCHED   (ENET_BIT(6U))
 Touched bit. More...
 
#define ICSSG_FDB_ENTRY_VALID   (ENET_BIT(7U))
 Valid bit. More...
 

Macro Definition Documentation

◆ ICSSG_PUBLIC_IOCTL

#define ICSSG_PUBLIC_IOCTL (   x)
Value:
ENET_IOCTL_PER_ICSSG | \
ENET_IOCTL_MIN(x))

Helper macro to create IOCTL commands for ICSSG per.

◆ ICSSG_PORT_NUM

#define ICSSG_PORT_NUM   (3U)

Number of supported ports (host port, physical ports 1 and 2).

◆ ICSSG_MAC_PORT_MAX

#define ICSSG_MAC_PORT_MAX   (ICSSG_PORT_NUM - 1U)

Maximum number of MAC ports per ICSSG instance.

◆ ICSSG_PER_DUALMAC_PORT_MAX

#define ICSSG_PER_DUALMAC_PORT_MAX   (1U)

Maximum number of MAC ports in a ICSSG peripheral in Dual-MAC mode. Note that each port in Dual-MAC is handled as a separate Enet peripheral.

◆ ICSSG_PER_SWITCH_PORT_MAX

#define ICSSG_PER_SWITCH_PORT_MAX   (ICSSG_MAC_PORT_MAX)

Maximum number of MAC ports in a ICSSG peripheral in Switch mode.

◆ ICSSG_INSTANCE_NUM

#define ICSSG_INSTANCE_NUM   (2U)

Number of supported icssg instances.

◆ ICSSG_MAX_NUM_BUFFER_POOLS

#define ICSSG_MAX_NUM_BUFFER_POOLS   (24U)

Max number of buffer pools.

◆ ICSSG_DUALMAC_TX_CH_NUM

#define ICSSG_DUALMAC_TX_CH_NUM   (8U)

Number of TX channels per slice in Dual-MAC mode.

◆ ICSSG_DUALMAC_RX_FLOW_NUM

#define ICSSG_DUALMAC_RX_FLOW_NUM   (8U)

Number of RX flows per slice in Dual-MAC mode.

◆ ICSSG_SWITCH_TX_CH_NUM

#define ICSSG_SWITCH_TX_CH_NUM   (8U)

Number of TX channels in Switch mode.

◆ ICSSG_SWITCH_RX_FLOW_NUM

#define ICSSG_SWITCH_RX_FLOW_NUM   (8U)

Number of RX flows in Switch mode.

◆ ICSSG_DUALMAC_PORT_BUFFER_POOL_NUM

#define ICSSG_DUALMAC_PORT_BUFFER_POOL_NUM   (0U)

Number of port buffer pools required for Dual-MAC.

◆ ICSSG_DUALMAC_HOST_EGRESS_QUEUE_NUM

#define ICSSG_DUALMAC_HOST_EGRESS_QUEUE_NUM   (2U)

Number of host egress queues required for Dual-MAC.

◆ ICSSG_SWITCH_PORT_BUFFER_POOL_NUM

#define ICSSG_SWITCH_PORT_BUFFER_POOL_NUM   (8U)

Number of port buffer pools required for Dual-MAC.

◆ ICSSG_SWITCH_HOST_EGRESS_QUEUE_NUM

#define ICSSG_SWITCH_HOST_EGRESS_QUEUE_NUM   (2U)

Number of host egress queues required for Dual-MAC.

◆ ICSSG_HOST_EGRESS_BUFFER_PADDING

#define ICSSG_HOST_EGRESS_BUFFER_PADDING   (2048U)

Host egress queue padding size.

◆ ICSSG_SCRATCH_BUFFER_SIZE

#define ICSSG_SCRATCH_BUFFER_SIZE   (ENET_UTILS_ALIGN((2048U), ICSSG_CACHELINE_ALIGNMENT))

Size of the scratch buffer used for error frames and large frames.

◆ ICSSG_FDB_ENTRY_P0_MEMBERSHIP

#define ICSSG_FDB_ENTRY_P0_MEMBERSHIP   (ENET_BIT(0U))

Host port membership.

Indicates host port membership.

◆ ICSSG_FDB_ENTRY_P1_MEMBERSHIP

#define ICSSG_FDB_ENTRY_P1_MEMBERSHIP   (ENET_BIT(1U))

Physical port 1 membership.

Indicates that MAC ID is connected to physical port 1.

◆ ICSSG_FDB_ENTRY_P2_MEMBERSHIP

#define ICSSG_FDB_ENTRY_P2_MEMBERSHIP   (ENET_BIT(2U))

Physical port 2 membership.

Indicates that MAC ID is connected to physical port 2.

◆ ICSSG_FDB_ENTRY_AGEABLE

#define ICSSG_FDB_ENTRY_AGEABLE   (ENET_BIT(3U))

Ageable bit.

Ageable bit is set for learned entries and cleared for static entries.

◆ ICSSG_FDB_ENTRY_BLOCK

#define ICSSG_FDB_ENTRY_BLOCK   (ENET_BIT(4U))

Block bit.

If set for SA then packet is dropped (can be used to implement a blacklist). If set for DA then packet is determined to be a special packet.

◆ ICSSG_FDB_ENTRY_SECURE

#define ICSSG_FDB_ENTRY_SECURE   (ENET_BIT(5U))

Secure bit.

If set for DA then the SA from the packet is not learned.

◆ ICSSG_FDB_ENTRY_TOUCHED

#define ICSSG_FDB_ENTRY_TOUCHED   (ENET_BIT(6U))

Touched bit.

If set, it means packet has been seen recently with source address + FID matching MAC address/FID of entry.

◆ ICSSG_FDB_ENTRY_VALID

#define ICSSG_FDB_ENTRY_VALID   (ENET_BIT(7U))

Valid bit.

Set if entry is valid.

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH0

#define ICSSG_RATE_SRC_SEL_FT1_MATCH0   (0U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH1

#define ICSSG_RATE_SRC_SEL_FT1_MATCH1   (1U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH2

#define ICSSG_RATE_SRC_SEL_FT1_MATCH2   (2U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH3

#define ICSSG_RATE_SRC_SEL_FT1_MATCH3   (3U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH4

#define ICSSG_RATE_SRC_SEL_FT1_MATCH4   (4U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH5

#define ICSSG_RATE_SRC_SEL_FT1_MATCH5   (5U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH6

#define ICSSG_RATE_SRC_SEL_FT1_MATCH6   (6U)

◆ ICSSG_RATE_SRC_SEL_FT1_MATCH7

#define ICSSG_RATE_SRC_SEL_FT1_MATCH7   (7U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH0

#define ICSSG_RATE_SRC_SEL_FT3_MATCH0   (8U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH1

#define ICSSG_RATE_SRC_SEL_FT3_MATCH1   (9U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH2

#define ICSSG_RATE_SRC_SEL_FT3_MATCH2   (10U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH3

#define ICSSG_RATE_SRC_SEL_FT3_MATCH3   (11U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH4

#define ICSSG_RATE_SRC_SEL_FT3_MATCH4   (12U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH5

#define ICSSG_RATE_SRC_SEL_FT3_MATCH5   (13U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH6

#define ICSSG_RATE_SRC_SEL_FT3_MATCH6   (14U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH7

#define ICSSG_RATE_SRC_SEL_FT3_MATCH7   (15U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH8

#define ICSSG_RATE_SRC_SEL_FT3_MATCH8   (16U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH9

#define ICSSG_RATE_SRC_SEL_FT3_MATCH9   (17U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH10

#define ICSSG_RATE_SRC_SEL_FT3_MATCH10   (18U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH11

#define ICSSG_RATE_SRC_SEL_FT3_MATCH11   (19U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH12

#define ICSSG_RATE_SRC_SEL_FT3_MATCH12   (20U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH13

#define ICSSG_RATE_SRC_SEL_FT3_MATCH13   (21U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH14

#define ICSSG_RATE_SRC_SEL_FT3_MATCH14   (22U)

◆ ICSSG_RATE_SRC_SEL_FT3_MATCH15

#define ICSSG_RATE_SRC_SEL_FT3_MATCH15   (23U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_UC

#define ICSSG_RATE_SRC_SEL_FT_RX_UC   (24U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_MC

#define ICSSG_RATE_SRC_SEL_FT_RX_MC   (25U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_BC

#define ICSSG_RATE_SRC_SEL_FT_RX_BC   (26U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_SAV

#define ICSSG_RATE_SRC_SEL_FT_RX_SAV   (27U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_FWD

#define ICSSG_RATE_SRC_SEL_FT_RX_FWD   (28U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_RCV

#define ICSSG_RATE_SRC_SEL_FT_RX_RCV   (29U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_VLAN

#define ICSSG_RATE_SRC_SEL_FT_RX_VLAN   (30U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_DA_P

#define ICSSG_RATE_SRC_SEL_FT_RX_DA_P   (31U)

◆ ICSSG_RATE_SRC_SEL_FT_RX_DA_I

#define ICSSG_RATE_SRC_SEL_FT_RX_DA_I   (32U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW0

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW0   (33U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW1

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW1   (34U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW2

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW2   (35U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW3

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW3   (36U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW4

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW4   (37U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW5

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW5   (38U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW6

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW6   (39U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW7

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW7   (40U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW8

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW8   (41U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW9

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW9   (42U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW10

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW10   (43U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW11

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW11   (44U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW12

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW12   (45U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW13

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW13   (46U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW14

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW14   (47U)

◆ ICSSG_RATE_SRC_SEL_RX_CLASS_RAW15

#define ICSSG_RATE_SRC_SEL_RX_CLASS_RAW15   (48U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH0

#define ICCSG_RX_CLASS_DATA_FT3_MATCH0   (0U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH1

#define ICCSG_RX_CLASS_DATA_FT3_MATCH1   (1U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH2

#define ICCSG_RX_CLASS_DATA_FT3_MATCH2   (2U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH3

#define ICCSG_RX_CLASS_DATA_FT3_MATCH3   (3U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH4

#define ICCSG_RX_CLASS_DATA_FT3_MATCH4   (4U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH5

#define ICCSG_RX_CLASS_DATA_FT3_MATCH5   (5U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH6

#define ICCSG_RX_CLASS_DATA_FT3_MATCH6   (6U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH7

#define ICCSG_RX_CLASS_DATA_FT3_MATCH7   (7U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH8

#define ICCSG_RX_CLASS_DATA_FT3_MATCH8   (8U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH9

#define ICCSG_RX_CLASS_DATA_FT3_MATCH9   (9U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH10

#define ICCSG_RX_CLASS_DATA_FT3_MATCH10   (10U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH11

#define ICCSG_RX_CLASS_DATA_FT3_MATCH11   (11U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH12

#define ICCSG_RX_CLASS_DATA_FT3_MATCH12   (12U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH13

#define ICCSG_RX_CLASS_DATA_FT3_MATCH13   (13U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH14

#define ICCSG_RX_CLASS_DATA_FT3_MATCH14   (14U)

◆ ICCSG_RX_CLASS_DATA_FT3_MATCH15

#define ICCSG_RX_CLASS_DATA_FT3_MATCH15   (15U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH0

#define ICCSG_RX_CLASS_DATA_FT1_MATCH0   (16U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH1

#define ICCSG_RX_CLASS_DATA_FT1_MATCH1   (17U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH2

#define ICCSG_RX_CLASS_DATA_FT1_MATCH2   (18U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH3

#define ICCSG_RX_CLASS_DATA_FT1_MATCH3   (19U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH4

#define ICCSG_RX_CLASS_DATA_FT1_MATCH4   (20U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH5

#define ICCSG_RX_CLASS_DATA_FT1_MATCH5   (21U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH6

#define ICCSG_RX_CLASS_DATA_FT1_MATCH6   (22U)

◆ ICCSG_RX_CLASS_DATA_FT1_MATCH7

#define ICCSG_RX_CLASS_DATA_FT1_MATCH7   (23U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_DA_I

#define ICCSG_RX_CLASS_DATA_FT_RX_DA_I   (24U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_DA_P

#define ICCSG_RX_CLASS_DATA_FT_RX_DA_P   (25U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_VLAN

#define ICCSG_RX_CLASS_DATA_FT_RX_VLAN   (26U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_RCV

#define ICCSG_RX_CLASS_DATA_FT_RX_RCV   (27U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_FWD

#define ICCSG_RX_CLASS_DATA_FT_RX_FWD   (28U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_BC

#define ICCSG_RX_CLASS_DATA_FT_RX_BC   (29U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_MC

#define ICCSG_RX_CLASS_DATA_FT_RX_MC   (30U)

◆ ICCSG_RX_CLASS_DATA_FT_RX_SAV

#define ICCSG_RX_CLASS_DATA_FT_RX_SAV   (31U)

◆ ICSSG_TAS_MIN_CYCLE_TIME_NS

#define ICSSG_TAS_MIN_CYCLE_TIME_NS   (1000000)

Minimum cycle time supported by implementation (in ns).

◆ ICSSG_TAS_MIN_WINDOW_DURATION_NS

#define ICSSG_TAS_MIN_WINDOW_DURATION_NS   (10000)

Minimum TAS window duration supported by implementation (in ns).

Typedef Documentation

◆ Icssg_MdioLinkStateChangeCb

typedef void(* Icssg_MdioLinkStateChangeCb) (Icssg_MdioLinkStateChangeInfo *info, void *appArg)

Icssg PHY link state change callback function.

Callback for PHY link state change interrupt (MDIO_LINKINT). This callback is invoked from interrupt context.

Enumeration Type Documentation

◆ Icssg_Instance_Num

ICSSG instance numbers.

Enumerator
ICSSG_INSTANCE_NUM_0 

Instance number 0

ICSSG_INSTANCE_NUM_1 

Instance number 1

ICSSG_INSTANCE_NUM_2 

Instance number 2

◆ Icssg_Ioctl

ICSSG IOCTL commands.

Enumerator
ICSSG_MACPORT_IOCTL_ENABLE_PROMISC_MODE 

Enable promiscuous mode.

IOCTL params:

Type: Synchronous.

ICSSG_MACPORT_IOCTL_DISABLE_PROMISC_MODE 

Disable promiscuous mode.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_VLAN_RESET_TABLE 

Populate VLAN table with default VLAN entry configuration.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_VLAN_SET_ENTRY 

Update a VLAN table entry.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_VLAN_GET_ENTRY 

Get VLAN entry for VLAN table for requested VLAN id.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_SET_PORT_STATE 

Set port state.

Sets the port state in one of the following states (refer to Icssg_PortState):

  • Disabled
  • Blocking
  • Forwarding
  • Forwarding without learning
  • TAS trigger
  • TAS enable
  • TAS reset
  • TAS disable

IOCTL params:

Type: Asynchronous.

ICSSG_FDB_IOCTL_ADD_ENTRY 

Add FDB entry.

IOCTL params:

Type: Asynchronous.

ICSSG_FDB_IOCTL_REMOVE_ENTRY 

Delete FDB entry.

IOCTL params:

Type: Asynchronous.

ICSSG_FDB_IOCTL_REMOVE_ALL_ENTRIES 

Delete all FDB entries.

IOCTL params:

  • inArgs: None
  • outArgs: None

Type: Asynchronous

ICSSG_FDB_IOCTL_REMOVE_AGEABLE_ENTRIES 

Remote all ageable entries.

IOCTL params:

  • inArgs: None
  • outArgs: None

Type: Asynchronous.

ICSSG_MACPORT_IOCTL_SET_MACADDR 

Add MAC address of the interface.

IOCTL params:

Type: Synchronous.

ICSSG_HOSTPORT_IOCTL_SET_MACADDR 

Add MAC address of the host port interface.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_TAS_TRIGGER 
ICSSG_PER_IOCTL_TAS_ENABLE 
ICSSG_PER_IOCTL_TAS_DISABLE 
ICSSG_PER_IOCTL_TAS_RESET 
ICSSG_PER_IOCTL_VLAN_SET_HOSTPORT_DFLT_VID 

Set the default VLAN ID and PCP bits for host port.

Sets the default VLAN ID and PCP bits for host port. Only the VID and PCP fields from the passed VLAN configuration are valid, the CFI bit is ignored.

IOCTL params:

Type: Synchronous.

ICSSG_PER_IOCTL_VLAN_SET_MACPORT_DFLT_VID 

Set the default VLAN ID and PCP bits for specified MAC port.

IOCTL params:

Type: Synchronous.

ICSSG_FDB_IOCTL_SET_AGING_PERIOD 

Set the aging period of the FDB.

Sets the FDB aging period in nanoseconds.

IOCTL params:

  • inArgs: uint64_t
  • outArgs: None

Type: Synchronous.

ICSSG_MACPORT_IOCTL_ENABLE_UCAST_FLOOD 

Enable flooding of unicast packets to host port.

IOCTL params:

Type: Asynchronous.

ICSSG_MACPORT_IOCTL_DISABLE_UCAST_FLOOD 

Disable flooding of unicast packets to host port.

IOCTL params:

Type: Asynchronous.

ICSSG_MACPORT_IOCTL_ENABLE_MCAST_FLOOD 

Enable flooding of multicast packets to host port.

IOCTL params:

Type: Asynchronous.

ICSSG_MACPORT_IOCTL_DISABLE_MCAST_FLOOD 

Disable flooding of multicast packets to host port.

IOCTL params:

Type: Asynchronous.

ICSSG_MACPORT_IOCTL_SET_ACCEPT_FRAME_CHECK 

Set the criteria for accepting VLAN tagged/untagged packets.

Sets the accept criteria to:

  • Accept only VLAN tagged frames
  • Accept only untagged and priority tagged frames
  • Accept all frames (default configuration)

IOCTL params:

Type: Synchronous.

ICSSG_MACPORT_IOCTL_SET_INGRESS_RATE_LIM 

Configure ingress rate limiting.

IOCTL params:

Type: Synchronous.

ICSSG_MACPORT_IOCTL_SET_QUEUE_CUT_THROUGH_PREEMPT_SELECT 

cut through or prempt select configuration.

IOCTL params:

Type: Synchronous.

ICSSG_MACPORT_IOCTL_CONFIG_SPL_FRAME_PRIO 

special frame priority configuration.

IOCTL params:

Type: Synchronous.

ICSSG_INTERNAL_IOCTL_REGISTER_HANDLER 

Register Handler for the IOCTL CMD.

IOCTL params:

  • inArgs: IcssgInternalIoctlHandlerTableEntry_t
  • outArgs: None

Type: Synchronous.

◆ Icssg_QueuePreemptMode

Queue preemptive mode: express or preemptive.

Enumerator
ICSSG_QUEUE_PREEMPT_MODE_EXPRESS 

Express queue

ICSSG_QUEUE_PREEMPT_MODE_PREEMPT 

Preemptive queue

◆ Icssg_QueueForwardMode

Queue forward mode: cut-through or store-and-forward.

Enumerator
ICSSG_QUEUE_FORWARD_MODE_STOREANDFWD 

Store-and-forward queue

ICSSG_QUEUE_FORWARD_MODE_CUTTHROUGH 

Cut-through queue

◆ Icssg_PortState

Port states.

Enumerator
ICSSG_PORT_STATE_DISABLED 

Disabled state. No frames can be sent or received, but there can be a link.

ICSSG_PORT_STATE_BLOCKING 

Blocking state. At the port, only sync/management frames are sent or received (e.g. gPTP, LLDP, MRP)

ICSSG_PORT_STATE_FORWARD 

Forwarding state. Forward frames as per MC/Stream/Static Registration FDB. Learning is enabled for frames received locally.

ICSSG_PORT_STATE_FORWARD_WO_LEARNING 

Forwarding without learning state.

ICSSG_PORT_STATE_TAS_TRIGGER 

TAS trigger state

ICSSG_PORT_STATE_TAS_ENABLE 

TAS enable state

ICSSG_PORT_STATE_TAS_RESET 

TAS reset state

ICSSG_PORT_STATE_TAS_DISABLE 

TAS disable state

◆ Icssg_AcceptFrameCheck

Acceptable frame check criteria.

Enumerator
ICSSG_ACCEPT_ONLY_VLAN_TAGGED 

Accept only VLAN-tagged frames

ICSSG_ACCEPT_ONLY_UNTAGGED_PRIO_TAGGED 

Accept only untagged or priority-tagged frames

ICSSG_ACCEPT_ALL 

Accept all frames

Function Documentation

◆ EnetCb_GetFwPoolMem()

const Icssg_FwPoolMem* EnetCb_GetFwPoolMem ( Enet_Type  enetType,
uint32_t  instId 
)

ICSSG memory pool callback function.

Initializes the ICSSG memory pool callback function.

Parameters
enetTypeEnet Peripheral type
instIdInstance Number

◆ IcssgMacPort_initCfg()

void IcssgMacPort_initCfg ( IcssgMacPort_Cfg macPortCfg)

Initialises Mac Port COnfiguration.

Gets Application configuration related to ICSSG.

Parameters
macPortCfgPointer to ICSSG mac port configuration structure

◆ Icssg_getSliceNum()

uint32_t Icssg_getSliceNum ( Enet_Type  enetType,
uint32_t  instId,
Enet_MacPort  macPort 
)

ICSSG memory pool callback function.

Initializes the ICSSG memory pool callback function.

Parameters
enetTypeEnet Peripheral type
instIdInstance Number
macPortEnet Mac Port
ENET_IOCTL_PER_BASE
@ ENET_IOCTL_PER_BASE
Definition: enet_ioctl.h:239