AM263x MCU+ SDK  09.00.00
enet_base.h File Reference

Introduction

This file contains the type definitions and helper macros for the Enet Peripheral interface.

Go to the source code of this file.

Data Structures

struct  Enet_Obj
 Enet object. More...
 

Macros

#define ENET_FEAT_ALL   (0xFFFFFFFFU)
 Feature mask which indicates that all of the configurable features are enabled. More...
 
#define ENET_FEAT_BASE   (0x00000000U)
 Feature masks which indicates that none of the configurable features are enabled. More...
 
#define ENET_FEAT_IS_EN(feats, mask)   (((feats) & (mask)) != 0U)
 Check if a configurable feature is enabled or not. More...
 
#define ENET_ERRATA_NONE   (0x00000000U)
 Errata mask which indicates that none of the erratas is applicable. More...
 
#define ENET_ERRATA_IS_ANY(mask)   ((mask) != ENET_ERRATA_NONE)
 Check if any errata is applicable, from an errata mask. More...
 
#define ENET_ERRATA_IS_EN(erratas, mask)   (((erratas) & (mask)) != 0U)
 Check if an errata is applicable. More...
 

Typedefs

typedef struct Enet_Obj_s * Enet_Handle
 Ethernet driver handle. More...
 

Functions

static EnetPer_Handle Enet_getPerHandle (Enet_Handle hEnet)
 Get the Enet Peripheral handle associated with Enet driver. More...
 

Macro Definition Documentation

◆ ENET_FEAT_ALL

#define ENET_FEAT_ALL   (0xFFFFFFFFU)

Feature mask which indicates that all of the configurable features are enabled.

◆ ENET_FEAT_BASE

#define ENET_FEAT_BASE   (0x00000000U)

Feature masks which indicates that none of the configurable features are enabled.

◆ ENET_FEAT_IS_EN

#define ENET_FEAT_IS_EN (   feats,
  mask 
)    (((feats) & (mask)) != 0U)

Check if a configurable feature is enabled or not.

◆ ENET_ERRATA_NONE

#define ENET_ERRATA_NONE   (0x00000000U)

Errata mask which indicates that none of the erratas is applicable.

◆ ENET_ERRATA_IS_ANY

#define ENET_ERRATA_IS_ANY (   mask)    ((mask) != ENET_ERRATA_NONE)

Check if any errata is applicable, from an errata mask.

◆ ENET_ERRATA_IS_EN

#define ENET_ERRATA_IS_EN (   erratas,
  mask 
)    (((erratas) & (mask)) != 0U)

Check if an errata is applicable.

Typedef Documentation

◆ Enet_Handle

typedef struct Enet_Obj_s* Enet_Handle

Ethernet driver handle.

Ethernet driver opaque handle used to call any Enet related APIs.

Function Documentation

◆ Enet_getPerHandle()

static EnetPer_Handle Enet_getPerHandle ( Enet_Handle  hEnet)
inlinestatic

Get the Enet Peripheral handle associated with Enet driver.

Gets the underlying Enet Peripheral handle associated with the given Enet driver.

Parameters
hEnetEnet handle
Returns
EthPer handle