DCL_PID object for storing PID specific parameters.
Data Fields | |
float32_t | Kp |
Proportional gain. More... | |
float32_t | Ki |
Integral gain. More... | |
float32_t | Kd |
Derivative gain. More... | |
float32_t | Kr |
Set point weight, default is 1. More... | |
float32_t | c1 |
D path filter coefficient 1, default is 1. More... | |
float32_t | c2 |
D path filter coefficient 2, default is 0. More... | |
float32_t | Umax |
Upper saturation limit. More... | |
float32_t | Umin |
Lower saturation limit More... | |
float32_t | d2 |
D path feedback value (Kd * c1) More... | |
float32_t | d3 |
D path feedback value (c2) More... | |
float32_t | i10 |
I path feedback value. More... | |
float32_t | i14 |
I path saturation storage. More... | |
DCL_PID_SPS * | sps |
updates controller parameter More... | |
DCL_CSS * | css |
configuration & debugging More... | |
float32_t dcl_pid::Kp |
Proportional gain.
float32_t dcl_pid::Ki |
Integral gain.
float32_t dcl_pid::Kd |
Derivative gain.
float32_t dcl_pid::Kr |
Set point weight, default is 1.
float32_t dcl_pid::c1 |
D path filter coefficient 1, default is 1.
float32_t dcl_pid::c2 |
D path filter coefficient 2, default is 0.
float32_t dcl_pid::Umax |
Upper saturation limit.
float32_t dcl_pid::Umin |
Lower saturation limit
float32_t dcl_pid::d2 |
D path feedback value (Kd * c1)
float32_t dcl_pid::d3 |
D path feedback value (c2)
float32_t dcl_pid::i10 |
I path feedback value.
float32_t dcl_pid::i14 |
I path saturation storage.
DCL_PID_SPS* dcl_pid::sps |
updates controller parameter
DCL_CSS* dcl_pid::css |
configuration & debugging