DCL_DF11 object for storing df11 specific parameters.
Data Fields | |
float32_t | b0 |
pos. coefficient to e(k) More... | |
float32_t | b1 |
pos. coefficient to e(k-1) More... | |
float32_t | a1 |
neg. coefficient to u(k-1) More... | |
float32_t | d1 |
e(k-1) More... | |
float32_t | d2 |
u(k-1) More... | |
DCL_DF11_SPS * | sps |
Pointer to the shadow parameter set. More... | |
DCL_CSS * | css |
Pointer to the common support structure. More... | |
float32_t dcl_df11::b0 |
pos. coefficient to e(k)
float32_t dcl_df11::b1 |
pos. coefficient to e(k-1)
float32_t dcl_df11::a1 |
neg. coefficient to u(k-1)
float32_t dcl_df11::d1 |
e(k-1)
float32_t dcl_df11::d2 |
u(k-1)
DCL_DF11_SPS* dcl_df11::sps |
Pointer to the shadow parameter set.
DCL_CSS* dcl_df11::css |
Pointer to the common support structure.