Defines the 64bit CSS structure.
Data Fields | |
float64_t | tpt |
Test point. More... | |
float64_t | t_sec |
Controller period in seconds. More... | |
volatile uint32_t | sts |
Status word. More... | |
uint32_t | err_line |
Error location line (errno) More... | |
uint32_t | err |
Error status code. More... | |
const char * | err_func |
Error function name. More... | |
float64_t DCL_CSSF64::tpt |
Test point.
float64_t DCL_CSSF64::t_sec |
Controller period in seconds.
volatile uint32_t DCL_CSSF64::sts |
Status word.
uint32_t DCL_CSSF64::err_line |
Error location line (errno)
uint32_t DCL_CSSF64::err |
Error status code.
const char* DCL_CSSF64::err_func |
Error function name.