IO-Link Master Types.
IO-Link definitions for Master and Device.
Data Structures | |
| struct | IOL_SDirectParam1 |
| This structure stores the Direct Parameter Page 1. More... | |
| struct | IOL_SEventEntry |
| This structure defines a event buffer entry. More... | |
Macros | |
| #define | NULL ((void*)0) |
| #define | FALSE ((TBOOL)0) |
| #define | TRUE ((TBOOL)1) |
Enumerations | |
| enum | IOL_ETransferMode { IOL_eTransferMode_INACTIVE = 0 , IOL_eTransferMode_COM1 , IOL_eTransferMode_COM2 , IOL_eTransferMode_COM3 , IOL_eTransferMode_DI , IOL_eTransferMode_DO } |
| This enumeration indicates the requested operation mode. More... | |
| enum | IOL_EODLen { IOL_eODLen_1_Byte = 0 , IOL_eODLen_2_Byte , IOL_eODLen_8_Byte , IOL_eODLen_32_Byte } |
| This enumeration indicates the number of OD bytes in M-sequence. | |
| enum | IOL_ETransferStatus { IOL_eTransferStatus_OK , IOL_eTransferStatus_PARITY_ERROR , IOL_eTransferStatus_FRAMING_ERROR , IOL_eTransferStatus_OVERRUN } |
| This enumeration contains supplementary information on the transfer. status. More... | |
| enum | IOL_EErrorInfo { IOL_eErrorInfo_NONE = 0 , IOL_eErrorInfo_NO_COMM , IOL_eErrorInfo_STATE_CONFLICT , IOL_eErrorInfo_PARAMETER_CONFLICT , IOL_eErrorInfo_TIMING_CONFLICT , IOL_eErrorInfo_NO_DATA , IOL_eErrorInfo_VALUE_OUT_OF_RANGE , IOL_eErrorInfo_ISDU_TIMEOUT , IOL_eErrorInfo_ISDU_NOT_SUPPORTED , IOL_eErrorInfo_TIMEOUT } |
| This enumeration contains error information. More... | |
| enum | IOL_EComChannel { IOL_eComChannel_PROCESS = 0x00 , IOL_eComChannel_PAGE = 0x20 , IOL_eComChannel_DIAGNOSIS = 0x40 , IOL_eComChannel_ISDU = 0x60 } |
| This enumeration indicates the communication channel for the access to the user data. | |
| enum | IOL_EDirection { IOL_eDirection_WRITE = 0x00 , IOL_eDirection_READ = 0x80 } |
| This enumeration contains ISDU transport direction. More... | |
| enum | IOL_EDLMode { IOL_eDLMode_INACTIVE = 0 , IOL_eDLMode_STARTUP , IOL_eDLMode_PREOPERATE , IOL_eDLMode_OPERATE , IOL_eDLMode_UNPAIRING } |
| This enumeration indicates the requested mode of the Master's DL on an individual port. More... | |
| enum | IOL_EDLRealMode { IOL_eDLRealMode_INACTIVE = 0 , IOL_eDLRealMode_COM1 , IOL_eDLRealMode_COM2 , IOL_eDLRealMode_COM3 , IOL_eDLRealMode_COMLOST , IOL_eDLRealMode_ESTABCOM , IOL_eDLRealMode_ACTIVE , IOL_eDLRealMode_STARTUP , IOL_eDLRealMode_PREOPERATE , IOL_eDLRealMode_OPERATE , IOL_eDLRealMode_INVALID } |
| This enumeration indicates the status of the DL-mode handler. More... | |
| enum | IOL_EMSequence { IOL_eMSequence_TYPE_0 = 0 , IOL_eMSequence_TYPE_1 = 0x40 , IOL_eMSequence_TYPE_2 = 0x80 , IOL_eMSequence_TYPE_MASK = 0xC0 } |
| This enumeration contains the M-sequence types. More... | |
| enum | IOL_EPDInStatus { IOL_ePDInStatus_VALID = 0 , IOL_ePDInStatus_INVALID = 0x40 } |
| This enumeration indicates the qualifier status of the Process Data (PD). More... | |
| enum | IOL_EPDOutStatus { IOL_ePDOutStatus_PDOUTVALID = 0 , IOL_ePDOutStatus_PDOUTINVALID , IOL_ePDOutStatus_RTFAULT } |
| This enumeration indicates the qualifier status of the Process Data (PD). More... | |
| enum | IOL_EMHInfo { IOL_eMHInfo_COMLOST = 0 , IOL_eMHInfo_ILLEGAL_MESSAGETYPE , IOL_eMHInfo_CHECKSUM_MISMATCH } |
| This enumeration contains the exception indication of the message handler. More... | |
| enum | IOL_ETargetMode { IOL_eTargetMode_INACTIVE = 0 , IOL_eTargetMode_DI , IOL_eTargetMode_DO , IOL_eTargetMode_CFGCOM , IOL_eTargetMode_AUTOCOM , IOL_eTargetMode_COM1 , IOL_eTargetMode_COM2 , IOL_eTargetMode_COM3 , IOL_eTargetMode_OSSDE , IOL_eTargetMode_SAFETYCOM } |
| This enumeration indicates the requested operational mode of the port. More... | |
| enum | IOL_EIQMode { IOL_eIQMode_INACTIVE = 0 , IOL_eIQMode_IN , IOL_eIQMode_OUT } |
| This enumeration indicates the requested IQ mode of the port. More... | |
| enum | IOL_EBaudrate { IOL_eBaudrate_AUTO = 0 , IOL_eBaudrate_COM1 , IOL_eBaudrate_COM2 , IOL_eBaudrate_COM3 } |
| This enumeration indicates the transmission rate. More... | |
| enum | IOL_EPortMode { IOL_ePortMode_INACTIVE = 0 , IOL_ePortMode_DI , IOL_ePortMode_DO , IOL_ePortMode_COMREADY , IOL_ePortMode_READY_TO_OPERATE , IOL_ePortMode_SM_OPERATE , IOL_ePortMode_COMLOST , IOL_ePortMode_REVISION_FAULT , IOL_ePortMode_COMP_FAULT , IOL_ePortMode_SERNUM_FAULT , IOL_ePortMode_DS_FAULT , IOL_ePortMode_CYCTIME_FAULT , IOL_ePortMode_PORTPOWEROFF } |
| This enumeration indicates changes or faults of the local communication mode. More... | |
| enum | IOL_EDeviceMode { IOL_eDeviceMode_INACTIVE = 0 , IOL_eDeviceMode_IDLE , IOL_eDeviceMode_SIO , IOL_eDeviceMode_ESTABCOM , IOL_eDeviceMode_COMx , IOL_eDeviceMode_STARTUP , IOL_eDeviceMode_IDENT_STARTUP , IOL_eDeviceMode_IDENT_CHANGE , IOL_eDeviceMode_PREOPERATE , IOL_eDeviceMode_OPERATE , IOL_eDeviceMode_PAIRING , IOL_eDeviceMode_TIMEOUT , IOL_eDeviceMode_TEMPORARY , IOL_eDeviceMode_PERMANENT , IOL_eDeviceMode_PAIRED , IOL_eDeviceMode_UNPAIRED , IOL_eDeviceMode_UNPAIRING } |
| This enumeration indicates changes of communication states to the Device application. More... | |
| enum | IOLD_EWDeviceMode { IOLD_eWDeviceModeMode_INACTIVE = 0 , IOLD_eWDeviceModeMode_STARTUP = 1 , IOLD_eWDeviceModeMode_IDENT_STARTUP = 2 , IOLD_eWDeviceModeMode_IDENT_CHANGE = 3 , IOLD_eWDeviceModeMode_PREOPERATE = 4 , IOLD_eWDeviceModeMode_OPERATE = 5 } |
| This enumeration indicates changes of communication states to the WDevice. | |
| enum | IOL_EIService { IOL_eIService_NO_SERVICE = 0 , IOL_eIService_WR_REQ_8B_IDX , IOL_eIService_WR_REQ_8B_IDX_SIDX , IOL_eIService_WR_REQ_16B_IDX_SIDX , IOL_eIService_WR_RES_NOK , IOL_eIService_WR_RES_OK , IOL_eIService_RESERVED_1 , IOL_eIService_RESERVED_2 , IOL_eIService_RESERVED_3 , IOL_eIService_RD_REQ_8B_IDX , IOL_eIService_RD_REQ_8B_IDX_SIDX , IOL_eIService_RD_REQ_16B_IDX_SIDX , IOL_eIService_RD_RES_NOK , IOL_eIService_RD_RES_OK , IOL_eIService_RESERVED_4 , IOL_eIService_RESERVED_5 } |
| This enumeration defines the I-Services of the ISDU. | |
| enum | IOL_EDirectParam { IOL_eDirectParam_MasterCommand = 0 , IOL_eDirectParam_MasterCycleTime , IOL_eDirectParam_MinCycleTime , IOL_eDirectParam_MSequenceCapability , IOL_eDirectParam_RevisionID , IOL_eDirectParam_ProcessDataIn , IOL_eDirectParam_ProcessDataOut , IOL_eDirectParam_VendorID1 , IOL_eDirectParam_VendorID2 , IOL_eDirectParam_DeviceID1 , IOL_eDirectParam_DeviceID2 , IOL_eDirectParam_DeviceID3 , IOL_eDirectParam_FunctionID1 , IOL_eDirectParam_FunctionID2 , IOL_eDirectParam_Reserved , IOL_eDirectParam_SystemCommand , IOL_eDirectParam_MAX } |
| This enumeration is a index list of the Direct Parameter Page 1. | |
| enum | IOL_EMasterCommand { IOL_eMasterCommand_Fallback = 0x5A , IOL_eMasterCommand_Inactive = 0x5C , IOL_eMasterCommand_PreDLink = 0x5D , IOL_eMasterCommand_FullDLink = 0x5E , IOL_eMasterCommand_Unpairing = 0x5F , IOL_eMasterCommand_MasterIdent = 0x95 , IOL_eMasterCommand_DeviceIdent = 0x96 , IOL_eMasterCommand_DeviceStartup = 0x97 , IOL_eMasterCommand_ProcessDataOutputOperate = 0x98 , IOL_eMasterCommand_DeviceOperate = 0x99 , IOL_eMasterCommand_DevicePreoperate = 0x9A , IOL_eMasterCommand_Jump_0 = 0xF0 , IOL_eMasterCommand_Jump_1 = 0xF1 , IOL_eMasterCommand_Jump_2 = 0xF2 , IOL_eMasterCommand_Jump_3 = 0xF3 , IOL_eMasterCommand_Jump_4 = 0xF4 , IOL_eMasterCommand_Jump_5 = 0xF5 , IOL_eMasterCommand_Jump_6 = 0xF6 , IOL_eMasterCommand_Jump_7 = 0xF7 , IOL_eMasterCommand_Jump_8 = 0xF8 , IOL_eMasterCommand_Jump_9 = 0xF9 , IOL_eMasterCommand_Jump_10 = 0xFA , IOL_eMasterCommand_Jump_11 = 0xFB , IOL_eMasterCommand_Jump_12 = 0xFC , IOL_eMasterCommand_Jump_13 = 0xFD , IOL_eMasterCommand_Jump_14 = 0xFE , IOL_eMasterCommand_WakeUp = 0xFF } |
| This enumeration indicates the Master Commands. | |
| enum | IOL_EISDUIndex { IOL_eISDUIndex_DirectParam1 = 0 , IOL_eISDUIndex_DirectParam2 = 1 , IOL_eISDUIndex_SystemCommand = 2 , IOL_eISDUIndex_DataStorage = 3 , IOL_eISDUIndex_DeviceAccessLocks = 12 , IOL_eISDUIndex_ProfileCharacteristic = 13 , IOL_eISDUIndex_PDInputDescriptor = 14 , IOL_eISDUIndex_PDOutputDescriptor = 15 , IOL_eISDUIndex_VendorName = 16 , IOL_eISDUIndex_VendorText = 17 , IOL_eISDUIndex_ProductName = 18 , IOL_eISDUIndex_ProductID = 19 , IOL_eISDUIndex_ProductText = 20 , IOL_eISDUIndex_SerialNumber = 21 , IOL_eISDUIndex_HardwareRevision = 22 , IOL_eISDUIndex_FirmwareRevision = 23 , IOL_eISDUIndex_AppSpecificTag = 24 , IOL_eISDUIndex_FunctionTag = 25 , IOL_eISDUIndex_LocationTag = 26 , IOL_eISDUIndex_ErrorCount = 32 , IOL_eISDUIndex_DeviceStatus = 36 , IOL_eISDUIndex_DetailedDeviceStatus = 37 , IOL_eISDUIndex_ProcessDataInput = 40 , IOL_eISDUIndex_ProcessDataOutput = 41 , IOL_eISDUIndex_WDeviceMode = 0x5000 , IOL_eISDUIndex_WirelessSystemMgmnt = 0x5001 , IOL_eISDUIndex_WirelessSystemCfg = 0x5002 , IOL_eISDUIndex_LinkQuality = 0x5003 , IOL_eISDUIndex_WBridgeInfo = 0x5004 , IOL_eISDUIndex_WirelessRadioInfo = 0x5005 , IOL_eISDUIndex_AdaptiveHopTable = 0x5006 , IOL_eISDUIndex_WCycleTime = 0x5007 } |
| This enumeration indicates the predefined index values for ISDU. | |
| enum | IOL_EErrorType { IOL_eErrorType_NONE = 0 , IOL_eErrorType_APP_DEV = 0x8000 , IOL_eErrorType_IDX_NOTAVAIL = 0x8011 , IOL_eErrorType_SUBIDX_NOTAVAIL = 0x8012 , IOL_eErrorType_SERV_NOTAVAIL = 0x8020 , IOL_eErrorType_SERV_NOTAVAIL_LOCCTRL = 0x8021 , IOL_eErrorType_SERV_NOTAVAIL_DEVCTRL = 0x8022 , IOL_eErrorType_IDX_NOT_WRITEABLE = 0x8023 , IOL_eErrorType_PAR_VALOUTOFRNG = 0x8030 , IOL_eErrorType_PAR_VALGTLIM = 0x8031 , IOL_eErrorType_PAR_VALLTLIM = 0x8032 , IOL_eErrorType_VAL_LENOVRRUN = 0x8033 , IOL_eErrorType_VAL_LENUNDRUN = 0x8034 , IOL_eErrorType_FUNC_NOTAVAIL = 0x8035 , IOL_eErrorType_FUNC_UNAVAILTEMP = 0x8036 , IOL_eErrorType_PAR_SETINVALID = 0x8040 , IOL_eErrorType_PAR_SETINCONSIST = 0x8041 , IOL_eErrorType_APP_DEVNOTRDY = 0x8082 , IOL_eErrorType_UNSPECIFIC = 0x8100 , IOL_eErrorType_VENDOR_SPECIFIC_BEGIN = 0x8101 , IOL_eErrorType_VENDOR_SPECIFIC_END = 0x81FF , IOL_eErrorType_COM_ERR = 0x1000 , IOL_eErrorType_I_SERVICE_TIMEOUT = 0x1100 , IOL_eErrorType_M_ISDU_CHECKSUM = 0x5600 , IOL_eErrorType_M_ISDU_ILLEGAL = 0x5700 , IOL_eErrorType_ARGBLOCK_NOT_SUPPORTED = 0x4001 , IOL_eErrorType_ARGBLOCK_INCONSISTENT = 0x4002 , IOL_eErrorType_DEVICE_NOT_ACCESSIBLE = 0x4003 , IOL_eErrorType_SERVICE_NOT_SUPPORTED = 0x4004 , IOL_eErrorType_DEVICE_NOT_IN_OPERATE = 0x4005 , IOL_eErrorType_MEMORY_OVERRUN = 0x4006 , IOL_eErrorType_PORT_NUM_INVALID = 0x4011 , IOL_eErrorType_ARGBLOCK_LENGTH_INVALID = 0x4034 , IOL_eErrorType_SERVICE_TEMP_UNAVAILABLE = 0x4036 , IOL_eErrorType_INCONSISTENT_DS_DATA = 0x4039 , IOL_eErrorType_ACCESS_RIGHT_NOT_GRANTED = 0x4042 } |
| This enumeration indicates the permissible ISDU ErrorTypes resulting from the Device application. More... | |
| enum | IOL_EECode { IOL_eECode_NO_MALFUNCTION = 0x0000 , IOL_eECode_GENERAL_MALFUNCTION = 0x1000 , IOL_eECode_TEMP_FAULT = 0x4000 , IOL_eECode_TEMP_OVERRUN = 0x4210 , IOL_eECode_TEMP_UNDERRUN = 0x4220 , IOL_eECode_HW_FAULT = 0x5000 , IOL_eECode_COMP_MALFUNCTION = 0x5010 , IOL_eECode_MEM_LOSS = 0x5011 , IOL_eECode_BATTERIES_LOW = 0x5012 , IOL_eECode_SUPPLY_FAULT = 0x5100 , IOL_eECode_FUSE_OPEN = 0x5101 , IOL_eECode_SUPPLY_OVERRUN = 0x5110 , IOL_eECode_SUPPLY_UNDERRUN = 0x5111 , IOL_eECode_SEC_SUPPLY_FAULT = 0x5112 , IOL_eECode_SW_FAULT = 0x6000 , IOL_eECode_PARAM_ERROR = 0x6320 , IOL_eECode_PARAM_MISSING = 0x6321 , IOL_eECode_PARAM_CHANGED = 0x6350 , IOL_eECode_WIRE_BREAK = 0x7700 , IOL_eECode_WIRE_BREAK_D1 = 0x7701 , IOL_eECode_WIRE_BREAK_D2 = 0x7702 , IOL_eECode_WIRE_BREAK_D3 = 0x7703 , IOL_eECode_WIRE_BREAK_D4 = 0x7704 , IOL_eECode_WIRE_BREAK_D5 = 0x7705 , IOL_eECode_WIRE_BREAK_D6 = 0x7706 , IOL_eECode_WIRE_BREAK_D7 = 0x7707 , IOL_eECode_WIRE_BREAK_D8 = 0x7708 , IOL_eECode_WIRE_BREAK_D9 = 0x7709 , IOL_eECode_WIRE_BREAK_D10 = 0x770A , IOL_eECode_WIRE_BREAK_D11 = 0x770B , IOL_eECode_WIRE_BREAK_D12 = 0x770C , IOL_eECode_WIRE_BREAK_D13 = 0x770D , IOL_eECode_WIRE_BREAK_D14 = 0x770E , IOL_eECode_WIRE_BREAK_D15 = 0x770F , IOL_eECode_SHORT_CIRCUIT = 0x7710 , IOL_eECode_GROUND_FAULT = 0x7711 , IOL_eECode_APP_FAULT = 0x8C00 , IOL_eECode_SIM_ACTIVE = 0x8C01 , IOL_eECode_PD_OVERRUN = 0x8C10 , IOL_eECode_MEASUREMENT_OVERRUN = 0x8C20 , IOL_eECode_PD_UNDERRUN = 0x8C30 , IOL_eECode_MAINT_CLEANING = 0x8C40 , IOL_eECode_MAINT_REFILL = 0x8C41 , IOL_eECode_MAINT_EXCHANGE = 0x8C42 , IOL_eECode_EVENT = 0xFF31 , IOL_eECode_DS_UPLOAD_REQ = 0xFF91 , IOL_eECode_IOLW_RETRY_ERROR_R = 0xFFB0 , IOL_eECode_IOLW_HMI_BUTTON_PRESS = 0xFFB1 } |
| This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP). More... | |
| enum | IOL_EEPortCode { IOL_eEPortCode_NoDevice = 0x1800 , IOL_eEPortCode_StartupParamError = 0x1801 , IOL_eEPortCode_IncorrectVendorId = 0x1802 , IOL_eEPortCode_IncorrectDeviceId = 0x1803 , IOL_eEPortCode_ShortCircuit = 0x1804 , IOL_eEPortCode_PhyOvertemperature = 0x1805 , IOL_eEPortCode_ShortCircuitLP = 0x1806 , IOL_eEPortCode_OvercurrentAtLp = 0x1807 , IOL_eEPortCode_DeviceEventOverflow = 0x1808 , IOL_eEPortCode_BackupMemOutOfRange = 0x1809 , IOL_eEPortCode_BackupIdentityFault = 0x180A , IOL_eEPortCode_BackupUnspecificError = 0x180B , IOL_eEPortCode_BackupUploadFault = 0x180C , IOL_eEPortCode_BackupDownloadFault = 0x180D , IOL_eEPortCode_P24MissingUndervoltage = 0x180E , IOL_eEPortCode_ShortCircuitP24 = 0x180F , IOL_eEPortCode_ShortCircuitIQ = 0x1810 , IOL_eEPortCode_ShortCircuitAtCQ = 0x1811 , IOL_eEPortCode_OvercurrentIQ = 0x1812 , IOL_eEPortCode_OvercurrentCQ = 0x1813 , IOL_eEPortCode_EvalExpired = 0x1F00 , IOL_eEPortCode_Overload = 0x1F01 , IOL_eEPortCode_InvalidCycleTime = 0x6000 , IOL_eEPortCode_RevisionFault = 0x6001 , IOL_eEPortCode_ISDUBatchFailed = 0x6002 , IOL_eEPortCode_NEW_SLAVE = 0xFF21 , IOL_eEPortCode_DEV_COM_LOST = 0xFF22 , IOL_eEPortCode_DS_IDENT_MISMATCH = 0xFF23 , IOL_eEPortCode_DS_BUFFER_OVERFLOW = 0xFF24 , IOL_eEPortCode_DS_ACCESS_DENIED = 0xFF25 , IOL_eEPortCode_PortStatusChanged = 0xFF26 , IOL_eEPortCode_DataStorageComplete = 0xFF27 , IOL_eEPortCode_IncorectEventSignalling = 0xFF31 , IOL_eEPortCode_IOLW_RETRY_ERROR_L = 0x3000 , IOL_eEPortCode_IOLW_IMA_TIMEOUT = 0x3001 , IOL_eEPortCode_IOLW_U_ID_CHANGED = 0x3002 } |
| This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP). More... | |
| enum | IOL_EEInstance { IOL_eEInstance_UNKNOWN = 0 , IOL_eEInstance_PHY , IOL_eEInstance_DL , IOL_eEInstance_AL , IOL_eEInstance_APPLICATION , IOL_eEInstance_SYSTEM , IOL_eEInstance_RESERVED_5 , IOL_eEInstance_RESERVED_6 } |
| This enumeration indicates the particular source (instance) of an event thus refining its evaluation on the receiver side. More... | |
| enum | IOL_EESource { IOL_eESource_DEVICE = 0 , IOL_eESource_MASTER } |
| This enumeration indicates the source of the event. More... | |
| enum | IOL_EEType { IOL_eEEType_RESERVED = 0 , IOL_eEEType_NOTIFICATION , IOL_eEEType_WARNING , IOL_eEEType_ERROR } |
| This enumeration indicates the event category. More... | |
| enum | IOL_EEMode { IOL_eEEMode_RESERVED = 0 , IOL_eEEMode_SINGLE_SHOT , IOL_eEEMode_DISAPPEARS , IOL_eEEMode_APPEARS } |
| This enumeration indicates the event mode. More... | |
| enum | IOL_EDSCommand { IOL_eDSCommand_Reserved = 0 , IOL_eDSCommand_UploadStart , IOL_eDSCommand_UploadEnd , IOL_eDSCommand_DownloadStart , IOL_eDSCommand_DownloadEnd , IOL_eDSCommand_Break } |
| This enumeration indicates the DS commands. | |
| enum | IOL_ESystemCommand { IOL_eSystemCommand_Reserved = 0 , IOL_eSystemCommand_UploadStart , IOL_eSystemCommand_UploadEnd , IOL_eSystemCommand_DownloadStart , IOL_eSystemCommand_DownloadEnd , IOL_eSystemCommand_DownloadEndStore , IOL_eSystemCommand_Break , IOL_eSystemCommand_BM_UNLOCK_S = 80 , IOL_eSystemCommand_BM_UNLOCK_F = 81 , IOL_eSystemCommand_BM_UNLOCK_T = 82 , IOL_eSystemCommand_BM_ACTIVATE = 83 , IOL_eSystemCommand_LocatorStart = 126 , IOL_eSystemCommand_LocatorStop = 127 , IOL_eSystemCommand_DeviceReset = 128 , IOL_eSystemCommand_ApplicationReset = 129 , IOL_eSystemCommand_RestoreFactorySettings = 130 , IOL_eSystemCommand_BackToBox = 131 } |
| This enumeration indicates the predefined system commands. | |
| enum | IOL_ESlotType { IOL_eSlotType_SSLOT = 0 , IOL_eSlotType_DSLOT = 1 } |
| Physical layer slot types. | |
| enum | IOL_ESlotLenType { IOL_eSlotLength_SSLOT = 1 , IOL_eSlotLength_DSLOT = 14 } |
| Physical layer slot length. | |
| enum IOL_EBaudrate |
This enumeration indicates the transmission rate.
| Enumerator | |
|---|---|
| IOL_eBaudrate_AUTO | Master accepts transmission rate found during IOL_eDLRealMode_ESTABCOM "ESTABLISHCOM". |
| IOL_eBaudrate_COM1 | Transmission rate of COM1 (4,8 kbit/s). |
| IOL_eBaudrate_COM2 | Transmission rate of COM2 (38,4 kbit/s). |
| IOL_eBaudrate_COM3 | Transmission rate of COM3 (230,4 kbit/s). |
| enum IOL_EDeviceMode |
This enumeration indicates changes of communication states to the Device application.
| enum IOL_EDirection |
| enum IOL_EDLMode |
This enumeration indicates the requested mode of the Master's DL on an individual port.
| enum IOL_EDLRealMode |
This enumeration indicates the status of the DL-mode handler.
| enum IOL_EECode |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP).
| enum IOL_EEInstance |
This enumeration indicates the particular source (instance) of an event thus refining its evaluation on the receiver side.
| enum IOL_EEMode |
| enum IOL_EEPortCode |
This enumeration lists the specified EventCode identifiers and their definitions. The EventCodes are created by the technology specific Device application (instance = APP).
| enum IOL_EErrorInfo |
This enumeration contains error information.
| enum IOL_EErrorType |
This enumeration indicates the permissible ISDU ErrorTypes resulting from the Device application.
| enum IOL_EESource |
| enum IOL_EEType |
| enum IOL_EIQMode |
| enum IOL_EMHInfo |
| enum IOL_EMSequence |
This enumeration contains the M-sequence types.
TYPE_1_1 forces interleave mode of process and On-request Data transmission, see 7.3.4.2 of IO-Link Specification v1.1.3.
| enum IOL_EPDInStatus |
| enum IOL_EPDOutStatus |
This enumeration indicates the qualifier status of the Process Data (PD).
| enum IOL_EPortMode |
This enumeration indicates changes or faults of the local communication mode.
| enum IOL_ETargetMode |
This enumeration indicates the requested operational mode of the port.
| enum IOL_ETransferMode |
This enumeration indicates the requested operation mode.
| enum IOL_ETransferStatus |
This enumeration contains supplementary information on the transfer. status.