Welcome to Motor Control SDK for AM261X. This SDK contains examples, libraries, and tools to develop RTOS and no-RTOS based applications for real-time motor control on the Arm® Cortex®-R5F CPU and related peripherals. It includes position sense examples and real-time control library examples.
Real-time communication with encoders is typically handled by the Programmable Real-Time Unit Industrial Communication Subsystem (PRU-ICSS). The PRU-ICSS is a co-processor subsystem containing Programmable Real-Time (PRU) cores that implement the low-level firmware. The PRU-ICSS frees up the main Arm-based cores in the device for other functions, such as control and data processing.
Applications and PRU-ICSS firmwares for position sense are provided in the SDK.
To get started, see GETTING STARTED page.
Given below is a block diagram of the software modules in this SDK
The main software components in the block diagram specific to motor control are described below
| Software Components | Documentation Page | Description |
|---|---|---|
| Position Sense Encoders | ||
| BISS-C | BISS-C | Driver and PRU-ICSS firmware for BISS-C encoder interface |
| EnDat | EnDat | Driver and PRU-ICSS firmware for EnDat encoder interface |
| HDSL | HDSL | Driver and PRU-ICSS firmware for Hiperface DSL encoder interface |
| Nikon A-format | Nikon A-format | Driver and PRU-ICSS firmware for Nikon A-format encoder interface |
| Tamagawa | Tamagawa | Driver and PRU-ICSS firmware for Tamagawa encoder interface |
| Real Time Libraries | ||
| Control algorithms | Control algorithms | Library for control algorithms and techniques used in motors such as PMSM and BLDC |
| Datalog | Datalog | Library for storing the real time values of user selectable variables |
| Digital Control Library (DCL) | Digital Control Library (DCL) | Header-only library for digital control applications |
| Observer algorithms | Observer algorithms | Header-only library for encoder/observer algorithms used in both sensored/sensorless field oriented control (FOC) |
| Software Frequency Response Analyzer | Software Frequency Response Analyzer | Library that enables developers to quickly measure the frequency response of their digital power converter. |
| Transforms | Transformation Algorithm | Transformation including Clarke, Park, Space Vector Generation used in motor control applications. |
| Examples and Demos | ||
| Examples and Demos | Examples and Demos | Examples and demos showing usage of different SW libraries and APIs for motor control |
For details on software components of Industrial Communications SDK and MCU+ SDK, please refer to AM261X Industrial Communications SDK and AM261X MCU+ SDK respectively.
Given below is an overview of the directory structure to help you navigate the SDK and related tools.
| Folder/Files | Description |
|---|---|
| ${SDK_INSTALL_PATH}/ | |
| README_FIRST_AM261X.html | Open this file in a web browser to reach this user guide |
| makefile | Top level makefile to build the whole SDK using "make" |
| imports.mak | Top level makefile to list paths to dependent tools |
| docs/ | Offline browseable HTML documentation |
| examples/ | Example applications for AM261X, across multiple boards |
| source/ | Device drivers, middleware libraries and APIs |
Given below are the paths where the different tools needed outside the SDK, like CCS, SysConfig are installed by default in Windows. In Linux, the tools are installed by default in ${HOME}/ti.
| Folder/Files | Description |
|---|---|
| C:/ti/ccs20.3.0 | Code Composer Studio |
| C:/ti/sysconfig_1.25.0 | SysConfig. NOTE, SysConfig is also installed as part of CCS at ${CCS_INSTALL_PATH}/ccs/utils/sysconfig_x.x.x |
| C:/ti/ti-cgt-armllvm_4.0.3.LTS | TI ARM CLANG compiler tool chain |
The licensing information of this SDK, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest.
A complete manifest along with export control information is detailed in "${SDK_INSTALL_PATH}/docs/manifest.html" file.
For additional help and support, see https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum
This user guide is generated using Doxygen, v1.8.20. See https://www.doxygen.nl/index.html