Introduction
The HDSL firmware running on ICSS-PRU provides a well-defined interface to execute the HDSL protocol.
- Note
- This implementation using Peripheral input/output mode of PRU-ICSS. Refer Peripheral IF mode for more details.
Features Supported
- Safe position
- Fast position, speed
- Communication status
- External pulse synchronization using IEP CAP (capture) event
- 1 to 10 frames per cycle
- 8 kHz to 50 kHz cycle frequency
- Uses IEP CAP6 for PRU slice 1 and CAP7 for PRU slice 0 (NOTE: CAP6 and CAP7 support falling edge detection as well. In HDSL, rising edge is used always.)
- Register interface to be compatible with SICK HDSL FPGA IP Core (apart from the differences listed in TI HDSL Exceptions List)
- Parameter channel communication
- Short message
- Long message
- Safety
- Pipeline Channel Data
- Single channel support (with PRU Core Clock frequency of 225 MHz) per PRU
- Cores used: PRU0/PRU1
- Two channel example and one channel example on LP-AM261 (tested on ICSSM1 instance and PRU0/PRU1)
- Tested with three different encoder makes (EDM35, EKS36, EKM36)
Features Not Supported
In general, peripherals or features not mentioned as part of the "Features Supported" section are not supported, including the below:
- 100m cable
- Pipeline Channel Status
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- Attention
- For each PRU-ICSS slice being used for HDSL, one module instance should be created in SysConfig. For dual channel example using 2 PRUs, 2 instances need to be added.
SysConfig can be used to configure the following:
- Selecting the ICSSM instance (Tested on ICSSM1)
- Selecting the ICSSM PRU slice (Tested on ICSSM1-PRU0 and ICSSM1-PRU1)
- Configuring PINMUX
- Channel selection
- Mode Selection (Free Run / Sync mode)
- Booster Pack Support: Enable when using BP-AM2BLDCSERVO
- Note
- HDSL firmware supports operation with PRU-ICSS Core Clock running at 225 MHz only due to clock divider requirements.
PRU-ICSS Resource Usage
- Utilizes the Peripheral IF mode (3-channel peripheral interface mode) for HDSL communication. Maximum of 3 channels are available per PRU slice. (Refer Peripheral IF mode for more details)
- Each channel has 4 pins (Clock, Data out, Data in, Output enable)
- Following table contains details of memory usage, IEP usage and interrupt controller usage:
- Attention
- In addition to the following resources used by PRU firmware, SDK examples also configure ICSSM0 IEP0 CMP1 for generating SYNC OUT0 used as sync pulse input.
| Configuration per slice | PRU Core | Memory Usage | IEP Usage | Interrupt Controller (INTC) Usage | Description |
| Single channel | PRUx | DMEM: 1773 Bytes: 256B for HDSL Registers (0x0 to 0xFF) + 1517B for LUTs (0x100 to 0x6EC)
IMEM: ~ 7.6 kB (For Sync mode. For Free Run mode, less IMEM is used) | IEP0: CAP7 (slice 0) or CAP6 (slice 1) | INTC events/inputs numbers 16, 18, 19, 20, 21, 22 (pr[0/1]_pru_mst_intr[0/2/3/4/5/6]_intr_req) are used to trigger interrupts to Arm® Cortex®-R5F for EVENT, V-frame, H-frame, EVENT_S and H-frame respectively | IEP CAP event is used for external pulse synchronization in Sync mode only |
- Note
- For pin usage, see Pin Multiplexing section.
HDSL Design
HDSL Protocol Design explains the design in detail.
Register List
TI HDSL Register List contains the description of registers in TI's HDSL implementation.
Exceptions
TI HDSL Exceptions List lists the exceptions in TI's HDSL implementation when compared with SICK HDSL FPGA IP Core. Please note that not all the corresponding register fields are implemented, and see the description of register for more details.
Datasheet
Synchronization Pulse Jitter
- Synchronization Pulse Jitter is under 100ns. Please refer to the image below for jitter calculation waveforms.
HDSL Sync mode waveforms for 2 channels
HDSL Sync mode jitter analysis
Protocol Package Lengths with different ES and Sync Pulse Frequency values
NOTE: Images below show TX_EN signal in "Red" and RX signal in "Yellow".
| ES Value | Cycle Time (in us) | Cycle Frequency (in kHz) | Observed Protocol Package Length (in us) |
| 1 | 25 | 40 | 25.06 |
| 1 | 20 | 50 | 19.942 |
| 2 | 25 | 40 | Between 12.26 and 12.80 |
| 5 | 62.5 | 16 | Between 11.94 and 12.60 |
| 10 | 125 | 8 | Between 11.94 and 12.90 |
Example
HDSL Diagnostic
API
APIs for HDSL Encoder
- Note
- Arm is a registered trademark of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.