AM261x MCU+ SDK  10.02.00
Ram_DevConfig Struct Reference

Data Fields

uint8_t cmdRd
 
uint8_t cmdWr
 
uint8_t cmdReset
 
uint8_t cmdRegRd
 
uint8_t cmdRegWr
 
uint8_t dummyClksRd
 
uint8_t dummyClksWr
 
uint8_t dummyClksCmd
 

Field Documentation

◆ cmdRd

uint8_t Ram_DevConfig::cmdRd

◆ cmdWr

uint8_t Ram_DevConfig::cmdWr

◆ cmdReset

uint8_t Ram_DevConfig::cmdReset

◆ cmdRegRd

uint8_t Ram_DevConfig::cmdRegRd

◆ cmdRegWr

uint8_t Ram_DevConfig::cmdRegWr

◆ dummyClksRd

uint8_t Ram_DevConfig::dummyClksRd

◆ dummyClksWr

uint8_t Ram_DevConfig::dummyClksWr

◆ dummyClksCmd

uint8_t Ram_DevConfig::dummyClksCmd