AM261x INDUSTRIAL COMMUNICATIONS SDK  10.02.00
icss_timeSync_utils.h File Reference

Go to the source code of this file.

Functions

void TimeSync_addWord (uint8_t *src, uint32_t word)
 Add a word to the packet stream. More...
 
void TimeSync_addHalfWord (volatile uint8_t *src, uint16_t halfWord)
 Add a half word to the packet stream. More...
 
uint32_t TimeSync_calcChecksum (uint8_t *packet, uint16_t len)
 Compute checksum used in IP/UDP packets for a given stream. More...
 
void TimeSync_calcIPChecksum (uint8_t *packet)
 Compute checksum for IP Header and modify in place. More...
 
void TimeSync_convEndianess (volatile void *src, volatile void *dst, uint8_t numBytes)
 Convert specified number of bytes in source from big endian bytes to little endian and vice versa. Assumption : More...
 
void TimeSync_convEnd6to8 (volatile void *src, void *dst)
 Takes in a 6 byte reverse byte endian source and puts it in an 64 bit double word with correct endianness. This function is specific to PTP Assumption : More...
 
uint32_t TimeSync_getIEPCountValue (TimeSync_ParamsHandle_t timeSyncHandle)
 Returns the IEP Count value based on the IEP Clock Frequency. More...
 
uint32_t TimeSync_prepareIEPCfgCommand (TimeSync_ParamsHandle_t timeSyncHandle, compensationType compType)
 Returns a prepared command for the IEP Global CFG Register. More...