AM261x Motor Control SDK  10.02.00
APIs for Voltage Frequency Generator (VS_FREQ)

Introduction

Here is the list of VS_FREQ function APIs

Files

file  vs_freq.h
 Contains the public interface to the stator voltage frequency generator (VS_FREQ)
 

Data Structures

struct  VS_FREQ_Handle
 Defines the angle generator (ANGLE_COMP) object. More...
 

Functions

static float32_t VS_FREQ_getVd_out (VS_FREQ_Handle handle)
 Gets the Vd output value in VS_FREQ. More...
 
static float32_t VS_FREQ_getVq_out (VS_FREQ_Handle handle)
 
static void VS_FREQ_setMaxFreq (VS_FREQ_Handle handle, float32_t maxFreq)
 Sets the parameters maximum frequency. More...
 
static void VS_FREQ_setVsMagPu (VS_FREQ_Handle handle, float32_t maxVsMag_pu)
 Sets the parameters VsMag_pu. More...
 
void VS_FREQ_setProfile (VS_FREQ_Handle handle, float32_t LowFreq, float32_t HighFreq, float32_t VoltMin, float32_t VoltMax)
 Sets the parameters. More...
 
VS_FREQ_Handle VS_FREQ_init (void *pMemory, const size_t numBytes)
 Initializes the angle generator (VS_FREQ) module. More...
 
static void VS_FREQ_run (VS_FREQ_Handle handle, const float32_t Freq_pu)
 Generates an output command voltage for a specific input command frequency according to the specified volts/hertz profile. More...
 

Function Documentation

◆ VS_FREQ_getVd_out()

static float32_t VS_FREQ_getVd_out ( VS_FREQ_Handle  handle)
inlinestatic

Gets the Vd output value in VS_FREQ.

Parameters
[in]handleThe volts/hertz (VS_FREQ) handle
Returns
The Vd output value in VS_FREQ, pu

◆ VS_FREQ_getVq_out()

static float32_t VS_FREQ_getVq_out ( VS_FREQ_Handle  handle)
inlinestatic
Parameters
[in]handleThe volts/hertz profile (VS_FREQ) handle
Returns
The Vq output value in VS_FREQ, pu

◆ VS_FREQ_setMaxFreq()

static void VS_FREQ_setMaxFreq ( VS_FREQ_Handle  handle,
float32_t  maxFreq 
)
inlinestatic

Sets the parameters maximum frequency.

Parameters
[in]handleThe volts/hertz profile (VS_FREQ) handle
[in]maxFreqThe maixmum frequency for volts/hertz profile, Hz

◆ VS_FREQ_setVsMagPu()

static void VS_FREQ_setVsMagPu ( VS_FREQ_Handle  handle,
float32_t  maxVsMag_pu 
)
inlinestatic

Sets the parameters VsMag_pu.

Parameters
[in]handleThe volts/hertz profile (VS_FREQ) handle
[in]maxVsMag_puThe maixmum magintude for volts/hertz profile, pu

◆ VS_FREQ_setProfile()

void VS_FREQ_setProfile ( VS_FREQ_Handle  handle,
float32_t  LowFreq,
float32_t  HighFreq,
float32_t  VoltMin,
float32_t  VoltMax 
)

Sets the parameters.

Parameters
[in]handleThe volts/hertz profile (VS_FREQ) handle
[in]LowFreqThe low frequency for volts/hertz profile, Hz
[in]HighFreqThe high frequency for volts/hertz profile, Hz
[in]VoltMinThe minimum frequency for volts/hertz profile, Volts
[in]VoltMaxThe maximum frequency for volts/hertz profile, Volts

◆ VS_FREQ_init()

VS_FREQ_Handle VS_FREQ_init ( void *  pMemory,
const size_t  numBytes 
)

Initializes the angle generator (VS_FREQ) module.

Parameters
[in]pMemoryA pointer to the memory for the object
[in]numBytesThe number of bytes allocated for the object, bytes\
Returns
The volts/hertz profile (VS_FREQ) object handle

◆ VS_FREQ_run()

static void VS_FREQ_run ( VS_FREQ_Handle  handle,
const float32_t  Freq_pu 
)
static

Generates an output command voltage for a specific input command frequency according to the specified volts/hertz profile.

Parameters
[in]handleThe volts/hertz profile (VS_FREQ) handle
[in]Freq_puThe input frequency in pu