AM243x Motor Control SDK  11.00.00
SDFM Interface Design

Introduction

This design implements Sigma delta interface on TI Sitara™ processors using PRU-ICSS. ICSS SDFM is a Sigma delta filter for phase current measurement. Only two lines are required for each channel, a differential pair each for SDFM clock & SDFM data. Clock is provided by an external device or internal device and data comes from a sigma delta modulator in the form of a digital bit stream.

System Overview

Implementation

The Sigma delta filter is implemented on TI Sitara™ processors using PRU-ICSS.

The design is split into three parts:

  1. Sigma delta hardware support in PRU
  2. Firmware running in PRU
  3. Driver running in Arm®-based core

Applications are supposed to use the ICSS SDFM driver APIs to leverage SDFM functionality. The SDK example uses the SDFM hardware capability in Slice 1 of PRU-ICSSG0.

Specifications

Parameter Default Value Details
Normal Current Over-sampling Ratio (OSR) 64 Tested with 8, 16, 32, 64, 128, and 256
Over Current OSR 16 Tested with 8, 16, 32, 64, 128 and 256
SINC Filter Types SINC3 Tested with SINC1, SINC2 and SINC3
Clock Source Common clock source for all nine channels Tested with: Independent clock source for each channel, Shared clock source for three channels and Common clock source for all nine channels.
SDFM Clock generation source ICSSG eCAP ICSSG PRU GPO1, ICSSG eCAP and ICSSG IEP
Sigma Delta Modulator Clock 20 MHz Tested with 5MHz, 10MHz and 20MHz clock from PRU-ICSSG ECAP and 5MHz clock from SoC EPWM1
Simulated EPWM frequency 8 KHz Tested up to 20KHz
IEP frequency 300 MHz Tested with 200MHz, 225MHz and 300MHz

ICSS SDFM PRU hardware

Refer to section 6.4.5.2.2.3.5 Sigma Delta (SD) Decimation Filtering in Technical Reference Manual(TRM) of AM243x for details.

ICSS SDFM Firmware Implementation

Following section describes the firmware implementation of Sigma Delta Decimation Filter on PRU-ICSS.

Firmware Architecture

Overall Block Diagram
  • Firmware first clears the PRU registers and task manager.
  • Next if phase compensation is enabled, it measures phase delay
  • Then it waits for the Arm-based core to set SDFM enable bit. After the enable bit is set, it sends an acknowledgement to Arm-based core.
  • After this, the firmware does initialization of PRU-ICSSG's SDFM hardware interface, task manager and IEP0.
  • SDFM Firmware has two approaches to do sampling:
    1. Normal Mode: It reads sample data from the accumulator shadow register when the sample ready flag is active.
    2. Snoop Mode: It reads sample data directly from the accumulator and the desired one sample timing is achieved by using the IEP CMP event.
  • Normal Mode:
    • Continuous Mode: It performs continuous sampling for all three channels independently. Each channel store sample in memory and generates an independent R5F event when sample is ready. It also performs over-current comparison if the sample values cross the threshold range, It triggers the PRU-ICSS PWM trip.
    • Trigger Mode: It starts the sampling when a CMP event is hit. First, it clears all accumulator and differentiation registers. Then it starts sampling for all three channels. It performs continuous SINC filter order times sampling for all three channels. Once the sampling is done for all channels, it store samples in memory and triggers a R5F interrupt.
      Firmware flow chart for normal mode
  • Snoop Mode:
    • If threshold comparator is enabled, then a free run over current loop is setup, else it sets up an infinite waiting loop. In over current loop, the firmware reads sample data from the shadow copy register and does low and high threshold comparison with sample data, and depending on the configuration it generates over current trip in PRU-ICSS PWM trip zone block. Also if zero cross detection is enabled, it detects zero cross.
    • Time triggered normal current task is configured to be triggered based on IEP CMP event. When the CMP event hits, the task manager sets the program counter to normal current task. In normal current task, firmware reads sample data from accumulator and it checks for fourth normal current sample (for SINC3 filtering). If the current normal current sample belongs to fourth normal current sample, then it stores the same in data memory DMEM as normal current raw data and triggers interrupt.
    • At the end of normal current firmware task, execution flow comes into infinite waiting loop or over current loop.

Normal Current (NC)

This section describes normal current implementation for snoop mode.

There are two different variations of normal current.

  • Trigger based: It starts execution when the trigger point is acquired (first time CMP event hits) and performs four continuous samplings to bring the accumulator and differentiator registers to stable state for the configured normal current OSR. Initially the CMP register is configured with the first sample trigger start time and then until the next third continuous normal current sample it is updated with the normal current OSR sampling time. At the end of the fourth normal current sample again, it is updated with the second sample start time if double update is enabled otherwise with the first sample trigger start time.
  • Continuous sampling: It starts execution when the first time CMP event hits. Every time it updates CMP event register with the normal current OSR sampling time for next continuous sample, stores sample values in DMEM and triggers R5F interrupt.
Normal Current
Single Update

Normal current sampling is done per EPWM cycle.

Single Update
Double Update

Normal current sampling is done twice in one EPWM cycle.

Double Update

Over Current (OC)/Threshold Comparator

This section describes the over current implementation. It performs continuous sampling (free run) and when the sample value crosses the high or low threshold, the corresponding PWM trip status gets set and TZ_OUT pin goes high. It also stores high and low threshold status in DMEM for all channels, SDFM_getHighThresholdStatus API returns high threshold status for specified SDFM channel number and SDFM_getLowThresholdStatus API returns low threshold status for specified SDFM channel number.

Over current
Mapping between Over current errors and PRU-ICSS PWM TZ blocks

Note: Not supported for Normal Mode based sampling when Normal Current trigger mode is used

Zero Cross Comparator

This section describes the zero cross implementation. It compares the current sample and the previous sample values with zero cross threshold value.

There are two cases:

  • Current sample value is greater than zero cross threshold value: If the latest previous sample value is less than the zc threshold value, it changes the direction of the corresponding GPIO pin from low to high otherwise keeps the GPIO in the same direction.
  • Current sample value is less than zero cross threshold value: If the latest previous sample value is greater than the zc threshold value, it changes the direction of the corresponding GPIO pin from high to low otherwise keeps the GPIO in the same direction.
Zero cross
Zero cross GPIO behaviour

Note: Supported only for Snoop Mode based sampling

Sync with EPWM and trigger timing

This section describes the EPWM to SDFM synchronization and trigger timing for each EPWM cycle. At the end of every EPWM cycle, the EPWM generates a sync out event that resets the IEP timer. The firmware initiates normal current sampling at the sample trigger point in each EPWM cycle. It takes four consecutive samples to bring the accumulator and differentiator registers to stable state. It takes the first sample at the trigger point and the next three samples, each after ONE_SAMPLE_TIME. Here ONE_SAMPLE_TIME is: OSR*(1/SD_CLK)

Sync with EPWM and trigger timing

Fast Detect and Trip generation

The Fast Detect block is used for fast over current detection. It comparatively measures the number of zeros and ones presented in a programmable sliding window of 4 to 32 bits. It starts the comparison after the first 32 sample clocks. Based on the configured zero max/min count limits, it compares zero counter with these limits. If zero counter crosses limit, then it sends an error signal to respective PRU-ICSS PWM Trip zone block. PWM TZ block receives this error signal and sets trip status bit to bring TZ_OUT pin output state to high.

Note: To identify the sigma delta fast detect error trip cause, SDFM_getFastDetectErrorStatus API can be used and to clear the PRU-ICSS PWM trip status, SDFM_clearPwmTripStatus API can be used.

Mapping between Fast detect errors and PWM TZ blocks

Note: Channels 6 to 8 Fast Detect is not mapped with any PRU-ICSS PWM trip zone block. This is a hardware limitation.

Data/Clock Phase Compensation

Following points describe the process for measurement of phase difference between clock and data

  • Set PRU IO mode to GPIO mode (default) for direct capture of input data and clock pins
  • First wait for rising edge on the SD data pin, then check the nearest upcoming edge to the SD clock pin. If the nearest edge of clock pin is falling, then it measures the time between the rising edge of the data pin and the falling edge of the SD clock. Otherwise it measures time between the rising edge of both data and clock pins.
  • It measures the delay 8 times and repeats the measurements until it obtains either identical values or values that vary by no more than 1 PRU cycle for 8 iterations.
  • Based on the clock polarity, phase delay is calculated. If clock polarity and upcoming nearest edge of clock pin for rising edge of data pin are same, then final phase delay will be half SD clock duty cycle time minus calculated time. Otherwise phase delay will be SD clock one cycle period time minus calculated time
    Phase Compensation

Fast Detect trip through PRU firmware

This section describes an alternative method to generate EPWM trips for fast detect errors using PRU firmware. This approach can be implemented as shown in the corresponding flowchart. It requires one PRU core to trigger a task when an overcurrent or fast detect error event occurs. Within this task, an EPWM software trip can be generated by setting the One-Shot Trip Event bit in the EPWM trip zone register.

Fast detect EPWM trip

Assembly code for EPWM0 trip

; Constants for memory-mapped registers
.define PADMMR_UNLOCK1 0x43005008
.define PADMMR_UNLOCK2 0x4300500c
.define EALLOW_REG 0x43004140
.define INT_CLEAR_REG 0x30020024
.define EPWM0_FORCE_REG 0x23000030
; Unlock PADMMR config register (Partition 1)
LDI32 r0, PADMMR_UNLOCK1 ; Load address
LDI32 r1, 0x68EF3490 ; Load unlock key 1
SBBO r1, r0, 0, 4 ; Store value to address
LDI32 r0, PADMMR_UNLOCK2 ; Load address
LDI32 r1, 0xD172BC5A ; Load unlock key 2
SBBO r1, r0, 0, 4 ; Store value to address
; Enable EALLOW - access to EPWM trip registers
LDI32 r0, EALLOW_REG ; Load address
LDI r1, 0x0010 ; Load value
SBBO r1, r0, 0, 2 ; Store 16-bit value
tm_trip_EPWM:
; Clear interrupt for event 110
LDI32 r0, INT_CLEAR_REG ; Load address
LDI r1, 63 ; Load value
SBBO r1, r0, 0, 1 ; Store 8-bit value
; Trip EPWM0 single shot in EPWM0 FORCE register
LDI32 r0, EPWM0_FORCE_REG ; Load address
LDI r1, 0x0004 ; Load value
SBBO r1, r0, 0, 2 ; Store 16-bit value
XIN TM_YIELD_XID, &R0.b3, 1 ; exit task after two instructions/cycles
NOP
NOP

<sdk-install-dir>/mcu_plus_sdk/examples/pru_io/empty> empty project can be used to write your own project for EPWM trip zone. You can modify this example to write your own firmware. <sdk-install-dir>/mcu_plus_sdk/examples/pru_io/> contains some PRU projects which can act as reference. PRU sources are usually separated out in a firmware/ subfolder in all these example project folders. To change the core in project properties, you can develop firmware for other PRU cores.

  • Fast Detect Error Event: The Fast Detect block generates the sd_fd_zero/one_max/min(of 72) PRU internal event upon detecting an error. This event can be routed to the PRU Task Manager via INTC channel/host. setup route: Event 63 sd_fd_zero/one_max/min(of 72) -> INTC channel/host 12 -> task manager
  • PRU Fast Detect to EPWM trip:
    • Max Latency is ~ 278 ns
    • PRU Interrupt latency: 32 ns
    • Interconnect jitter ~ 80 ns

AM64x/AM243x EVM Pin Multiplexing

Pin name Signal name Function
GPIO_ZC_TH_CH0 MCU_SPI0_D1/B6 Ch0 High threshold output
GPIO_ZC_TH_CH1 MCU_SPI1_CS0/A7 Ch1 High threshold output
GPIO_ZC_TH_CH2 MCU_SPI1_D1/C8 Ch2 High threshold output
SD0_D PIN_PRG0_PRU0_GPO1 Channel0 data input
SD1_D PIN_PRG0_PRU0_GPO3 Channel1 data input
SD2_D PIN_PRG0_PRU0_GPO5 Channel2 data input
PRG0_ECAP0_IN_APWM_OUT PIN_PRG0_PRU1_GPO15 ECAP output frequency
GPIO_MTR_1_PWM_EN GPMC0_AD15/Y20 Enable EPWM0 on 3-axis board
SD8_CLK PIN_PRG0_PRU0_GPO16 Common SDFM clock input pin

LP-AM243 Pin Multiplexing

Pin name Signal name Function
GPIO_ZC_TH_CH0 PRG1_PRU0_GPO18 (J7.64)Ch0 Zero cross output
GPIO_ZC_TH_CH1 PRG0_PRU1_GPO2 (J7.65)Ch1 Zero cross output
GPIO_ZC_TH_CH2 PRG0_PRU1_GPO1 (J7.67)Ch2 Zero cross output
SD0_D PIN_PRG0_PRU0_GPO1 (J4.32)Channel0 data input
SD1_D PIN_PRG0_PRU0_GPO3 (J2.19)Channel1 data input
SD2_D PIN_PRG0_PRU0_GPO5 (J2.13)Channel2 data input
PRG0_ECAP0_IN_APWM_OUT PIN_PRG0_PRU1_GPO15 (J6.59)ECAP output frequency
SD8_CLK PIN_PRG0_PRU0_GPO16 (J1.7)Common SDFM clock input pin
PWM0_TZ_OUT PIN_PRG0_PRU0_GPO19 (J5.45)TZ output pin for Axis-1
PWM1_TZ_OUT PIN_PRG0_PRU1_GPO19 (J8.76)TZ output pin for Axis-2
PWM2_TZ_OUT PIN_PRG0_PRU1_GPO8 (J6.57)TZ output pin for Axis-3
PRG0_IEP0_EDC_SYNC_OUT0 PIN_PRG0_PRU0_GPO19 (J5.45)SYNC_OUT0
PRG0_IEP0_EDC_SYNC_OUT1 PIN_PRG0_PRU0_GPO17 (J2.18) SYNC_OUT1
Note
Arm is a registered trademark of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.