These examples demonstrate both trigger-based and continuous normal current sampling. The examples support Normal Current, Over Current, and Fast Detect configurations.
There are three different examples based on the number of SDFM channels and the mode of Normal Current sampling.
Note: Normal Current trigger mode examples do not support Over Current.
Only one core, PRU, is used for these examples.
The load share mode of PRU-ICSSG is enabled for this example. Three cores—RTU-PRU, PRU, and TX-PRU—are used.
| Folder/Files | Description |
|---|---|
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_three_channel_single_pru_mode | Application specific sources for ICSS SDFM for trigger based normal current sampling for three channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_nine_channel_with_continuous_mode | Application specific sources for ICSS SDFM for continuous normal current sampling for nine channels |
| ${SDK_INSTALL_PATH}/examples/current_sense/icss_sdfm_three_channel_with_continuous_mode | Application specific sources for ICSS SDFM for continuous normal current sampling for three channels |
| ${SDK_INSTALL_PATH}/examples/current_sense | Common source for ICSS SDFM applications |
| ${SDK_INSTALL_PATH}/source/current_sense/sdfm | |
| firmware/ | Folder containing ICSS SDFM firmware sources |
| driver/ | ICSS SDFM driver source |
| include/ | Folder containing ICSS SDFM structures and APIs declarations |
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 freertos |
| ICSSG | ICSSG0 |
| PRU | PRU0 (single channel) |
| PRU0, RTU-PRU0, TXPRU0 (multi channel using three PRUs - load share mode) | |
| Toolchain | ti-arm-clang |
| Board | am243x-evm, am243x-lp |
| Examples folder | examples/current_sense |
Other than the basic EVM setup mentioned in EVM Setup , the additional hardware listed below is required to run this demo
| Test Details | Steps | Pass/Fail Criteria |
|---|---|---|
| 1. Normal current sample data for trigger mode | 1. Run example on supported board | The drawn graph and raw data should look like the attached image |
| 2. Draw the graph of sdfm_ch_samples array |
NC sample data | |
| 2. Normal current sample data for continuous mode | 1. Run example on supported board | The drawn graph and raw data should look like the attached image |
| 2. Draw the graph of raw the graph of sdfm_ch_samples array |
NC sample data | |
| 3. To check raw data for Single Update (64 Normal Current (NC) OSR) | 1. Set NC OSR to 64 | The drawn graph and raw data should look like the attached image |
| 2. Set single update trigger time to half of EPWM cycle time | ||
| 3. Build and run example | ||
| 4. Draw graph for Raw data |
Single Update Raw data | |
| 4. To check Raw data for Double Update | 1. Set NC OSR to 64 | The drawn graphs and raw data should look like the attached image |
| 2. Enable double update | ||
| 3. Set single update trigger time to 1/4 of EPWM cycle time | ||
| 4. Set double update trigger time to 3/4 of EPWM cycle time | ||
| 5. Build and run example | ||
| 6. Draw graph for Raw data |
Double Update Raw data | |
The pattern of the graph should be different from the single update graph. It takes 2 samples in one EPWM cycle so the graph pattern should look more like a sine wave compared to the single update graph | ||
| 5. To test SINC1/SINC2/SINC3 filter | 1. Set NC OSR to 64 | Raw data should have different resolution for different SINC filter |
| 2. Set accumulator source to SINC1/SINC2/SINC3 | SINC3 raw data resolution = OSR *(SINC2 raw data resolution) = OSR*OSR*(SINC1 raw data resolution) | |
| 3. Build and run example | ||
| 6. To check Threshold comparator and Over current for continuous mode example | 1. Enable Comparator filter | Trip status bit must be set for the respective pwm trip zone block and TZ_OUT pin must be high |
| 2. Set High Threshold to 3500 and low threshold to 2500 (low and high threshold values should be configured based on raw data resolution for 16 OSR) | ||
| 3. Set Over current and Normal current OSR to 16 | High Low Threshold status bits must be constantly unset and set | |
| 4. Probe PWMm_TZ_OUT pin | ||
| 5. Build and run example | ||
| 6. Capture signal in Logic analyzer | Trip must be triggered for the respective pwm trip zone block | |
| 7. To check NC Samples with Different NC OSR Values | 1. Set NC OSR values between 8 to 256 | Raw data should have different resolution for different OSR values |
| 2. Build and run example | ||
| 3. Observe resolution of raw data | ||
| 8. To check NC samples with different sdfm clock values | 1. Set NC OSR to 64 | Raw data range should not exceed the OSR limits |
| 2. Set ecap_divider variable in sdfm_example.c file for different sd clock generation | ||
| 3. Set Sigma delta clock equal to ecap generated clock | ||
| 4. Build and run example | ||
| 5. Observe resolution of raw data | ||
| 9. To check Fast detect | 1. Set NC OSR to 64 | Trip must be triggered for the respective pwm trip zone block |
| 2. Enable Fast detect and disable Comparator | ||
| 3. Set Fast Detect fields with these values { window size = 4, Zero max = 18, Zero min = 2} | Zero max/min Threshold hit bits must be constantly unset and set | |
| 4. Build and run example | One max/min threshold hit bits must be unset | |
| 5. 1) Observe TZ_OUT PIN. 2) Check zero/one count max & zero/one count min threshold hit bits in memory map | ||
| 10.Testing with sdfm clock from EPWM | 1. Make hardware setup like attached image | All test case results should match with ECAP test case results |
2.
SDFM: HW set for clock from EPWM | ||
| 3. Enable "APP_EPWM1_ENABLE" macro in app_sdfm.c file | ||
| 4. Set EPWM1 output frequency to 12.5MHz or 5MHz in app_sdfm.c file | ||
| 5. Set Sigma delta clock equal to EPWM1 output frequency | ||
| 6. Build and run example | ||
| 7. Test all test cases from 1 to 5 with EPWM clock | ||
| 11. To test EPWM Synchronization source | 1. Set synchronization source to EPWM3 | All test cases should work properly |
| 2. Set NC OSR to 64 | The drawn graph and raw data should look like the attached image | |
| 3. Set single update trigger time to half of EPWM cycle time | ||
| 4. Add and configure EPWM3 instance in SysConfig | ||
| 5. Build and run example | ||
| 6. Draw graph for Raw data |
Single Update Raw data | |
| 12. To test SDFM clock generation from eCAP | 1. Set SDCLK Generation From to eCAP | |
| 2. SDFM Clock to 20MHz | Generated clock should come out on PRGx_ECAP0_IN_APWM_OUT signal | |
| 3. Configure PRGx_ECAP0_IN_APWM_OUT pin inside PRU ICSSG ECAP SysConfig module | ||
| 4. Build and run example | ||
| 13. To test SDFM clock generation from ICSSG PRU GPO1 | 1. Set SDCLK Generation From to PRU-ICSSG (PRG<k>_PRU1/0_GPI1) | |
| 2. SDFM Clock to 20MHz | Generated clock should come out on PRG<k>_PRU1/0_GPI1 signal | |
| 3. Build and run example | ||
| 14. To test SDFM clock generation from IEP | 1. Set SDCLK Generation From to IEP | |
| 2. SDFM Clock to 20MHz | Generated clock should come out on two pins corresponding to SYNC0 and SYNC1 | |
| 3. Configure SYNC_OUT0 and SYNC_OUT0 pins inside PRU ICSSG IEP SysConfig module | ||
| 4. Build and run example |