AM243x Motor Control SDK  11.00.00
APIs for Nikon A-Format Encoder

Introduction

Here is the list of APIs used for Nikon A-Format encoder communication protocol

Functions

int32_t nikon_command_wait (struct nikon_priv *priv)
 Wait till PRU finishes Nikon transaction. More...
 
int32_t nikon_get_pos (struct nikon_priv *priv, uint32_t cmd)
 Get single cycle Nikon position data. More...
 
void nikon_config_clock (struct nikon_priv *priv, struct nikon_clk_cfg *clk_cfg)
 Configure Nikon clock. More...
 
struct nikon_privnikon_init (PRUICSS_Handle gPruIcssXHandle, uint32_t slice, float_t frequency, uint32_t core_clk_freq, uint32_t uart_clk_freq, uint32_t tx_rx_clock_source, uint32_t mask, uint32_t totalch, uint32_t protocol_version)
 Initialize Nikon firmware interface address and get the pointer to struct nikon_priv instance. More...
 
void nikon_config_clr_cfg0 (struct nikon_priv *priv)
 Clear the channel specific frame size cfg registers. More...
 
int32_t nikon_calc_clock (struct nikon_priv *priv, struct nikon_clk_cfg *clk_cfg)
 Calculate Rx and Tx divisors for given frequency. More...
 
void nikon_generate_cdf (struct nikon_priv *priv, uint32_t cmd)
 Generate CDF command to be sent to encoder. Update encoder ID appropriately with nikon_update_enc_addr API. More...
 
uint64_t nikon_reverse_bits (uint64_t bits, uint32_t num_bits)
 Reverse the bits (LSB to be sent out first) provided as parameters. More...
 
uint32_t nikon_calc_3bitcrc (struct nikon_priv *priv, uint32_t cmd)
 Calculate 3 bit otf crc and generate tx command. More...
 
void nikon_config_load_share (struct nikon_priv *priv, uint8_t mask)
 Configure Load Share mode for Nikon receiver. More...
 
void nikon_config_periodic_trigger (struct nikon_priv *priv)
 Configure periodic trigger operation mode. More...
 
void nikon_config_host_trigger (struct nikon_priv *priv)
 Configure host trigger operation mode. More...
 
int32_t nikon_wait_for_encoder_detection (struct nikon_priv *priv)
 Detect whether the connected encoder is of selected frequency. More...
 
void nikon_update_enc_len (struct nikon_priv *priv, uint32_t num_encoders, uint32_t single_turn_len[], uint32_t multi_turn_len[], uint32_t ch)
 Update number of encoders connected in bus or one-to-one and update data lengths of those encoders. More...
 
void nikon_update_clock_freq (struct nikon_priv *priv, float_t frequency)
 Update the operating baud rate as user specified baud rate through UART menu. More...
 
uint32_t nikon_get_current_channel (struct nikon_priv *priv, uint32_t ch_idx)
 Retrives the current channel in use. More...
 
uint32_t nikon_get_totalchannels (struct nikon_priv *priv)
 Retrives total number of channels configured. More...
 
void nikon_update_enc_addr (struct nikon_priv *priv, uint32_t enc_addr, uint32_t ls_ch)
 Update encoder address as specified by the user. Default initial address is 0. More...
 
void nikon_update_eeprom_addr (struct nikon_priv *priv, uint8_t addr, uint32_t ls_ch)
 Access encoder's EEPROM location specified by the user. More...
 
void nikon_update_eeprom_data (struct nikon_priv *priv, uint16_t data, uint32_t ls_ch)
 Write data at specified EEPROM location. More...
 
void nikon_update_id_code (struct nikon_priv *priv, uint32_t data, uint32_t ls_ch)
 Assign the specified 24bits as Identification code of encoder. More...
 
void nikon_update_velocity_coefficient (struct nikon_priv *priv, uint32_t data, uint32_t ls_ch)
 Assign the specified 19 bits as velocity coefficient of encoder. More...
 
void nikon_update_eeprom_bank (struct nikon_priv *priv, uint8_t bank, uint32_t ls_ch)
 Configure bank for memory operations in Nikon 3.0. More...
 

Function Documentation

◆ nikon_command_wait()

int32_t nikon_command_wait ( struct nikon_priv priv)

Wait till PRU finishes Nikon transaction.

Parameters
[in]privcookie returned by nikon_init

◆ nikon_get_pos()

int32_t nikon_get_pos ( struct nikon_priv priv,
uint32_t  cmd 
)

Get single cycle Nikon position data.

Parameters
[in]privcookie returned by nikon_init
[in]cmdcommand code specified by user

◆ nikon_config_clock()

void nikon_config_clock ( struct nikon_priv priv,
struct nikon_clk_cfg clk_cfg 
)

Configure Nikon clock.

Parameters
[in]privcookie returned by nikon_init
[in]clk_cfgpointer to structure containing clock configuration data

◆ nikon_init()

struct nikon_priv* nikon_init ( PRUICSS_Handle  gPruIcssXHandle,
uint32_t  slice,
float_t  frequency,
uint32_t  core_clk_freq,
uint32_t  uart_clk_freq,
uint32_t  tx_rx_clock_source,
uint32_t  mask,
uint32_t  totalch,
uint32_t  protocol_version 
)

Initialize Nikon firmware interface address and get the pointer to struct nikon_priv instance.

Parameters
[in]gPruIcssXHandleNikon firmware interface address
[in]sliceICSS PRU SLICE
[in]frequencyInput frequency
[in]core_clk_freqCore clock frequency
[in]uart_clk_freqUart clock frequency
[in]tx_rx_clock_sourceClock Source Selection
[in]maskMask for the selected channels
[in]totalchTotal number of selected channels
[in]protocol_versionNIKON_PROTOCOL_V2_1 or NIKON_PROTOCOL_V3_0
Return values
privpointer to struct nikon_priv instance

◆ nikon_config_clr_cfg0()

void nikon_config_clr_cfg0 ( struct nikon_priv priv)

Clear the channel specific frame size cfg registers.

Parameters
[in]privcookie returned by nikon_init

◆ nikon_calc_clock()

int32_t nikon_calc_clock ( struct nikon_priv priv,
struct nikon_clk_cfg clk_cfg 
)

Calculate Rx and Tx divisors for given frequency.

Parameters
[in]privcookie returned by nikon_init
[in]clk_cfgpointer to structure containing clock configuration data.

◆ nikon_generate_cdf()

void nikon_generate_cdf ( struct nikon_priv priv,
uint32_t  cmd 
)

Generate CDF command to be sent to encoder. Update encoder ID appropriately with nikon_update_enc_addr API.

Parameters
[in]privcookie returned by nikon_init
[in]cmdcommand code requested by the user.

◆ nikon_reverse_bits()

uint64_t nikon_reverse_bits ( uint64_t  bits,
uint32_t  num_bits 
)

Reverse the bits (LSB to be sent out first) provided as parameters.

Parameters
[in]bitsfield to be reversed as specified by the user.
[in]num_bitswidth of field to be reversed.
Return values
resreturn the reversed field.

◆ nikon_calc_3bitcrc()

uint32_t nikon_calc_3bitcrc ( struct nikon_priv priv,
uint32_t  cmd 
)

Calculate 3 bit otf crc and generate tx command.

Parameters
[in]privcookie returned by nikon_init
[in]cmdcdf or mdf command to be included in 3 bit crc calculation.

◆ nikon_config_load_share()

void nikon_config_load_share ( struct nikon_priv priv,
uint8_t  mask 
)

Configure Load Share mode for Nikon receiver.

Parameters
[in]privcookie returned by nikon_init
[in]maskchannel mask

◆ nikon_config_periodic_trigger()

void nikon_config_periodic_trigger ( struct nikon_priv priv)

Configure periodic trigger operation mode.

Parameters
[in]privcookie returned by nikon_init

◆ nikon_config_host_trigger()

void nikon_config_host_trigger ( struct nikon_priv priv)

Configure host trigger operation mode.

Parameters
[in]privcookie returned by nikon_init

◆ nikon_wait_for_encoder_detection()

int32_t nikon_wait_for_encoder_detection ( struct nikon_priv priv)

Detect whether the connected encoder is of selected frequency.

Parameters
[in]privcookie returned by nikon_init

◆ nikon_update_enc_len()

void nikon_update_enc_len ( struct nikon_priv priv,
uint32_t  num_encoders,
uint32_t  single_turn_len[],
uint32_t  multi_turn_len[],
uint32_t  ch 
)

Update number of encoders connected in bus or one-to-one and update data lengths of those encoders.

Parameters
[in]privcookie returned by nikon_init
[in]num_encodersnumber of encoders connected to each channel
[in]single_turn_lenEncoder's single turn resolution
[in]multi_turn_lenEncoder's multi turn resolution
[in]chchannel in use

◆ nikon_update_clock_freq()

void nikon_update_clock_freq ( struct nikon_priv priv,
float_t  frequency 
)

Update the operating baud rate as user specified baud rate through UART menu.

Parameters
[in]privcookie returned by nikon_init
[in]frequencyfrequency as specified by the user

◆ nikon_get_current_channel()

uint32_t nikon_get_current_channel ( struct nikon_priv priv,
uint32_t  ch_idx 
)

Retrives the current channel in use.

Parameters
[in]privcookie returned by nikon_init
[in]ch_idxindex of current channel to be selected
Return values
channel[ch_idx]current channel in use

◆ nikon_get_totalchannels()

uint32_t nikon_get_totalchannels ( struct nikon_priv priv)

Retrives total number of channels configured.

Parameters
[in]privcookie returned by nikon_init
Return values
totalchannelstotal number of channels configured

◆ nikon_update_enc_addr()

void nikon_update_enc_addr ( struct nikon_priv priv,
uint32_t  enc_addr,
uint32_t  ls_ch 
)

Update encoder address as specified by the user. Default initial address is 0.

Parameters
[in]privcookie returned by nikon_init
[in]enc_addrencoder address specified by the user
[in]ls_chchannel in use in load share or 0 in case of single channel mode

◆ nikon_update_eeprom_addr()

void nikon_update_eeprom_addr ( struct nikon_priv priv,
uint8_t  addr,
uint32_t  ls_ch 
)

Access encoder's EEPROM location specified by the user.

Parameters
[in]privcookie returned by nikon_init
[in]addrEEPROM address (Bits [7:0] in addr)
[in]ls_chchannel in use in load share or 0 in case of single channel mode

◆ nikon_update_eeprom_data()

void nikon_update_eeprom_data ( struct nikon_priv priv,
uint16_t  data,
uint32_t  ls_ch 
)

Write data at specified EEPROM location.

Parameters
[in]privcookie returned by nikon_init
[in]datadata to write at EEPROM location (Bits [15:0] in data)
[in]ls_chchannel in use in load share or 0 in case of single channel mode

◆ nikon_update_id_code()

void nikon_update_id_code ( struct nikon_priv priv,
uint32_t  data,
uint32_t  ls_ch 
)

Assign the specified 24bits as Identification code of encoder.

Parameters
[in]privcookie returned by nikon_init
[in]datadata to assign as ID code (Bits [23:0] in data will be used)
[in]ls_chchannel in use in load share or 0 in case of single channel mode

◆ nikon_update_velocity_coefficient()

void nikon_update_velocity_coefficient ( struct nikon_priv priv,
uint32_t  data,
uint32_t  ls_ch 
)

Assign the specified 19 bits as velocity coefficient of encoder.

Parameters
[in]privcookie returned by nikon_init
[in]datadata to assign as velocity coefficient (Bits [18:0] in data will be used)
[in]ls_chchannel in use in load share or 0 in case of single channel mode

◆ nikon_update_eeprom_bank()

void nikon_update_eeprom_bank ( struct nikon_priv priv,
uint8_t  bank,
uint32_t  ls_ch 
)

Configure bank for memory operations in Nikon 3.0.

Parameters
[in]privCookie returned by nikon_init
[in]bankBank number to be set (Bits [7:0] in bank)
[in]ls_chchannel in use in load share or 0 in case of single channel mode