hsrPrp_Config Structure storing the global variables
Data Fields | |
| uint16_t | redSeqNr |
| uint16_t | supSeqNr |
| int * | collision_pkt_dropped |
| int * | num_of_collision_occured |
| ICSS_EMAC_Handle | icssEmacHandle |
| uint32_t | redPruCheckTimerHostTableFlag |
| uint32_t | redPruCheckTimerNodeTableClear |
| ClockP_Object | redPruCheckTimer |
| ClockP_Object | redLifeCheckTimer |
| RED_FRAME * | redSupFrame |
| TaskP_Object | redSupTask |
| TaskP_Object | hsrPrpNodetableRefreshTask |
| SemaphoreP_Object | redLifeCheckSemaphore |
| SemaphoreP_Object | nodesTableSemaphore |
| RED_INDEX_ARRAY_ENTRY * | indexArrayBase |
| RED_BIN_ARRAY_ENTRY * | binArrayBase |
| RED_NODE_TABLE_ENTRY * | nodeTableBase |
| uint16_t hsrPrp_Config::redSeqNr |
| uint16_t hsrPrp_Config::supSeqNr |
| int* hsrPrp_Config::collision_pkt_dropped |
| int* hsrPrp_Config::num_of_collision_occured |
| ICSS_EMAC_Handle hsrPrp_Config::icssEmacHandle |
| uint32_t hsrPrp_Config::redPruCheckTimerHostTableFlag |
| uint32_t hsrPrp_Config::redPruCheckTimerNodeTableClear |
| ClockP_Object hsrPrp_Config::redPruCheckTimer |
| ClockP_Object hsrPrp_Config::redLifeCheckTimer |
| RED_FRAME* hsrPrp_Config::redSupFrame |
| TaskP_Object hsrPrp_Config::redSupTask |
| TaskP_Object hsrPrp_Config::hsrPrpNodetableRefreshTask |
| SemaphoreP_Object hsrPrp_Config::redLifeCheckSemaphore |
| SemaphoreP_Object hsrPrp_Config::nodesTableSemaphore |
| RED_INDEX_ARRAY_ENTRY* hsrPrp_Config::indexArrayBase |
| RED_BIN_ARRAY_ENTRY* hsrPrp_Config::binArrayBase |
| RED_NODE_TABLE_ENTRY* hsrPrp_Config::nodeTableBase |