Functions | |
| void | HsrFrameFill (hsrPrpHandle *, RED_FRAME *pRedFrame, const uint8_t *pFrame, int32_t frameSize) |
| void | HsrFrameUpdatePathId (RED_FRAME *pRedFrame, uint16_t pathId) |
| Updates PATH ID of a RED_FRAME. More... | |
| RED_FRAME * | HsrSupFrameAllocate (hsrPrpHandle *) |
| Allocates a RED_FRAME that holds HSR Supervision frame. More... | |
| void | HsrSupFrameUpdateSrcAdd (RED_FRAME *pRedFrame, uint8_t *srcAdd) |
| Updates Source Address of a HSR Supervision frame. More... | |
| void | HsrSupFrameUpdatePathId (RED_FRAME *pRedFrame, uint16_t pathId) |
| void | HsrSupFrameUpdateSeqNr (hsrPrpHandle *, RED_FRAME *pRedFrame) |
| void | HsrSupFrameIncrementSeqNr (hsrPrpHandle *) |
| void HsrFrameFill | ( | hsrPrpHandle * | , |
| RED_FRAME * | pRedFrame, | ||
| const uint8_t * | pFrame, | ||
| int32_t | frameSize | ||
| ) |
| void HsrFrameUpdatePathId | ( | RED_FRAME * | pRedFrame, |
| uint16_t | pathId | ||
| ) |
| RED_FRAME* HsrSupFrameAllocate | ( | hsrPrpHandle * | ) |
| void HsrSupFrameUpdateSrcAdd | ( | RED_FRAME * | pRedFrame, |
| uint8_t * | srcAdd | ||
| ) |
Updates Source Address of a HSR Supervision frame.
| pRedFrame | pointer to a RED_FRAME |
| srcAdd | pointer to a new source address value |
| void HsrSupFrameUpdatePathId | ( | RED_FRAME * | pRedFrame, |
| uint16_t | pathId | ||
| ) |
| void HsrSupFrameUpdateSeqNr | ( | hsrPrpHandle * | , |
| RED_FRAME * | pRedFrame | ||
| ) |
| void HsrSupFrameIncrementSeqNr | ( | hsrPrpHandle * | ) |