Tamagawa Interface Received data.
Data Fields | |
| uint32_t | abs |
| uint32_t | abm |
| uint8_t | cf |
| uint8_t | sf |
| uint8_t | enid |
| uint8_t | almc |
| uint8_t | adf |
| uint8_t | edf |
| uint8_t | crc |
| uint32_t rx_frames_received::abs |
Data in one revolution
| uint32_t rx_frames_received::abm |
Multi-turn Data
| uint8_t rx_frames_received::cf |
Control Frame
| uint8_t rx_frames_received::sf |
Status Frame
| uint8_t rx_frames_received::enid |
Encoder ID
| uint8_t rx_frames_received::almc |
Encoder error
| uint8_t rx_frames_received::adf |
EEPROM address
| uint8_t rx_frames_received::edf |
EEPROM data
| uint8_t rx_frames_received::crc |
CRC