Defines DCL_PID shadow parameter set used for updating controller parameter.
Data Fields | |
| float32_t | Kp |
| Proportional gain. More... | |
| float32_t | Ki |
| Integral gain. More... | |
| float32_t | Kd |
| Derivative gain. More... | |
| float32_t | Kr |
| Set point weight, default is 1. More... | |
| float32_t | c1 |
| D path low-pass filter coefficient 1, default is 1. More... | |
| float32_t | c2 |
| D path low-pass filter coefficient 2, default is 0. More... | |
| float32_t | Umax |
| Upper saturation limit. More... | |
| float32_t | Umin |
| Lower saturation limit. More... | |
| float32_t DCL_PID_SPS::Kp |
Proportional gain.
| float32_t DCL_PID_SPS::Ki |
Integral gain.
| float32_t DCL_PID_SPS::Kd |
Derivative gain.
| float32_t DCL_PID_SPS::Kr |
Set point weight, default is 1.
| float32_t DCL_PID_SPS::c1 |
D path low-pass filter coefficient 1, default is 1.
| float32_t DCL_PID_SPS::c2 |
D path low-pass filter coefficient 2, default is 0.
| float32_t DCL_PID_SPS::Umax |
Upper saturation limit.
| float32_t DCL_PID_SPS::Umin |
Lower saturation limit.